How to set output signal of KMZ80 to SENT style?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to set output signal of KMZ80 to SENT style?

2,630 次查看
freshtiny
Contributor I

I was told that KMZ80 chip is delivered by NXP with default AD signal style, and if customers want to use SENT signal style, we have to calibrate the chip by ourselves, is that correct?
Could we purchase KMZ80 with SENT signal style directly? I did not find useful related description about setting method of output signal format from KMZ80 product data sheet(rev.3 -- 26 April 2019).

标签 (1)
0 项奖励
回复
4 回复数

2,557 次查看
wtfan
NXP Employee
NXP Employee

Hi Ma Liang,

Thanks for using KMZ80, you will need a programming kit to program the sensor register to switch to SENT output mode, please get in touch with cindy.zhang@nxp.com to get a kit.

Rgs,

Wenting

0 项奖励
回复

2,557 次查看
freshtiny
Contributor I

> please get in touch with cindy.zhang@nxp.com to get a kit.
OK, I'll contact later.

0 项奖励
回复

2,557 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Liang,

As you can notice in the datasheet (Chapter 8), the KMZ80 provides a digital output signal on pin OUT/DATA (if bit 12 in register SYS_SETTING is set to logic 1) compliant with the SAE J2716 SENT standard.

 

The measured angle α is converted linearly into a value, which is digital encoded in SENT frames. Either a positive or a negative angular slope characteristic is provided for this purpose.

 

Best regards,

Tomas

0 项奖励
回复

2,557 次查看
freshtiny
Contributor I

Thank you, now I notice that.

0 项奖励
回复