Hi, is there a way to save the i2c free programmable slave address of MMA995xL sensor module ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, is there a way to save the i2c free programmable slave address of MMA995xL sensor module ?

1,344 Views
nxp_user
Contributor I

Hi, is there a way to save the i2c free programmable slave address of MMA995xL sensor module ?

Labels (1)
0 Kudos
Reply
3 Replies

1,144 Views
nxp_user
Contributor I

MMA9550L

Thanks

0 Kudos
Reply

1,144 Views
JackITB
NXP Employee
NXP Employee

Ok thanks,

One possibility is to do this "programmatically": i.e. add a custom application that changes the Slave Port Address during MMA9550L initialization (see SP_ADDR register in MMA955xL Hardware Reference manual p.108). You can find information about developing custom user application in AN4129.

Regards,   Jacques.

0 Kudos
Reply

1,144 Views
JackITB
NXP Employee
NXP Employee

Hi Enrico,

Yes, this should be doable. Nevertheless we need more information from you, more specifically which version are you considering (between MMA9550, MMA9551, MMA9553, MMA9555, MMA9559...), as their Firmware differ and may be a limiting factor.

Regards,   Jacques.

0 Kudos
Reply