Hi, is there a way to save the i2c free programmable slave address of MMA995xL sensor module ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi, is there a way to save the i2c free programmable slave address of MMA995xL sensor module ?

1,369件の閲覧回数
nxp_user
Contributor I

Hi, is there a way to save the i2c free programmable slave address of MMA995xL sensor module ?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,169件の閲覧回数
nxp_user
Contributor I

MMA9550L

Thanks

0 件の賞賛
返信

1,169件の閲覧回数
JackITB
NXP Employee
NXP Employee

Ok thanks,

One possibility is to do this "programmatically": i.e. add a custom application that changes the Slave Port Address during MMA9550L initialization (see SP_ADDR register in MMA955xL Hardware Reference manual p.108). You can find information about developing custom user application in AN4129.

Regards,   Jacques.

0 件の賞賛
返信

1,169件の閲覧回数
JackITB
NXP Employee
NXP Employee

Hi Enrico,

Yes, this should be doable. Nevertheless we need more information from you, more specifically which version are you considering (between MMA9550, MMA9551, MMA9553, MMA9555, MMA9559...), as their Firmware differ and may be a limiting factor.

Regards,   Jacques.

0 件の賞賛
返信