Hi Jane, ​I need pressure sensor which can be use to detect the changes in pressure inside the tube. ​Also it can able to detect the small variation also. ​Please suggest suitable sensor. ​ ​Priyesh Sah

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hi Jane, ​I need pressure sensor which can be use to detect the changes in pressure inside the tube. ​Also it can able to detect the small variation also. ​Please suggest suitable sensor. ​ ​Priyesh Sah

766 次查看
PriyeshSah
Contributor I


I need pressure sensor which can be use to detect the changes in pressure inside the tube.
Also it can able to detect the small variation also.
Please suggest suitable sensor.

Priyesh Sah

0 项奖励
回复
1 回复

679 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Priyesh,

I have already answered this question internally (Case #00131810). If you have any additional questions, please use this Case.

Best regards,

Tomas

0 项奖励
回复