Hi Jane, ​I need pressure sensor which can be use to detect the changes in pressure inside the tube. ​Also it can able to detect the small variation also. ​Please suggest suitable sensor. ​ ​Priyesh Sah

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi Jane, ​I need pressure sensor which can be use to detect the changes in pressure inside the tube. ​Also it can able to detect the small variation also. ​Please suggest suitable sensor. ​ ​Priyesh Sah

767 Views
PriyeshSah
Contributor I


I need pressure sensor which can be use to detect the changes in pressure inside the tube.
Also it can able to detect the small variation also.
Please suggest suitable sensor.

Priyesh Sah

0 Kudos
Reply
1 Reply

680 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Priyesh,

I have already answered this question internally (Case #00131810). If you have any additional questions, please use this Case.

Best regards,

Tomas

0 Kudos
Reply