Help: Distance Sensor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help: Distance Sensor

ソリューションへジャンプ
5,044件の閲覧回数
Apoorv_iitd
Contributor I

I am working on a micromouse. I need some Accurate Proximity Sensors. Could anyone help me out on this field.

タグ(1)
0 件の賞賛
返信
1 解決策
3,758件の閲覧回数
Joshevelle
Senior Contributor I

I would recommend you the MPR121, very low power: 29 μA supply current with 12 electrodes being monitored with 64 ms response time and IRQ enabled.

Proximity sensors are very small (3x3mm). If you want to accelerate the evaluation stage of your project I would highly recommend you to get the KITMPR121EVM: KITMPR121EVM Product Summary Page

Is a very low cost evaluation board for the MPR121 and you can test the device out of the box.

hope it helps =)

Josh

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,759件の閲覧回数
Joshevelle
Senior Contributor I

I would recommend you the MPR121, very low power: 29 μA supply current with 12 electrodes being monitored with 64 ms response time and IRQ enabled.

Proximity sensors are very small (3x3mm). If you want to accelerate the evaluation stage of your project I would highly recommend you to get the KITMPR121EVM: KITMPR121EVM Product Summary Page

Is a very low cost evaluation board for the MPR121 and you can test the device out of the box.

hope it helps =)

Josh

0 件の賞賛
返信
3,758件の閲覧回数
GrungeRey
Contributor I
Try MPR03X or MPR084 if needed more sensor.
0 件の賞賛
返信