Help: Distance Sensor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Help: Distance Sensor

跳至解决方案
5,029 次查看
Apoorv_iitd
Contributor I

I am working on a micromouse. I need some Accurate Proximity Sensors. Could anyone help me out on this field.

标记 (1)
0 项奖励
回复
1 解答
3,743 次查看
Joshevelle
Senior Contributor I

I would recommend you the MPR121, very low power: 29 μA supply current with 12 electrodes being monitored with 64 ms response time and IRQ enabled.

Proximity sensors are very small (3x3mm). If you want to accelerate the evaluation stage of your project I would highly recommend you to get the KITMPR121EVM: KITMPR121EVM Product Summary Page

Is a very low cost evaluation board for the MPR121 and you can test the device out of the box.

hope it helps =)

Josh

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,744 次查看
Joshevelle
Senior Contributor I

I would recommend you the MPR121, very low power: 29 μA supply current with 12 electrodes being monitored with 64 ms response time and IRQ enabled.

Proximity sensors are very small (3x3mm). If you want to accelerate the evaluation stage of your project I would highly recommend you to get the KITMPR121EVM: KITMPR121EVM Product Summary Page

Is a very low cost evaluation board for the MPR121 and you can test the device out of the box.

hope it helps =)

Josh

0 项奖励
回复
3,743 次查看
GrungeRey
Contributor I
Try MPR03X or MPR084 if needed more sensor.
0 项奖励
回复