Help: Distance Sensor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help: Distance Sensor

Jump to solution
5,042 Views
Apoorv_iitd
Contributor I

I am working on a micromouse. I need some Accurate Proximity Sensors. Could anyone help me out on this field.

Tags (1)
0 Kudos
Reply
1 Solution
3,756 Views
Joshevelle
Senior Contributor I

I would recommend you the MPR121, very low power: 29 μA supply current with 12 electrodes being monitored with 64 ms response time and IRQ enabled.

Proximity sensors are very small (3x3mm). If you want to accelerate the evaluation stage of your project I would highly recommend you to get the KITMPR121EVM: KITMPR121EVM Product Summary Page

Is a very low cost evaluation board for the MPR121 and you can test the device out of the box.

hope it helps =)

Josh

View solution in original post

0 Kudos
Reply
2 Replies
3,757 Views
Joshevelle
Senior Contributor I

I would recommend you the MPR121, very low power: 29 μA supply current with 12 electrodes being monitored with 64 ms response time and IRQ enabled.

Proximity sensors are very small (3x3mm). If you want to accelerate the evaluation stage of your project I would highly recommend you to get the KITMPR121EVM: KITMPR121EVM Product Summary Page

Is a very low cost evaluation board for the MPR121 and you can test the device out of the box.

hope it helps =)

Josh

0 Kudos
Reply
3,756 Views
GrungeRey
Contributor I
Try MPR03X or MPR084 if needed more sensor.
0 Kudos
Reply