FXOS8700CQ: Magnetometer Offset/Threshold Value Problem 

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FXOS8700CQ: Magnetometer Offset/Threshold Value Problem 

2,301 次查看
lukelynch
Contributor III

Hello,

 

I have a problem with my threshold value and offset value on the z-axis off the magnetometer.

 

With no magnets in place, I take a couple of readings and get an average. I then left shift this value one place and write it to the M_OFF_Z register to account for the natural magnetic field of the earth. This works perfectly, i take some readings after i have wrote to the registers and the readings are roughly 0.

 

My problem is when with the threshold value i feel. With my offset done, i put a magnet in place, take a couple of readings to get an average, I then directly write this number(absolute, not shifted etc) to the z-axis Threshold register. I then go to test this to make sure its all ok (when the magnetic field strength on the z-axis exceeds that of the threshold value it will generate an interrupt). But my interrupt is generated before it can reach the value of the threshold value. My interrupt is generated exactly my threshold value minus my offset value (before been left shifted).

 

From my understanding from the datasheet:" The thresholds for each axis are applied after the magnetic data has been adjusted by the offset values stored in the M_OFF_X/Y/Z registers when M_CTRL_REG3[m_raw] = 0".  my m_raw is 0.

 

From what i can see my offset is ignoring by threshold. Can anyone help me with this?

 

Regards,

Luke.

标签 (1)
0 项奖励
回复
4 回复数

1,772 次查看
aswins
NXP Employee
NXP Employee

Hi Luke,

                 Greetings!.The problem is currently under investigation with the design team for FXOS8700. It will be resolved in a week.Will update you shortly.

Thanks for your patience.!

Regards

Aswin

0 项奖励
回复

1,772 次查看
michaelestanley
NXP Employee
NXP Employee

Luke,

Has Aswin covered this in the other thread, or do we need to pull him in here?

Mike

0 项奖励
回复

1,772 次查看
lukelynch
Contributor III

I don't think this specific problem has been covered in the last topic.

Aswin help would be great.

0 项奖励
回复

1,772 次查看
reyes
NXP TechSupport
NXP TechSupport

aswins can you please take a look at Luke's question from above, please?

0 项奖励
回复