FXOS8700CQ上电后,其SCL/SDA引脚的初始电平是高还是低???

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FXOS8700CQ上电后,其SCL/SDA引脚的初始电平是高还是低???

ソリューションへジャンプ
2,216件の閲覧回数
胡维坤
Contributor I

After power on the FXOS8700CQ, is the SCL/SDA pin hign or low at the first??

ラベル(2)
0 件の賞賛
返信
1 解決策
1,751件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Once set for I2C operation (SA0 pin connected to GND or VDDIO), both the SDA nad SCL pins will be in a high impedance state, so with pull-up resistors on the bus, the SDA and SCL lines are both high.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,752件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Once set for I2C operation (SA0 pin connected to GND or VDDIO), both the SDA nad SCL pins will be in a high impedance state, so with pull-up resistors on the bus, the SDA and SCL lines are both high.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 件の賞賛
返信
1,751件の閲覧回数
胡维坤
Contributor I

Dear Tomas Vaverka,

     Thanks for your answer, my last problem have been insolved but I have another question now.

     I have made the bus pulled up with 4.7KΩ resistors, and the  SDA and SCL both are hign when I reset FXOS8700CQ, so do INT1 and INT2, and I made the SDA0、SDA1 connected to GND. The question is the master can give the ST singal、 slave address and write bit correctly , but the slave(FXOS8700CQ) just cann't send the ACK to the master , so the register value cann't be read or write .

     First I guess that if the FXOS8700CQ doesn't work , but the INT1 and INT2 bins are both hign , while after I power it off they are both low ; Then the no.2 bin and no.8 bin are in a high impedance state , I don't know if it's true state or false state.

     By the way , the VDD and VDDIO connected together to 3.3V

0 件の賞賛
返信