After power on the FXOS8700CQ, is the SCL/SDA pin hign or low at the first??
Solved! Go to Solution.
Hi,
Once set for I2C operation (SA0 pin connected to GND or VDDIO), both the SDA nad SCL pins will be in a high impedance state, so with pull-up resistors on the bus, the SDA and SCL lines are both high.
Regards,
Tomas
PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.
Hi,
Once set for I2C operation (SA0 pin connected to GND or VDDIO), both the SDA nad SCL pins will be in a high impedance state, so with pull-up resistors on the bus, the SDA and SCL lines are both high.
Regards,
Tomas
PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.
Dear Tomas Vaverka,
Thanks for your answer, my last problem have been insolved but I have another question now.
I have made the bus pulled up with 4.7KΩ resistors, and the SDA and SCL both are hign when I reset FXOS8700CQ, so do INT1 and INT2, and I made the SDA0、SDA1 connected to GND. The question is the master can give the ST singal、 slave address and write bit correctly , but the slave(FXOS8700CQ) just cann't send the ACK to the master , so the register value cann't be read or write .
First I guess that if the FXOS8700CQ doesn't work , but the INT1 and INT2 bins are both hign , while after I power it off they are both low ; Then the no.2 bin and no.8 bin are in a high impedance state , I don't know if it's true state or false state.
By the way , the VDD and VDDIO connected together to 3.3V