FXLS8964 FXLS8974 - vector magnitude

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FXLS8964 FXLS8974 - vector magnitude

ソリューションへジャンプ
2,633件の閲覧回数
adrian_chmiel
Contributor III

Hi,

We replece discontinued FLXS8471 at new FXLS8974.

At this moment we use vector magnitude feature for detecting a change in the tilt angle.

New FXLS8974 has a different mechanism for vector magnitude and I'm not sure, there is possible to set for example detection angle change of 5deg?

of between 123deg to 127deg ? Or it's not so flexible?

 

Best regards

Adrian Chmiel

タグ(1)
0 件の賞賛
返信
1 解決策
2,625件の閲覧回数
JackITB
NXP Employee
NXP Employee

Hi Adrian,

As you mentioned, FXLS8974 has a different mechanism for vector magnitude vs FXLS8471.
Key difference being that FXLS8974 does not have the A_VECM_INIT_XYZ registers that can be substracted to the measured XYZ raw data.

So I don't see an easy way to implement your use case.

A potential idea could be to use the orientation detection block but you'll be limited to its discrete/fixed thresholds.

 

Best regards,  Jacques

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,626件の閲覧回数
JackITB
NXP Employee
NXP Employee

Hi Adrian,

As you mentioned, FXLS8974 has a different mechanism for vector magnitude vs FXLS8471.
Key difference being that FXLS8974 does not have the A_VECM_INIT_XYZ registers that can be substracted to the measured XYZ raw data.

So I don't see an easy way to implement your use case.

A potential idea could be to use the orientation detection block but you'll be limited to its discrete/fixed thresholds.

 

Best regards,  Jacques

0 件の賞賛
返信
2,556件の閲覧回数
adrian_chmiel
Contributor III

Thanks Jack.

 

Do you have aplication note for orientation detection block?

I try to understand base on datasheed and AN12004, but maybe you have something extra?

It's not clear for me how excacly is conected register ORIENT_BF_ZCOMP with ORIENT_THS and how to use it.

 

BR

Adrian

0 件の賞賛
返信