Displacement detection using FXOS8700CQ in FRDMK64F

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Displacement detection using FXOS8700CQ in FRDMK64F

924 次查看
yosabath
Contributor I

Dear All,

i am using FRDMK64F with matlab support package to identify the displacement.

The test case i am trying is that, moving the FRDM board like 'A' shape and collect the data and do a scatter plot on Matlab. The resultant pattern on the plot is always clumsy.

Base model sample rate is 1ms(task time). The ODR rate is 200Hz. also i tried other ODR rates but the result is same.

can anyone please help me?

Thanks,

Yosa

标签 (1)
0 项奖励
回复
1 回复

831 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi  Yosabath,

Is not the sample rate of 1ms too fast considering the ODR of 200Hz? 

Anyway, in theory double integration method gives you what you need, but in practice double integration accumulates the errors in the measurement, so the results are usually not very accurate or reliable to use for such a measurement.

Best regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

0 项奖励
回复