Difference between MPL3115A2 and MPL3115A2S

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference between MPL3115A2 and MPL3115A2S

Jump to solution
1,151 Views
CL_ENVEA
Contributor I

Hello,

 

I am wondering what is the difference between MPL3115A2 and MPL3115A2S

I can't tell why there is a change in reference as the datasheet seems identical.

Thanks in advance,

0 Kudos
Reply
1 Solution
1,147 Views
CL_ENVEA
Contributor I

I got a quick reply from the tech support: 100% compatible, just a new fab

View solution in original post

0 Kudos
Reply
2 Replies
1,148 Views
CL_ENVEA
Contributor I

I got a quick reply from the tech support: 100% compatible, just a new fab

0 Kudos
Reply
1,138 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear CL_ENVEA,

yes, this is correct. It is the same component. Thank you for posting the answer here, for other customer's convinience.

With Best Regards,

Jozef

0 Kudos
Reply