Difference between MPL3115A2 and MPL3115A2S

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between MPL3115A2 and MPL3115A2S

ソリューションへジャンプ
1,154件の閲覧回数
CL_ENVEA
Contributor I

Hello,

 

I am wondering what is the difference between MPL3115A2 and MPL3115A2S

I can't tell why there is a change in reference as the datasheet seems identical.

Thanks in advance,

0 件の賞賛
返信
1 解決策
1,150件の閲覧回数
CL_ENVEA
Contributor I

I got a quick reply from the tech support: 100% compatible, just a new fab

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,151件の閲覧回数
CL_ENVEA
Contributor I

I got a quick reply from the tech support: 100% compatible, just a new fab

0 件の賞賛
返信
1,141件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear CL_ENVEA,

yes, this is correct. It is the same component. Thank you for posting the answer here, for other customer's convinience.

With Best Regards,

Jozef

0 件の賞賛
返信