Controlling the Sensor Measurement Interface (SMI) in FXTH870911

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Controlling the Sensor Measurement Interface (SMI) in FXTH870911

ソリューションへジャンプ
1,273件の閲覧回数
TKB
Contributor II

Hi 

Is there a way for me to control the state of the Sensor Measurement Interface (SMI) i.e. turn it OFF or ON when required or is it done by the firmware defined subroutines only?

Exploring this path for additional power savings if possible.

Thanks

Tushar

タグ(1)
0 件の賞賛
返信
1 解決策
1,265件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Tushar,

This is handled by the TPMS_READ routines: the entire measurement chain is enabled at the beginning of the routine and disabled at the end. So when the program exits the routine, everything has been turned off.

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,266件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Tushar,

This is handled by the TPMS_READ routines: the entire measurement chain is enabled at the beginning of the routine and disabled at the end. So when the program exits the routine, everything has been turned off.

Best regards,

Tomas

0 件の賞賛
返信