Bi-directional Pressure Sensor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bi-directional Pressure Sensor

4,462 次查看
jaredweldon
Contributor I

Hi,

I am currently using the MP3V5050. Is there any sensor that can perform both negative and positive  pressure measurements from the same chip?

Can an absolute sensor measure both?

Thank you

标签 (1)
0 项奖励
回复
1 回复

822 次查看
darioarias
NXP Employee
NXP Employee

Hi Jared,

We do have a few pressure sensors that can handle both negative pressure and positive pressure without resulting in damage in the device. This sensors are MPXV7002 (-2 kPa / +2 kPa), MPXV7007 (-7 kPa/ +7 kPa) and MPXV7025 (-25 kPa/25 kPa).

Absolute pressure sensors cannot measure negative pressure, because they are meant to measure the environment's pressure which is always positive.

Darío

0 项奖励
回复