MMA8652FC - Bare metal example project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMA8652FC - Bare metal example project

MMA8652FC - Bare metal example project

Hi Everyone,

 

I would like to share here another simple bare-metal example code/demo for the Xtrinsic MMA8652FC digital accelerometer that I have created while working with the Freescale FRDM-KL25Z development platform and FRDM-FXS-MULTI(-B) sensor expansion board. To visualize the acceleration data that are read from the MMA8652FC using an interrupt technique through the I2C interface, I have used the FreeMASTER tool.

 

This example illustrates:

 

1. Initialization of the MKL25Z128 MCU (mainly I2C and PORT modules).

2. I2C data write and read operations.

3. Initialization of the accelerometer to achieve the highest resolution.

4. Simple offset calibration based on the AN4069.

5. Output data reading using an interrupt technique.

6. Conversion of the output values from registers 0x01 – 0x06 to real acceleration values in g’s.

7. Visualization of the output values in the FreeMASTER tool.

 

1. As you can see in the FRDM-FXS-MULTI(-B)/FRDM-KL25Z schematics and the image below, I2C signals are routed to the I2C1 module (PTC1 and PTC2 pins) of the KL25Z MCU and the INT1 output is connected to the PTA5 pin (make sure that pin #3 of J4 and pin #2 of J6 connector on the sensor expansion board are connected together). The INT1 output of the MMA8652FC is configured as a push-pull active-low output, so the corresponding PTA5 pin configuration is GPIO with an interrupt on falling edge.

 

12383_12383.jpg

 

The MCU is, therefore, configured as follows.

void MCU_Init(void)

{

     //I2C1 module initialization

     SIM_SCGC4 |= SIM_SCGC4_I2C1_MASK;        // Turn on clock to I2C1 module

     SIM_SCGC5 |= SIM_SCGC5_PORTC_MASK;       // Turn on clock to Port C module

     PORTC_PCR1 |= PORT_PCR_MUX(0x2);         // PTC1 pin is I2C1 SCL line

     PORTC_PCR2 |= PORT_PCR_MUX(0x2);         // PTC2 pin is I2C1 SDA line

     I2C1_F  |= I2C_F_ICR(0x14);              // SDA hold time = 2.125us, SCL start hold time = 4.25us, SCL stop hold time = 5.125us

     I2C1_C1 |= I2C_C1_IICEN_MASK;            // Enable I2C1 module

           

         //Configure the PTA5 pin (connected to the INT1 of the MMA8652FC) for falling edge interrupts

     SIM_SCGC5 |= SIM_SCGC5_PORTA_MASK;       // Turn on clock to Port A module

     PORTA_PCR5 |= (0|PORT_PCR_ISF_MASK|      // Clear the interrupt flag

                      PORT_PCR_MUX(0x1)|      // PTA5 is configured as GPIO

                      PORT_PCR_IRQC(0xA));    // PTA5 is configured for falling edge interrupts

           

        //Enable PORTA interrupt on NVIC

     NVIC_ICPR |= 1 << ((INT_PORTA - 16)%32);

     NVIC_ISER |= 1 << ((INT_PORTA - 16)%32);

}

 

2. The 7-bit I2C address of the MMA8652FC is fixed value 0x1D. As shown above, the SCL line is connected to the PTC1 pin and SDA line to the PTC2 pin. The I2C clock frequency is 125 kHz.

The screenshot below shows the write operation which writes the value 0x39 to the CTRL_REG1 (0x2A).

 

12384_12384.jpg

 

And here is the single byte read from the WHO_AM_I register 0x0D. As you can see, it returns the correct value 0x4A.

 

12385_12385.jpg

 

Multiple bytes of data can be read from sequential registers after each MMA8652FC acknowledgment (AK) is received until a no acknowledge (NAK) occurs from the KL25Z followed by a stop condition (SP) signaling an end of transmission. A burst read of 6 bytes from registers 0x01 to 0x06 is shown below. It also shows how the INT1 pin is automatically deasserted by reading the acceleration output data.

 

12386_12386.jpg

 

 

3. At the beginning of the initialization, all registers are reset to their default values by setting the RST bit of the CTRL_REG2 register. The dynamic range is set to ±2g and to achieve the highest resolution, the lowest ODR (1.56Hz) and the High Resolution mode are selected (more details in AN4075). The DRDY interrupt is enabled and routed to the INT1 interrupt pin that is configured to be a push-pull, active-low output.

void MMA8652FC_Init (void)

{

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, CTRL_REG2, 0x40);          // Reset all registers to POR values

    

     Pause(0x631);          // ~1ms delay

    

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, XYZ_DATA_CFG_REG, 0x00);   // +/-2g range with ~0.977mg/LSB 

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, CTRL_REG2, 0x02);          // High Resolution mode

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, CTRL_REG3, 0x00);          // Push-pull, active low interrupt

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, CTRL_REG4, 0x01);          // Enable DRDY interrupt

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, CTRL_REG5, 0x01);          // DRDY interrupt routed to INT1 - PTA5

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, CTRL_REG1, 0x39);          // ODR = 1.56Hz, Active mode      

}

 

4. A simple offset calibration method is implemented according to the AN4069.

 

void MMA8652FC_Calibration (void)

{

     char X_offset, Y_offset, Z_offset;

    

     DataReady = 0;      

         while (!DataReady){}          // Is a first set of data ready?

     DataReady = 0;

    

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, CTRL_REG1, 0x00);          // Standby mode     

    

     I2C_ReadMultiRegisters(MMA8652FC_I2C_ADDRESS, OUT_X_MSB_REG, 6, AccelData);          // Read data output registers 0x01-0x06       

           

     Xout_12_bit = ((short) (AccelData[0]<<8 | AccelData[1])) >> 4;             // Compute 12-bit X-axis acceleration output value

     Yout_12_bit = ((short) (AccelData[2]<<8 | AccelData[3])) >> 4;             // Compute 12-bit Y-axis acceleration output value

     Zout_12_bit = ((short) (AccelData[4]<<8 | AccelData[5])) >> 4;             // Compute 12-bit Z-axis acceleration output value

           

     X_offset = Xout_12_bit / 2 * (-1);          // Compute X-axis offset correction value

     Y_offset = Yout_12_bit / 2 * (-1);          // Compute Y-axis offset correction value

     Z_offset = (Zout_12_bit - SENSITIVITY_2G) / 2 * (-1);         // Compute Z-axis offset correction value

           

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, OFF_X_REG, X_offset);            

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, OFF_Y_REG, Y_offset);      

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, OFF_Z_REG, Z_offset);      

           

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, CTRL_REG1, 0x39);          // Active mode again

}

 

5. In the ISR, only the interrupt flag is cleared and the DataReady variable is set to indicate the arrival of new data.

 

void PORTA_IRQHandler()

{

     PORTA_PCR5 |= PORT_PCR_ISF_MASK;          // Clear the interrupt flag

     DataReady = 1;   

}

 

6. The output values from accelerometer registers 0x01 – 0x06 are first converted to signed 12-bit values and afterwards to real values in g’s.

 

if (DataReady)             // Is a new set of data ready?

{            

     DataReady = 0;

                                                                                                                  

     I2C_ReadMultiRegisters(MMA8652FC_I2C_ADDRESS, OUT_X_MSB_REG, 6, AccelData);          // Read data output registers 0x01-0x06

         

         // 12-bit accelerometer data

     Xout_12_bit = ((short) (AccelData[0]<<8 | AccelData[1])) >> 4;             // Compute 12-bit X-axis acceleration output value

     Yout_12_bit = ((short) (AccelData[2]<<8 | AccelData[3])) >> 4;             // Compute 12-bit Y-axis acceleration output value

     Zout_12_bit = ((short) (AccelData[4]<<8 | AccelData[5])) >> 4;             // Compute 12-bit Z-axis acceleration output value

                  

         // Accelerometer data converted to g's

     Xout_g = ((float) Xout_12_bit) / SENSITIVITY_2G;              // Compute X-axis output value in g's

     Yout_g = ((float) Yout_12_bit) / SENSITIVITY_2G;              // Compute Y-axis output value in g's

     Zout_g = ((float) Zout_12_bit) / SENSITIVITY_2G;              // Compute Z-axis output value in g's              

}  

 

7. The calculated values can be watched in the "Variables" window on the top right of the Debug perspective or in the FreeMASTER application. To open and run the FreeMASTER project, install the FreeMASTER application and FreeMASTER Communication Driver.

 

12387_12387.jpg

 

12388_12388.jpg

 

Attached you can find the complete source code written in the CW for MCU's (Eclipse IDE) including the FreeMASTER project.

 

If there are any questions regarding this simple application, do not hesitate to ask below. Your feedback or suggestions are also welcome.

 

Regards,

Tomas

ラベル(1)
添付
コメント

Hello Tomas,

I found this project very helpful, and I follow it to configure my MMA8652FC.

But I want to work with it using only 8 bits.

I'm able to configure it to use only 8 bits, and I get the Xout_8_bit, Yout_8_bit, Zout_8_bit. But how do I calculate the offset values?

X_offset_8_bit = ?

Y_offset_8_bit = ?

Z_offset_8_bit = ?

Can you help me?

Thanks.

Regards,

Sérgio

Hello Sérgio,

 

SENSITIVITY_2G_8bits        64

SENSITIVITY_4G_8bits        32

SENSITIVITY_8G_8bits        16

 

±2g:

X_offset_2G_8_bit = Xout_8_bit * 8 * (-1);   

Y_offset_2G_8_bit = Yout_8_bit * 8 * (-1);   

Z_offset_2G_8_bit = (Zout_8_bit - SENSITIVITY_2G_8bits) * 8 * (-1);

 

±4g:

X_offset_4G_8_bit = Xout_8_bit * 16 * (-1);   

Y_offset_4G_8_bit = Yout_8_bit * 16 * (-1);   

Z_offset_4G_8_bit = (Zout_8_bit - SENSITIVITY_4G_8bits) * 16 * (-1);

 

±8g:

X_offset_8G_8_bit = Xout_8_bit * 32 * (-1);   

Y_offset_8G_8_bit = Yout_8_bit * 32 * (-1);   

Z_offset_8G_8_bit = (Zout_8_bit - SENSITIVITY_8G_8bits) * 32 * (-1);

 

Best regards,

Tomas

Hello Tomas,

Thanks for all the help.

Regards,

Sérgio

%3CLINGO-SUB%20id%3D%22lingo-sub-1126869%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3EMMA8652FC%20-%20%E3%83%99%E3%82%A2%E3%83%A1%E3%82%BF%E3%83%AB%E3%82%B5%E3%83%B3%E3%83%97%E3%83%AB%E3%83%97%E3%83%AD%E3%82%B8%E3%82%A7%E3%82%AF%E3%83%88%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1126869%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%E3%81%AD%E3%81%88%E7%9A%86%E3%81%95%E3%82%93%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3E%E3%81%93%E3%81%93%E3%81%A7%E3%81%AF%E3%80%81%E3%83%95%E3%83%AA%E3%83%BC%E3%82%B9%E3%82%B1%E3%83%BC%E3%83%AB%E3%81%AE%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fdevelopment-boards%2Ffreedom-development-boards%2Fmcu-boards%2Ffreedom-development-platform-for-kinetis-kl14-kl15-kl24-kl25-mcus%3AFRDM-KL25Z%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3E%20FRDM-KL25Z%E9%96%8B%E7%99%BA%E3%83%97%E3%83%A9%E3%83%83%E3%83%88%E3%83%95%E3%82%A9%E3%83%BC%E3%83%A0%3C%2FA%3E%20%E3%81%A8%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fdevelopment-boards%2Ffreedom-development-boards%2Fsensors%2Ffreedom-development-platform-for-nxp-sensors-with-bluetooth-%3AFRDM-FXS-MULT2-B%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3E%20FRDM-FXS-MULTI(-B)%E3%82%BB%E3%83%B3%E3%82%B5%E6%8B%A1%E5%BC%B5%E3%83%9C%E3%83%BC%E3%83%89%3C%2FA%3E%20%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%A6%E4%BD%9C%E6%88%90%E3%81%97%E3%81%9F%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fproducts%2Fsensors%2Fmotion-sensors%2F3-axis%2F2g-4g-8g-low-g-12-bit-digital-accelerometer%3AMMA8652FC%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3E%20Xtrinsic%3C%2FA%3E%20MMA8652FC%E3%83%87%E3%82%B8%E3%82%BF%E3%83%AB%E5%8A%A0%E9%80%9F%E5%BA%A6%E8%A8%88%20%E3%81%AE%E7%B0%A1%E5%8D%98%E3%81%AA%E3%83%99%E3%82%A2%E3%83%A1%E3%82%BF%E3%83%AB%E3%81%AE%E3%82%B5%E3%83%B3%E3%83%97%E3%83%AB%E3%82%B3%E3%83%BC%E3%83%89%2F%E3%83%87%E3%83%A2%E3%82%92%E3%82%82%E3%81%861%E3%81%A4%E7%B4%B9%E4%BB%8B%E3%81%97%E3%81%9F%E3%81%84%E3%81%A8%E6%80%9D%E3%81%84%E3%81%BE%E3%81%99%E3%80%82I%3CSUP%3E2%3C%2FSUP%3EC%E3%82%A4%E3%83%B3%E3%82%BF%E3%83%BC%E3%83%95%E3%82%A7%E3%83%BC%E3%82%B9%E3%82%92%E4%BB%8B%E3%81%97%E3%81%9F%E5%89%B2%E3%82%8A%E8%BE%BC%E3%81%BF%E6%89%8B%E6%B3%95%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%A6MMA8652FC%E3%81%8B%E3%82%89%E8%AA%AD%E3%81%BF%E5%8F%96%E3%82%89%E3%82%8C%E3%82%8B%E5%8A%A0%E9%80%9F%E5%BA%A6%E3%83%87%E3%83%BC%E3%82%BF%E3%82%92%E8%A6%96%E8%A6%9A%E5%8C%96%E3%81%99%E3%82%8B%E3%81%9F%E3%82%81%E3%81%AB%E3%80%81%20%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fsoftware%2Fdevelopment-software%2Ffreemaster-run-time-debugging-tool%3AFREEMASTER%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EFreeMASTER%E3%83%84%E3%83%BC%E3%83%AB%3C%2FA%3E%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%BE%E3%81%97%E3%81%9F%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3E%E3%81%93%E3%81%AE%E3%82%B5%E3%83%B3%E3%83%97%E3%83%AB%E3%81%A7%E3%81%AF%E3%80%81%E6%AC%A1%E3%81%AE%E3%81%93%E3%81%A8%E3%82%92%E7%A4%BA%E3%81%97%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%0A%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2010pt%3B%20line-height%3A%201.5em%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2010pt%3B%20line-height%3A%201.5em%3B%22%3E1.%20MKL25Z128%20MCU(%E4%B8%BB%E3%81%ABI%3C%2FSPAN%3E%3CSPAN%20style%3D%22line-height%3A%201.5em%3B%22%3E%3CSUP%3E%E3%80%812%3C%2FSUP%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010pt%3B%20line-height%3A%201.5em%3B%22%3E%E3%80%81C%E3%80%81PORT%E3%83%A2%E3%82%B8%E3%83%A5%E3%83%BC%E3%83%AB%3C%2FSPAN%3E)%E3%81%AE%E5%88%9D%E6%9C%9F%E5%8C%96%3C%2FP%3E%0A%3CP%3E2.%20I%3CSUP%3E2%3C%2FSUP%3EC%E3%83%87%E3%83%BC%E3%82%BF%E3%81%AE%E6%9B%B8%E3%81%8D%E8%BE%BC%E3%81%BF%E3%81%8A%E3%82%88%E3%81%B3%E8%AA%AD%E3%81%BF%E5%8F%96%E3%82%8A%E6%93%8D%E4%BD%9C%E3%80%82%3C%2FP%3E%0A%3CP%3E3.%E6%9C%80%E9%AB%98%E3%81%AE%E8%A7%A3%E5%83%8F%E5%BA%A6%E3%82%92%E9%81%94%E6%88%90%E3%81%99%E3%82%8B%E3%81%9F%E3%82%81%E3%81%AE%E5%8A%A0%E9%80%9F%E5%BA%A6%E8%A8%88%E3%81%AE%E5%88%9D%E6%9C%9F%E5%8C%96%E3%80%82%3C%2FP%3E%0A%3CP%3E4.%20%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note%2FAN4069.pdf%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EAN4069%3C%2FA%3E%E3%81%AB%E5%9F%BA%E3%81%A5%E3%81%8F%E7%B0%A1%E5%8D%98%E3%81%AA%E3%82%AA%E3%83%95%E3%82%BB%E3%83%83%E3%83%88%E3%82%AD%E3%83%A3%E3%83%AA%E3%83%96%E3%83%AC%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%80%82%3C%2FP%3E%0A%3CP%3E5.%20%E5%89%B2%E3%82%8A%E8%BE%BC%E3%81%BF%E6%8A%80%E8%A1%93%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%A6%E3%83%87%E3%83%BC%E3%82%BF%E3%82%92%E8%AA%AD%E3%81%BF%E5%87%BA%E3%81%97%E3%81%A6%E5%87%BA%E5%8A%9B%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%0A%3CP%3E6.%20%E3%83%AC%E3%82%B8%E3%82%B9%E3%82%BF0x01%20%E2%80%93%200x06%E3%81%8B%E3%82%89%E3%81%AE%E5%87%BA%E5%8A%9B%E5%80%A4%E3%82%92g%E5%8D%98%E4%BD%8D%E3%81%AE%E5%AE%9F%E9%9A%9B%E3%81%AE%E5%8A%A0%E9%80%9F%E5%BA%A6%E5%80%A4%E3%81%AB%E5%A4%89%E6%8F%9B%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%0A%3CP%3E7.%20%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fsoftware%2Fdevelopment-software%2Ffreemaster-run-time-debugging-tool%3AFREEMASTER%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EFreeMASTER%E3%83%84%E3%83%BC%E3%83%AB%3C%2FA%3E%E3%81%A7%E3%81%AE%E5%87%BA%E5%8A%9B%E5%80%A4%E3%81%AE%E8%A6%96%E8%A6%9A%E5%8C%96%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3E1.FRDM-FXS-MULTI(-B)%2FFRDM-KL25Z%E3%81%AE%E5%9B%9E%E8%B7%AF%E5%9B%B3%E3%81%A8%E4%B8%8B%E3%81%AE%E7%94%BB%E5%83%8F%E3%81%A7%E3%82%8F%E3%81%8B%E3%82%8B%E3%82%88%E3%81%86%E3%81%AB%E3%80%81I2C%E4%BF%A1%E5%8F%B7%E3%81%AFKL25Z%20MCU%E3%81%AEI2C1%E3%83%A2%E3%82%B8%E3%83%A5%E3%83%BC%E3%83%AB(PTC1%E3%81%8A%E3%82%88%E3%81%B3PTC2%E3%83%94%E3%83%B3)%E3%81%AB%E3%83%AB%E3%83%BC%E3%83%86%E3%82%A3%E3%83%B3%E3%82%B0%E3%81%95%E3%82%8C%E3%80%81INT1%E5%87%BA%E5%8A%9B%E3%81%AFPTA5%E3%83%94%E3%83%B3%E3%81%AB%E6%8E%A5%E7%B6%9A%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99(%E3%82%BB%E3%83%B3%E3%82%B5%E3%83%BC%E6%8B%A1%E5%BC%B5%E3%83%9C%E3%83%BC%E3%83%89%E3%81%AEJ4%E3%81%AE%E3%83%94%E3%83%B3%233%E3%81%A8J6%E3%82%B3%E3%83%8D%E3%82%AF%E3%82%BF%E3%81%AE%E3%83%94%E3%83%B3%232%E3%81%8C%E4%B8%80%E7%B7%92%E3%81%AB%E6%8E%A5%E7%B6%9A%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%82%8B%E3%81%93%E3%81%A8%E3%82%92%E7%A2%BA%E8%AA%8D%E3%81%97%E3%81%A6%E3%81%8F%E3%81%A0%E3%81%95%E3%81%84)%E3%80%82MMA8652FC%E3%81%AEINT1%E5%87%BA%E5%8A%9B%E3%81%AF%E3%83%97%E3%83%83%E3%82%B7%E3%83%A5%E3%83%97%E3%83%AB%E3%82%A2%E3%82%AF%E3%83%86%E3%82%A3%E3%83%96LOW%E5%87%BA%E5%8A%9B%E3%81%A8%E3%81%97%E3%81%A6%E6%A7%8B%E6%88%90%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%82%8B%E3%81%9F%E3%82%81%E3%80%81%E5%AF%BE%E5%BF%9C%E3%81%99%E3%82%8BPTA5%E3%83%94%E3%83%B3%E6%A7%8B%E6%88%90%E3%81%AF%E3%80%81%E7%AB%8B%E3%81%A1%E4%B8%8B%E3%81%8C%E3%82%8A%E3%82%A8%E3%83%83%E3%82%B8%E3%81%AB%E5%89%B2%E3%82%8A%E8%BE%BC%E3%81%BF%E3%81%8C%E3%81%82%E3%82%8BGPIO%E3%81%A7%E3%81%99%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%2212383_12383.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%2212383_12383.jpg%22%20style%3D%22width%3A%20810px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F117659i98FD4BED6903F4DA%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%2212383_12383.jpg%22%20alt%3D%2212383_12383.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E12383_12383.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3E%E3%81%97%E3%81%9F%E3%81%8C%E3%81%A3%E3%81%A6%E3%80%81MCU%E3%81%AF%E6%AC%A1%E3%81%AE%E3%82%88%E3%81%86%E3%81%AB%E6%A7%8B%E6%88%90%E3%81%95%E3%82%8C%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Evoid%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%3CSTRONG%3EMCU_Init%3C%2FSTRONG%3E(%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Evoid%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%2F%2FI2C1%20module%20initialization%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20SIM_SCGC4%20%7C%3D%20SIM_SCGC4_I2C1_MASK%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20I2C1%E3%83%A2%E3%82%B8%E3%83%A5%E3%83%BC%E3%83%AB%E3%81%AB%E3%82%AF%E3%83%AD%E3%83%83%E3%82%AF%E3%82%92%E3%82%AA%E3%83%B3%E3%81%AB%E3%81%97%E3%81%BE%E3%81%99%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20SIM_SCGC5%20%7C%3D%20SIM_SCGC5_PORTC_MASK%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20%E3%83%9D%E3%83%BC%E3%83%88C%E3%83%A2%E3%82%B8%E3%83%A5%E3%83%BC%E3%83%AB%E3%81%B8%E3%81%AE%E3%82%AF%E3%83%AD%E3%83%83%E3%82%AF%E3%82%92%E3%82%AA%E3%83%B3%E3%81%AB%E3%81%97%E3%81%BE%E3%81%99%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20PORTC_PCR1%20%7C%3D%20PORT_PCR_MUX(0x2)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20PTC1%E3%83%94%E3%83%B3%E3%81%AFI2C1%20SCL%E3%83%A9%E3%82%A4%E3%83%B3%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20PORTC_PCR2%20%7C%3D%20PORT_PCR_MUX(0x2)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20PTC2%E3%83%94%E3%83%B3%E3%81%AFI2C1%20SDA%E3%83%A9%E3%82%A4%E3%83%B3%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20I2C1_F%20%7C%3D%20I2C_F_ICR(0x14)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20SDA%E3%83%9B%E3%83%BC%E3%83%AB%E3%83%89%E3%82%BF%E3%82%A4%E3%83%A0%3D2.125us%E3%80%81SCL%E3%82%B9%E3%82%BF%E3%83%BC%E3%83%88%E3%83%9B%E3%83%BC%E3%83%AB%E3%83%89%E3%82%BF%E3%82%A4%E3%83%A0%3D4.25us%E3%80%81SCL%E3%82%B9%E3%83%88%E3%83%83%E3%83%97%E3%83%9B%E3%83%BC%E3%83%AB%E3%83%89%E3%82%BF%E3%82%A4%E3%83%A0%3D5.125us%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20I2C1_C1%20%7C%3D%20I2C_C1_IICEN_MASK%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20I2C1%E3%83%A2%E3%82%B8%E3%83%A5%E3%83%BC%E3%83%AB%E3%82%92%E6%9C%89%E5%8A%B9%E3%81%AB%E3%81%99%E3%82%8B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3EPTA5%E3%83%94%E3%83%B3(MMA8652FC%E3%81%AEINT1%E3%81%AB%E6%8E%A5%E7%B6%9A)%E3%82%92%E7%AB%8B%E3%81%A1%E4%B8%8B%E3%81%8C%E3%82%8A%E3%82%A8%E3%83%83%E3%82%B8%E5%89%B2%E3%82%8A%E8%BE%BC%E3%81%BF%E7%94%A8%E3%81%AB%E6%A7%8B%E6%88%90%E3%81%97%E3%81%BE%E3%81%99%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20SIM_SCGC5%20%7C%3D%20SIM_SCGC5_PORTA_MASK%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20%E3%83%9D%E3%83%BC%E3%83%88A%E3%83%A2%E3%82%B8%E3%83%A5%E3%83%BC%E3%83%AB%E3%81%B8%E3%81%AE%E3%82%AF%E3%83%AD%E3%83%83%E3%82%AF%E3%82%92%E3%82%AA%E3%83%B3%E3%81%AB%E3%81%97%E3%81%BE%E3%81%99%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20PORTA_PCR5%20%7C%3D%20(0%7CPORT_PCR_ISF_MASK%7C%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20%E5%89%B2%E3%82%8A%E8%BE%BC%E3%81%BF%E3%83%95%E3%83%A9%E3%82%B0%E3%82%92%E3%82%AF%E3%83%AA%E3%82%A2%E3%81%99%E3%82%8B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20PORT_PCR_MUX(0x1)%7C%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20PTA5%20%E3%81%AF%20GPIO%20%E3%81%A8%E3%81%97%E3%81%A6%E6%A7%8B%E6%88%90%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20PORT_PCR_IRQC(0xA))%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20PTA5%20%E3%81%AF%E7%AB%8B%E3%81%A1%E4%B8%8B%E3%81%8C%E3%82%8A%E3%82%A8%E3%83%83%E3%82%B8%E5%89%B2%E3%82%8A%E8%BE%BC%E3%81%BF%E7%94%A8%E3%81%AB%E6%A7%8B%E6%88%90%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3ENVIC%E3%81%A7%E3%81%AEPORTA%E5%89%B2%E3%82%8A%E8%BE%BC%E3%81%BF%E3%81%AE%E6%9C%89%E5%8A%B9%E5%8C%96%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20NVIC_ICPR%20%7C%3D%201%20%26lt%3B%26lt%3B%20((%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%230000c0%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CEM%3EINT_PORTA%3C%2FEM%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E-%2016)%2532)%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20NVIC_ISER%20%7C%3D%201%20%26lt%3B%26lt%3B%20((%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%230000c0%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CEM%3EINT_PORTA%3C%2FEM%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E-%2016)%2532)%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7D%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3E2.%20MMA8652FC%E3%81%AE7%E3%83%93%E3%83%83%E3%83%88%3CSUP%3EI2C%3C%2FSUP%3E%E3%82%A2%E3%83%89%E3%83%AC%E3%82%B9%E3%81%AF%E5%9B%BA%E5%AE%9A%E5%80%A40x1D%E3%81%A7%E3%81%99%E3%80%82%E4%B8%8A%E5%9B%B3%E3%81%AE%E3%82%88%E3%81%86%E3%81%AB%E3%80%81SCL%E3%83%A9%E3%82%A4%E3%83%B3%E3%81%AFPTC1%E3%83%94%E3%83%B3%E3%81%AB%E3%80%81SDA%E3%83%A9%E3%82%A4%E3%83%B3%E3%81%AFPTC2%E3%83%94%E3%83%B3%E3%81%AB%E6%8E%A5%E7%B6%9A%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82I2C%E3%82%AF%E3%83%AD%E3%83%83%E3%82%AF%E5%91%A8%E6%B3%A2%E6%95%B0%E3%81%AF125kHz%E3%81%A7%E3%81%99%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%E4%BB%A5%E4%B8%8B%E3%81%AE%E3%82%B9%E3%82%AF%E3%83%AA%E3%83%BC%E3%83%B3%E3%82%B7%E3%83%A7%E3%83%83%E3%83%88%E3%81%AF%E3%80%81%E5%80%A4%200x39%20%E3%82%92CTRL_REG1%20(0x2A)%20%E3%81%AB%E6%9B%B8%E3%81%8D%E8%BE%BC%E3%82%80%E6%9B%B8%E3%81%8D%E8%BE%BC%E3%81%BF%E6%93%8D%E4%BD%9C%E3%82%92%E7%A4%BA%E3%81%97%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%209.0pt%3B%20font-family%3A%20'Arial'%2C'sans-serif'%3B%20background%3A%20white%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%209.0pt%3B%20font-family%3A%20'Arial'%2C'sans-serif'%3B%20background%3A%20white%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%2212384_12384.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%2212384_12384.jpg%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F117660i0EEB2A640B959CC9%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%2212384_12384.jpg%22%20alt%3D%2212384_12384.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E12384_12384.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%209.0pt%3B%20font-family%3A%20'Arial'%2C'sans-serif'%3B%20background%3A%20white%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%E3%81%9D%E3%81%97%E3%81%A6%E3%80%81WHO_AM_I%E3%83%AC%E3%82%B8%E3%82%B9%E3%82%BF0x0D%E3%81%8B%E3%82%89%E8%AA%AD%E3%81%BF%E5%8F%96%E3%82%89%E3%82%8C%E3%81%9F1%E3%83%90%E3%82%A4%E3%83%88%E3%81%AF%E6%AC%A1%E3%81%AE%E3%81%A8%E3%81%8A%E3%82%8A%E3%81%A7%E3%81%99%E3%80%82%E3%81%94%E8%A6%A7%E3%81%AE%E3%81%A8%E3%81%8A%E3%82%8A%E3%80%81%E6%AD%A3%E3%81%97%E3%81%84%E5%80%A40x4A%E3%82%92%E8%BF%94%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%20margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%2212385_12385.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%2212385_12385.jpg%22%20style%3D%22width%3A%20985px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F117661iF1B19761AF5AE278%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%2212385_12385.jpg%22%20alt%3D%2212385_12385.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E12385_12385.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%20margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%E5%90%84MMA8652FC%E7%A2%BA%E8%AA%8D%E5%BF%9C%E7%AD%94(AK)%E3%81%8C%E5%8F%97%E4%BF%A1%E3%81%95%E3%82%8C%E3%81%9F%E5%BE%8C%E3%80%81KL25Z%E3%81%8B%E3%82%89%E3%83%8E%E3%83%BC%E7%A2%BA%E8%AA%8D%E5%BF%9C%E7%AD%94(NAK)%E3%81%8C%E7%99%BA%E7%94%9F%E3%81%97%E3%80%81%E3%81%9D%E3%81%AE%E5%BE%8C%E3%81%AB%E9%80%81%E4%BF%A1%E7%B5%82%E4%BA%86%E3%82%92%E9%80%9A%E7%9F%A5%E3%81%99%E3%82%8B%E5%81%9C%E6%AD%A2%E6%9D%A1%E4%BB%B6(SP)%E3%81%8C%E7%99%BA%E7%94%9F%E3%81%99%E3%82%8B%E3%81%BE%E3%81%A7%E3%80%81%E3%82%B7%E3%83%BC%E3%82%B1%E3%83%B3%E3%82%B7%E3%83%A3%E3%83%AB%E3%83%AC%E3%82%B8%E3%82%B9%E3%82%BF%E3%81%8B%E3%82%89%E8%A4%87%E6%95%B0%E3%83%90%E3%82%A4%E3%83%88%E3%81%AE%E3%83%87%E3%83%BC%E3%82%BF%E3%82%92%E8%AA%AD%E3%81%BF%E5%8F%96%E3%82%8B%E3%81%93%E3%81%A8%E3%81%8C%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82%E3%83%AC%E3%82%B8%E3%82%B9%E3%82%BF0x01%E3%81%8B%E3%82%890x06%E3%81%B8%E3%81%AE6%E3%83%90%E3%82%A4%E3%83%88%E3%81%AE%E3%83%90%E3%83%BC%E3%82%B9%E3%83%88%E8%AA%AD%E3%81%BF%E5%87%BA%E3%81%97%E3%82%92%E4%BB%A5%E4%B8%8B%E3%81%AB%E7%A4%BA%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%E3%81%BE%E3%81%9F%E3%80%81%E5%8A%A0%E9%80%9F%E5%BA%A6%E5%87%BA%E5%8A%9B%E3%83%87%E3%83%BC%E3%82%BF%E3%82%92%E8%AA%AD%E3%81%BF%E5%87%BA%E3%81%99%E3%81%93%E3%81%A8%E3%81%AB%E3%82%88%E3%81%A3%E3%81%A6INT1%E3%83%94%E3%83%B3%E3%81%8C%E8%87%AA%E5%8B%95%E7%9A%84%E3%81%AB%E3%83%87%E3%82%A2%E3%82%B5%E3%83%BC%E3%83%88%E3%81%95%E3%82%8C%E3%82%8B%E6%A7%98%E5%AD%90%E3%82%82%E7%A4%BA%E3%81%97%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%20margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%2212386_12386.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%2212386_12386.jpg%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F117662i43F527D64FE4AC04%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%2212386_12386.jpg%22%20alt%3D%2212386_12386.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E12386_12386.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%20margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3E3.%20%E5%88%9D%E6%9C%9F%E5%8C%96%E3%81%AE%E9%96%8B%E5%A7%8B%E6%99%82%E3%81%AB%E3%80%81CTRL_REG2%E3%83%AC%E3%82%B8%E3%82%B9%E3%82%BF%E3%81%AERST%E3%83%93%E3%83%83%E3%83%88%E3%82%92%E8%A8%AD%E5%AE%9A%E3%81%99%E3%82%8B%E3%81%93%E3%81%A8%E3%81%AB%E3%82%88%E3%82%8A%E3%80%81%E3%81%99%E3%81%B9%E3%81%A6%E3%81%AE%E3%83%AC%E3%82%B8%E3%82%B9%E3%82%BF%E3%81%8C%E3%83%87%E3%83%95%E3%82%A9%E3%83%AB%E3%83%88%E5%80%A4%E3%81%AB%E3%83%AA%E3%82%BB%E3%83%83%E3%83%88%E3%81%95%E3%82%8C%E3%81%BE%E3%81%99%E3%80%82%E3%83%80%E3%82%A4%E3%83%8A%E3%83%9F%E3%83%83%E3%82%AF%E3%83%AC%E3%83%B3%E3%82%B8%E3%81%AF%C2%B12g%E3%81%AB%E8%A8%AD%E5%AE%9A%E3%81%95%E3%82%8C%E3%80%81%E6%9C%80%E9%AB%98%E3%81%AE%E5%88%86%E8%A7%A3%E8%83%BD%E3%82%92%E5%AE%9F%E7%8F%BE%E3%81%99%E3%82%8B%E3%81%9F%E3%82%81%E3%81%AB%E3%80%81%E6%9C%80%E4%BD%8E%E3%81%AEODR(1.56Hz)%E3%81%A8%E9%AB%98%E8%A7%A3%E5%83%8F%E5%BA%A6%E3%83%A2%E3%83%BC%E3%83%89%E3%81%8C%E9%81%B8%E6%8A%9E%E3%81%95%E3%82%8C%E3%81%BE%E3%81%99(%E8%A9%B3%E7%B4%B0%E3%81%AF%20%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note%2FAN4075.pdf%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EAN4075%3C%2FA%3E%E3%82%92%E5%8F%82%E7%85%A7)%E3%80%82DRDY%E5%89%B2%E3%82%8A%E8%BE%BC%E3%81%BF%E3%81%AF%E3%82%A4%E3%83%8D%E3%83%BC%E3%83%96%E3%83%AB%E3%81%95%E3%82%8C%E3%80%81%E3%83%97%E3%83%83%E3%82%B7%E3%83%A5%E3%83%97%E3%83%AB%E3%81%AE%E3%82%A2%E3%82%AF%E3%83%86%E3%82%A3%E3%83%96%E3%83%AD%E3%83%BC%E5%87%BA%E5%8A%9B%E3%81%AB%E8%A8%AD%E5%AE%9A%E3%81%95%E3%82%8C%E3%81%9FINT1%E5%89%B2%E3%82%8A%E8%BE%BC%E3%81%BF%E3%83%94%E3%83%B3%E3%81%AB%E9%80%81%E3%82%89%E3%82%8C%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Evoid%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%3CSTRONG%3EMMA8652FC_Init%3C%2FSTRONG%3E%20(%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Evoid%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20I2C_WriteRegister(MMA8652FC_I2C_ADDRESS%E3%80%81CTRL_REG2%E3%80%810x40)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20%E3%81%99%E3%81%B9%E3%81%A6%E3%81%AE%E3%83%AC%E3%82%B8%E3%82%B9%E3%82%BF%E3%82%92POR%E5%80%A4%E3%81%AB%E3%83%AA%E3%82%BB%E3%83%83%E3%83%88%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20%E4%B8%80%E6%99%82%E5%81%9C%E6%AD%A2(0x631)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20~1ms%E3%81%AE%E9%81%85%E5%BB%B6%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20I2C_WriteRegister(MMA8652FC_I2C_ADDRESS%E3%80%81XYZ_DATA_CFG_REG%E3%80%810x00)%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20%2B%2F-2g%E3%83%AC%E3%83%B3%E3%82%B8%E3%80%81~0.977mg%2FLSB%20%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20I2C_WriteRegister(MMA8652FC_I2C_ADDRESS%E3%80%81CTRL_REG2%E3%80%810x02)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20%E9%AB%98%E8%A7%A3%E5%83%8F%E5%BA%A6%E3%83%A2%E3%83%BC%E3%83%89%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20I2C_WriteRegister(MMA8652FC_I2C_ADDRESS%E3%80%81CTRL_REG3%E3%80%810x00)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20%E3%83%97%E3%83%83%E3%82%B7%E3%83%A5%E3%83%97%E3%83%AB%E3%80%81%E3%82%A2%E3%82%AF%E3%83%86%E3%82%A3%E3%83%96%20LOW%20%E5%89%B2%E3%82%8A%E8%BE%BC%E3%81%BF%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20I2C_WriteRegister(MMA8652FC_I2C_ADDRESS%E3%80%81CTRL_REG4%E3%80%810x01)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20DRDY%E5%89%B2%E3%82%8A%E8%BE%BC%E3%81%BF%E3%82%92%E3%82%A4%E3%83%8D%E3%83%BC%E3%83%96%E3%83%AB%E3%81%AB%E3%81%99%E3%82%8B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20I2C_WriteRegister(MMA8652FC_I2C_ADDRESS%E3%80%81CTRL_REG5%E3%80%810x01)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20INT1%20-%20PTA5%20%E3%81%AB%E3%83%AB%E3%83%BC%E3%83%86%E3%82%A3%E3%83%B3%E3%82%B0%E3%81%95%E3%82%8C%E3%81%9F%20DRDY%20%E5%89%B2%E3%82%8A%E8%BE%BC%E3%81%BF%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20I2C_WriteRegister(MMA8652FC_I2C_ADDRESS%E3%80%81CTRL_REG1%E3%80%810x39)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20ODR%3D1.56Hz%E3%80%81%E3%82%A2%E3%82%AF%E3%83%86%E3%82%A3%E3%83%96%E3%83%BB%E3%83%A2%E3%83%BC%E3%83%89%20%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7D%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E4.%20%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note%2FAN4069.pdf%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EAN4069%3C%2FA%3E%E3%81%AB%E6%BA%96%E6%8B%A0%E3%81%97%E3%81%9F%E3%82%B7%E3%83%B3%E3%83%97%E3%83%AB%E3%81%AA%E3%82%AA%E3%83%95%E3%82%BB%E3%83%83%E3%83%88%E3%82%AD%E3%83%A3%E3%83%AA%E3%83%96%E3%83%AC%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E6%96%B9%E6%B3%95%E3%81%8C%E5%AE%9F%E8%A3%85%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%20margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%E3%83%9C%E3%82%A4%E3%83%89%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%3CSTRONG%3EMMA8652FC_Calibration%3C%2FSTRONG%3E(%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%E3%83%9C%E3%82%A4%E3%83%89%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%20%E3%83%81%E3%83%A3%E3%83%BC%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EX_offset%E3%80%81Y_offset%E3%80%81Z_offset%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E3%83%87%E3%83%BC%E3%82%BF%E3%83%AC%E3%83%87%E3%82%A3%20%3D%200%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%E4%B8%80%E6%96%B9%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E(!DataReady)%7B%7D%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20%2F%2F%20%E6%9C%80%E5%88%9D%E3%81%AE%E3%83%87%E3%83%BC%E3%82%BF%E3%82%BB%E3%83%83%E3%83%88%E3%81%AF%E6%BA%96%E5%82%99%E3%81%8C%E3%81%A7%E3%81%8D%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%81%8B%3F%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E3%83%87%E3%83%BC%E3%82%BF%E3%83%AC%E3%83%87%E3%82%A3%20%3D%200%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20I2C_WriteRegister(MMA8652FC_I2C_ADDRESS%E3%80%81CTRL_REG1%E3%80%810x00)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20%E3%82%B9%E3%82%BF%E3%83%B3%E3%83%90%E3%82%A4%E3%83%A2%E3%83%BC%E3%83%89%20%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20I2C_ReadMultiRegisters(MMA8652FC_I2C_ADDRESS%2C%20OUT_X_MSB_REG%2C%206%2C%20AccelData)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20%E3%83%87%E3%83%BC%E3%82%BF%E5%87%BA%E5%8A%9B%E3%83%AC%E3%82%B8%E3%82%B9%E3%82%BF%E3%81%AE%E8%AA%AD%E5%87%BA%E3%81%97%200x01-0x06%20%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20Xout_12_bit%20%3D%20((%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%E3%82%B7%E3%83%A7%E3%83%BC%E3%83%88%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%20(AccelData%5B0%5D%26lt%3B%26lt%3B8%20%7CAccelData%5B1%5D))%20%26gt%3B%26gt%3B%204%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2012%E3%83%93%E3%83%83%E3%83%88X%E8%BB%B8%E5%8A%A0%E9%80%9F%E5%BA%A6%E5%87%BA%E5%8A%9B%E5%80%A4%E3%82%92%E8%A8%88%E7%AE%97%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20Yout_12_bit%20%3D%20((%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%E3%82%B7%E3%83%A7%E3%83%BC%E3%83%88%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%20(AccelData%5B2%5D%26lt%3B%26lt%3B8%20%7CAccelData%5B3%5D))%20%26gt%3B%26gt%3B%204%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2012%E3%83%93%E3%83%83%E3%83%88Y%E8%BB%B8%E5%8A%A0%E9%80%9F%E5%BA%A6%E5%87%BA%E5%8A%9B%E5%80%A4%E3%82%92%E8%A8%88%E7%AE%97%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20Zout_12_bit%20%3D%20((%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%E3%82%B7%E3%83%A7%E3%83%BC%E3%83%88%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%20(AccelData%5B4%5D%26lt%3B%26lt%3B8%20%7CAccelData%5B5%5D))%20%26gt%3B%26gt%3B%204%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2012%E3%83%93%E3%83%83%E3%83%88Z%E8%BB%B8%E5%8A%A0%E9%80%9F%E5%BA%A6%E5%87%BA%E5%8A%9B%E5%80%A4%E3%82%92%E8%A8%88%E7%AE%97%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20X_offset%20%3D%20Xout_12_bit%20%2F%202%20*(-1)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20X%E8%BB%B8%E3%82%AA%E3%83%95%E3%82%BB%E3%83%83%E3%83%88%E8%A3%9C%E6%AD%A3%E5%80%A4%E3%82%92%E8%A8%88%E7%AE%97%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20Y_offset%20%3D%20Yout_12_bit%20%2F%202%20*%20(-1)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20Y%20%E8%BB%B8%E3%82%AA%E3%83%95%E3%82%BB%E3%83%83%E3%83%88%E8%A3%9C%E6%AD%A3%E5%80%A4%E3%81%AE%E8%A8%88%E7%AE%97%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20Z_offset%20%3D%20(Zout_12_bit%20-%20SENSITIVITY_2G)%20%2F%202%20*%20(-1)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20Z%20%E8%BB%B8%E3%82%AA%E3%83%95%E3%82%BB%E3%83%83%E3%83%88%E8%A3%9C%E6%AD%A3%E5%80%A4%E3%81%AE%E8%A8%88%E7%AE%97%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EI2C_WriteRegister(MMA8652FC_I2C_ADDRESS%E3%80%81OFF_X_REG%E3%80%81X_offset)%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EI2C_WriteRegister(MMA8652FC_I2C_ADDRESS%E3%80%81OFF_Y_REG%E3%80%81Y_offset)%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EI2C_WriteRegister(MMA8652FC_I2C_ADDRESS%E3%80%81OFF_Z_REG%E3%80%81Z_offset)%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20I2C_WriteRegister(MMA8652FC_I2C_ADDRESS%E3%80%81CTRL_REG1%E3%80%810x39)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20%E5%86%8D%E3%81%B3%E3%82%A2%E3%82%AF%E3%83%86%E3%82%A3%E3%83%96%E3%83%A2%E3%83%BC%E3%83%89%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7D%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E5.%20ISR%20%E3%81%A7%E3%81%AF%E3%80%81%E5%89%B2%E3%82%8A%E8%BE%BC%E3%81%BF%E3%83%95%E3%83%A9%E3%82%B0%E3%81%AE%E3%81%BF%E3%81%8C%E3%82%AF%E3%83%AA%E3%82%A2%E3%81%95%E3%82%8C%E3%80%81%E6%96%B0%E3%81%97%E3%81%84%E3%83%87%E3%83%BC%E3%82%BF%E3%81%AE%E5%88%B0%E7%9D%80%E3%82%92%E7%A4%BA%E3%81%99%E3%81%9F%E3%82%81%E3%81%AB%20DataReady%20%E5%A4%89%E6%95%B0%E3%81%8C%E8%A8%AD%E5%AE%9A%E3%81%95%E3%82%8C%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3CSPAN%20style%3D%22font-weight%3A%20inherit%3B%20font-style%3A%20inherit%3B%20font-size%3A%2010pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010pt%3B%20font-style%3A%20inherit%3B%20font-family%3A%20inherit%3B%20font-weight%3A%20inherit%3B%22%3E%3CSTRONG%3E%E3%83%9C%E3%82%A4%E3%83%89%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-weight%3A%20inherit%3B%20font-style%3A%20inherit%3B%20font-size%3A%2010pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%3CSPAN%20style%3D%22font-style%3A%20inherit%3B%20font-family%3A%20inherit%3B%20font-weight%3A%20inherit%3B%22%3E%3CSTRONG%3EPORTA_IRQHandler%3C%2FSTRONG%3E%3C%2FSPAN%3E()%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3CSPAN%20style%3D%22font-weight%3A%20inherit%3B%20font-style%3A%20inherit%3B%20font-size%3A%2010pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3CSPAN%20style%3D%22font-weight%3A%20inherit%3B%20font-style%3A%20inherit%3B%20font-size%3A%2010pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20PORTA_PCR5%20%7C%3D%20PORT_PCR_ISF_MASK%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-weight%3A%20inherit%3B%20font-style%3A%20inherit%3B%20font-size%3A%2010pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20%E5%89%B2%E3%82%8A%E8%BE%BC%E3%81%BF%E3%83%95%E3%83%A9%E3%82%B0%E3%82%92%E3%82%AF%E3%83%AA%E3%82%A2%E3%81%99%E3%82%8B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3CSPAN%20style%3D%22font-weight%3A%20inherit%3B%20font-style%3A%20inherit%3B%20font-size%3A%2010pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E3%83%87%E3%83%BC%E3%82%BF%E3%83%AC%E3%83%87%E3%82%A3%20%3D%201%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3CSPAN%20style%3D%22font-weight%3A%20inherit%3B%20font-style%3A%20inherit%3B%20font-size%3A%2010pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7D%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%20margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E6.%E5%8A%A0%E9%80%9F%E5%BA%A6%E8%A8%88%E3%83%AC%E3%82%B8%E3%82%B9%E3%82%BF0x01%200x06%E3%81%8B%E3%82%89%E3%81%AE%E5%87%BA%E5%8A%9B%E5%80%A4%E3%81%AF%E3%80%81%E6%9C%80%E5%88%9D%E3%81%AB%E7%AC%A6%E5%8F%B7%E4%BB%98%E3%81%8D12%E3%83%93%E3%83%83%E3%83%88%E5%80%A4%E3%81%AB%E5%A4%89%E6%8F%9B%E3%81%95%E3%82%8C%E3%80%81%E3%81%9D%E3%81%AE%E5%BE%8C%E3%80%81g%E5%8D%98%E4%BD%8D%E3%81%AE%E5%AE%9F%E9%9A%9B%E3%81%AE%E5%80%A4%E3%81%AB%E5%A4%89%E6%8F%9B%E3%81%95%E3%82%8C%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%20margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Eif%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E(DataReady)%20%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20%E6%96%B0%E3%81%97%E3%81%84%E3%83%87%E3%83%BC%E3%82%BF%E3%82%BB%E3%83%83%E3%83%88%E3%81%AF%E6%BA%96%E5%82%99%E3%81%8C%E3%81%A7%E3%81%8D%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%81%8B%3F%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E3%83%87%E3%83%BC%E3%82%BF%E3%83%AC%E3%83%87%E3%82%A3%20%3D%200%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20I2C_ReadMultiRegisters(MMA8652FC_I2C_ADDRESS%2C%20OUT_X_MSB_REG%2C%206%2C%20AccelData)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20%E3%83%87%E3%83%BC%E3%82%BF%E5%87%BA%E5%8A%9B%E3%83%AC%E3%82%B8%E3%82%B9%E3%82%BF%E3%81%AE%E8%AA%AD%E5%87%BA%E3%81%97%200x01-0x06%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%2012-bit%20accelerometer%20data%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20Xout_12_bit%20%3D%20((%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%E3%82%B7%E3%83%A7%E3%83%BC%E3%83%88%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%20(AccelData%5B0%5D%26lt%3B%26lt%3B8%20%7CAccelData%5B1%5D))%20%26gt%3B%26gt%3B%204%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2012%E3%83%93%E3%83%83%E3%83%88X%E8%BB%B8%E5%8A%A0%E9%80%9F%E5%BA%A6%E5%87%BA%E5%8A%9B%E5%80%A4%E3%82%92%E8%A8%88%E7%AE%97%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20Yout_12_bit%20%3D%20((%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%E3%82%B7%E3%83%A7%E3%83%BC%E3%83%88%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%20(AccelData%5B2%5D%26lt%3B%26lt%3B8%20%7CAccelData%5B3%5D))%20%26gt%3B%26gt%3B%204%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2012%E3%83%93%E3%83%83%E3%83%88Y%E8%BB%B8%E5%8A%A0%E9%80%9F%E5%BA%A6%E5%87%BA%E5%8A%9B%E5%80%A4%E3%82%92%E8%A8%88%E7%AE%97%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20Zout_12_bit%20%3D%20((%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%E3%82%B7%E3%83%A7%E3%83%BC%E3%83%88%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%20(AccelData%5B4%5D%26lt%3B%26lt%3B8%20%7CAccelData%5B5%5D))%20%26gt%3B%26gt%3B%204%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2012%E3%83%93%E3%83%83%E3%83%88Z%E8%BB%B8%E5%8A%A0%E9%80%9F%E5%BA%A6%E5%87%BA%E5%8A%9B%E5%80%A4%E3%82%92%E8%A8%88%E7%AE%97%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%E5%8A%A0%E9%80%9F%E5%BA%A6%E8%A8%88%E3%81%AE%E3%83%87%E3%83%BC%E3%82%BF%E3%82%92%20g%20%E3%81%AB%E5%A4%89%E6%8F%9B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20Xout_g%20%3D%20((%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Efloat%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%20Xout_12_bit)%20%2F%20SENSITIVITY_2G%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20X%20%E8%BB%B8%E3%81%AE%E5%87%BA%E5%8A%9B%E5%80%A4%E3%82%92%20g%20%E3%81%A7%E8%A8%88%E7%AE%97%E3%81%97%E3%81%BE%E3%81%99%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20Yout_g%20%3D%20((%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Efloat%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%20Yout_12_bit)%20%2F%20SENSITIVITY_2G%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20Y%20%E8%BB%B8%E3%81%AE%E5%87%BA%E5%8A%9B%E5%80%A4%E3%82%92%20g%20%E3%81%A7%E8%A8%88%E7%AE%97%E3%81%97%E3%81%BE%E3%81%99%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20Zout_g%20%3D%20((%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%E6%B5%AE%E5%8B%95%E5%B0%8F%E6%95%B0%E7%82%B9%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E6%95%B0)%20Zout_12_bit)%20%2F%20SENSITIVITY_2G%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20Z%20%E8%BB%B8%E3%81%AE%E5%87%BA%E5%8A%9B%E5%80%A4%E3%82%92%20g%20%E3%81%A7%E8%A8%88%E7%AE%97%E3%81%97%E3%81%BE%E3%81%99%20%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20black%3B%20font-family%3A%20Consolas%3B%20font-size%3A%2010pt%3B%20line-height%3A%201.5em%3B%22%3E%7D%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20black%3B%20font-family%3A%20Consolas%3B%20font-size%3A%2010pt%3B%20line-height%3A%201.5em%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3E7.%20%E8%A8%88%E7%AE%97%E3%81%95%E3%82%8C%E3%81%9F%E5%80%A4%E3%81%AF%E3%80%81Debug%E3%83%91%E3%83%BC%E3%82%B9%E3%83%9A%E3%82%AF%E3%83%86%E3%82%A3%E3%83%96%E3%81%AE%E5%8F%B3%E4%B8%8A%E3%81%AB%E3%81%82%E3%82%8B%E3%80%8CVariables%E3%80%8D%E3%82%A6%E3%82%A3%E3%83%B3%E3%83%89%E3%82%A6%E3%81%BE%E3%81%9F%E3%81%AFFreeMASTER%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%A7%E7%A2%BA%E8%AA%8D%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82FreeMASTER%E3%83%97%E3%83%AD%E3%82%B8%E3%82%A7%E3%82%AF%E3%83%88%E3%82%92%E9%96%8B%E3%81%84%E3%81%A6%E5%AE%9F%E8%A1%8C%E3%81%99%E3%82%8B%E3%81%AB%E3%81%AF%E3%80%81%20%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fsoftware%2Fdevelopment-software%2Ffreemaster-run-time-debugging-tool%3AFREEMASTER%22%20target%3D%22_blank%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3EFreeMASTER%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%3C%2FA%3E%E3%81%A8%20%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fwebapp%2Fsps%2Fdownload%2Flicense.jsp%3FcolCode%3DFMASTERSCIDRV%22%20target%3D%22_blank%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3EFreeMASTER%E9%80%9A%E4%BF%A1%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%83%BC%3C%2FA%3E%E3%82%92%E3%82%A4%E3%83%B3%E3%82%B9%E3%83%88%E3%83%BC%E3%83%AB%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22line-height%3A%201.5em%3B%20color%3A%20%233d3d3d%3B%20font-size%3A%2010pt%3B%20font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22line-height%3A%201.5em%3B%20color%3A%20%233d3d3d%3B%20font-size%3A%2010pt%3B%20font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%2212387_12387.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%2212387_12387.jpg%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F117663i406293ABF1946E2D%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%2212387_12387.jpg%22%20alt%3D%2212387_12387.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E12387_12387.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3CBR%20%2F%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%2212388_12388.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%2212388_12388.jpg%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F117664iADBF69B1F6440CC8%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%2212388_12388.jpg%22%20alt%3D%2212388_12388.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E12388_12388.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3EFreeMASTER%E3%83%97%E3%83%AD%E3%82%B8%E3%82%A7%E3%82%AF%E3%83%88%E3%82%92%E5%90%AB%E3%82%80MCU(Eclipse%20IDE)%20%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fsoftware%2Fdevelopment-software%2Fcodewarrior-development-tools%2Fcodewarrior-legacy%2Fcodewarrior-for-mcus-eclipse-ide-coldfire-56800-e-dsc-qorivva-56xx-rs08-s08-s12z-11-1%3ACW-MCU10%22%20target%3D%22_blank%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3E%E3%81%AECW%3C%2FA%3E%E3%81%A7%E6%9B%B8%E3%81%8B%E3%82%8C%E3%81%9F%E5%AE%8C%E5%85%A8%E3%81%AA%E3%82%BD%E3%83%BC%E3%82%B9%E3%82%B3%E3%83%BC%E3%83%89%E3%81%8C%E6%B7%BB%E4%BB%98%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3E%E3%81%93%E3%81%AE%E7%B0%A1%E5%8D%98%E3%81%AA%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%AB%E9%96%A2%E3%81%97%E3%81%A6%E3%81%94%E8%B3%AA%E5%95%8F%E3%81%8C%E3%81%82%E3%82%8B%E5%A0%B4%E5%90%88%E3%81%AF%E3%80%81%E3%81%A9%E3%81%86%E3%81%9E%E3%81%8A%E6%B0%97%E8%BB%BD%E3%81%AB%E4%B8%8B%E8%A8%98%E3%81%AB%E3%81%94%E8%B3%AA%E5%95%8F%E3%81%8F%E3%81%A0%E3%81%95%E3%81%84%E3%80%82%E3%81%94%E6%84%8F%E8%A6%8B%E3%82%84%E3%81%94%E6%8F%90%E6%A1%88%E3%82%82%E5%A4%A7%E6%AD%93%E8%BF%8E%E3%81%A7%E3%81%99%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3E%E3%82%88%E3%82%8D%E3%81%97%E3%81%8F%E3%81%8A%E9%A1%98%E3%81%84%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%0A%3CP%3ETomas%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-LABS%20id%3D%22lingo-labs-1126869%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CLINGO-LABEL%3E%E5%8A%A0%E9%80%9F%E5%BA%A6%E3%82%BB%E3%83%B3%E3%82%B5%3C%2FLINGO-LABEL%3E%3C%2FLINGO-LABS%3E%3CLINGO-SUB%20id%3D%22lingo-sub-1126872%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3AMMA8652FC%20-%20%E3%83%99%E3%82%A2%E3%83%A1%E3%82%BF%E3%83%AB%E3%82%B5%E3%83%B3%E3%83%97%E3%83%AB%E3%83%97%E3%83%AD%E3%82%B8%E3%82%A7%E3%82%AF%E3%83%88%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1126872%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%26lt%3Bmeta%20http-equiv%3D%22Content-Type%22%20content%3D%22text%2Fhtml%3B%20charset%3Dutf-8%22%20%2F%26gt%3B%0A%3CP%3EHello%20Tomas%2C%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E3%81%99%E3%81%B9%E3%81%A6%E3%81%AE%E5%8A%A9%E3%81%91%E3%81%AB%E6%84%9F%E8%AC%9D%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E3%82%88%E3%82%8D%E3%81%97%E3%81%8F%E3%81%8A%E9%A1%98%E3%81%84%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3ES%C3%A9rgio%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-1126871%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3AMMA8652FC%20-%20%E3%83%99%E3%82%A2%E3%83%A1%E3%82%BF%E3%83%AB%E3%82%B5%E3%83%B3%E3%83%97%E3%83%AB%E3%83%97%E3%83%AD%E3%82%B8%E3%82%A7%E3%82%AF%E3%83%88%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1126871%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%26lt%3Bmeta%20http-equiv%3D%22Content-Type%22%20content%3D%22text%2Fhtml%3B%20charset%3Dutf-8%22%20%2F%26gt%3B%0A%3CDIV%20class%3D%22%22%3E%3CP%3EHello%20S%C3%A9rgio%2C%3C%2FP%3E%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%3CP%3ESENSITIVITY_2G_8bits%2064%3C%2FP%3E%3CP%3ESENSITIVITY_4G_8bits%2032%3C%2FP%3E%3CP%3ESENSITIVITY_8G_8bits%2016%3C%2FP%3E%3CBR%20%2F%3E%3CP%3E%C2%B12g%3A%3C%2FP%3E%3CP%3EX_offset_2G_8_bit%20%3D%20Xout_8_bit%20*%208%20*%20(-1)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%3CP%3EY_offset_2G_8_bit%20%3D%20Yout_8_bit%20*%208%20*%20(-1)%3B%3C%2FP%3E%3CP%3EZ_offset_2G_8_bit%20%3D%20(Zout_8_bit%20-%20SENSITIVITY_2G_8bits)%20*%208%20*%20(-1)%3B%3C%2FP%3E%3CBR%20%2F%3E%3CP%3E%C2%B14g%3A%3C%2FP%3E%3CP%3EX_offset_4G_8_bit%20%3D%20Xout_8_bit%20*%2016%20*%20(-1)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%3CP%3EY_offset_4G_8_bit%20%3D%20Yout_8_bit%20*%2016%20*%20(-1)%3B%3C%2FP%3E%3CP%3EZ_offset_4G_8_bit%20%3D%20(Zout_8_bit%20-%20SENSITIVITY_4G_8bits)%20*%2016%20*%20(-1)%3B%3C%2FP%3E%3CBR%20%2F%3E%3CP%3E%C2%B18g%3A%3C%2FP%3E%3CP%3EX_offset_8G_8_bit%20%3D%20Xout_8_bit%20*%2032%20*%20(-1)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%3CP%3EY_offset_8G_8_bit%20%3D%20Yout_8_bit%20*%2032%20*%20(-1)%3B%3C%2FP%3E%3CP%3EZ_offset_8G_8_bit%20%3D%20(Zout_8_bit%20-%20SENSITIVITY_8G_8bits)%20*%2032%20*%20(-1)%3B%3C%2FP%3E%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%3CP%3E%E3%82%88%E3%82%8D%E3%81%97%E3%81%8F%E3%81%8A%E9%A1%98%E3%81%84%E3%81%84%E3%81%9F%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3ETomas%3C%2FP%3E%3C%2FDIV%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-1126870%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3AMMA8652FC%20-%20%E3%83%99%E3%82%A2%E3%83%A1%E3%82%BF%E3%83%AB%E3%82%B5%E3%83%B3%E3%83%97%E3%83%AB%E3%83%97%E3%83%AD%E3%82%B8%E3%82%A7%E3%82%AF%E3%83%88%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1126870%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%26lt%3Bmeta%20http-equiv%3D%22Content-Type%22%20content%3D%22text%2Fhtml%3B%20charset%3Dutf-8%22%20%2F%26gt%3B%0A%3CP%3EHello%20Tomas%2C%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E3%81%93%E3%81%AE%E3%83%97%E3%83%AD%E3%82%B8%E3%82%A7%E3%82%AF%E3%83%88%E3%81%AF%E9%9D%9E%E5%B8%B8%E3%81%AB%E5%BD%B9%E3%81%AB%E7%AB%8B%E3%81%A1%E3%80%81%E3%81%9D%E3%82%8C%E3%81%AB%E5%BE%93%E3%81%A3%E3%81%A6MMA8652FC%E3%82%92%E6%A7%8B%E6%88%90%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E%E3%81%97%E3%81%8B%E3%81%97%E3%80%81%E7%A7%81%E3%81%AF8%E3%83%93%E3%83%83%E3%83%88%E3%81%A0%E3%81%91%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%A6%E4%BD%9C%E6%A5%AD%E3%81%97%E3%81%9F%E3%81%84%E3%81%A7%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E8%E3%83%93%E3%83%83%E3%83%88%E3%81%AE%E3%81%BF%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%99%E3%82%8B%E3%82%88%E3%81%86%E3%81%AB%E6%A7%8B%E6%88%90%E3%81%A7%E3%81%8D%E3%80%81Xout_8_bit%E3%80%81Yout_8_bit%E3%80%81Zout_8_bit%E3%81%8C%E5%BE%97%E3%82%89%E3%82%8C%E3%81%BE%E3%81%99%E3%80%82%E3%81%97%E3%81%8B%E3%81%97%E3%80%81%E3%82%AA%E3%83%95%E3%82%BB%E3%83%83%E3%83%88%E5%80%A4%E3%81%AF%E3%81%A9%E3%81%AE%E3%82%88%E3%81%86%E3%81%AB%E8%A8%88%E7%AE%97%E3%81%99%E3%82%8C%E3%81%B0%E3%82%88%E3%81%84%E3%81%AE%E3%81%A7%E3%81%97%E3%82%87%E3%81%86%E3%81%8B%E3%80%82%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EX_offset_8_bit%20%3D%3C%2FSPAN%3E%20%3F%3C%2FP%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EY_offset_8_bit%20%3D%3C%2FSPAN%3E%20%3F%3C%2FP%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EZ_offset_8_bit%20%3D%3C%2FSPAN%3E%20%3F%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E5%8A%A9%E3%81%91%E3%81%A6%E3%81%84%E3%81%9F%E3%81%A0%E3%81%91%E3%81%BE%E3%81%99%E3%81%8B%E3%80%82%3C%2FP%3E%3CP%3E%E3%81%82%E3%82%8A%E3%81%8C%E3%81%A8%E3%81%86%E3%81%94%E3%81%96%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E3%82%88%E3%82%8D%E3%81%97%E3%81%8F%E3%81%8A%E9%A1%98%E3%81%84%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3ES%C3%A9rgio%3C%2FP%3E%3C%2FLINGO-BODY%3E
評価なし
バージョン履歴
最終更新日:
‎02-03-2026 05:19 PM
更新者: