MMA8652FC - Bare metal example project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MMA8652FC - Bare metal example project

MMA8652FC - Bare metal example project

Hi Everyone,

 

I would like to share here another simple bare-metal example code/demo for the Xtrinsic MMA8652FC digital accelerometer that I have created while working with the Freescale FRDM-KL25Z development platform and FRDM-FXS-MULTI(-B) sensor expansion board. To visualize the acceleration data that are read from the MMA8652FC using an interrupt technique through the I2C interface, I have used the FreeMASTER tool.

 

This example illustrates:

 

1. Initialization of the MKL25Z128 MCU (mainly I2C and PORT modules).

2. I2C data write and read operations.

3. Initialization of the accelerometer to achieve the highest resolution.

4. Simple offset calibration based on the AN4069.

5. Output data reading using an interrupt technique.

6. Conversion of the output values from registers 0x01 – 0x06 to real acceleration values in g’s.

7. Visualization of the output values in the FreeMASTER tool.

 

1. As you can see in the FRDM-FXS-MULTI(-B)/FRDM-KL25Z schematics and the image below, I2C signals are routed to the I2C1 module (PTC1 and PTC2 pins) of the KL25Z MCU and the INT1 output is connected to the PTA5 pin (make sure that pin #3 of J4 and pin #2 of J6 connector on the sensor expansion board are connected together). The INT1 output of the MMA8652FC is configured as a push-pull active-low output, so the corresponding PTA5 pin configuration is GPIO with an interrupt on falling edge.

 

12383_12383.jpg

 

The MCU is, therefore, configured as follows.

void MCU_Init(void)

{

     //I2C1 module initialization

     SIM_SCGC4 |= SIM_SCGC4_I2C1_MASK;        // Turn on clock to I2C1 module

     SIM_SCGC5 |= SIM_SCGC5_PORTC_MASK;       // Turn on clock to Port C module

     PORTC_PCR1 |= PORT_PCR_MUX(0x2);         // PTC1 pin is I2C1 SCL line

     PORTC_PCR2 |= PORT_PCR_MUX(0x2);         // PTC2 pin is I2C1 SDA line

     I2C1_F  |= I2C_F_ICR(0x14);              // SDA hold time = 2.125us, SCL start hold time = 4.25us, SCL stop hold time = 5.125us

     I2C1_C1 |= I2C_C1_IICEN_MASK;            // Enable I2C1 module

           

         //Configure the PTA5 pin (connected to the INT1 of the MMA8652FC) for falling edge interrupts

     SIM_SCGC5 |= SIM_SCGC5_PORTA_MASK;       // Turn on clock to Port A module

     PORTA_PCR5 |= (0|PORT_PCR_ISF_MASK|      // Clear the interrupt flag

                      PORT_PCR_MUX(0x1)|      // PTA5 is configured as GPIO

                      PORT_PCR_IRQC(0xA));    // PTA5 is configured for falling edge interrupts

           

        //Enable PORTA interrupt on NVIC

     NVIC_ICPR |= 1 << ((INT_PORTA - 16)%32);

     NVIC_ISER |= 1 << ((INT_PORTA - 16)%32);

}

 

2. The 7-bit I2C address of the MMA8652FC is fixed value 0x1D. As shown above, the SCL line is connected to the PTC1 pin and SDA line to the PTC2 pin. The I2C clock frequency is 125 kHz.

The screenshot below shows the write operation which writes the value 0x39 to the CTRL_REG1 (0x2A).

 

12384_12384.jpg

 

And here is the single byte read from the WHO_AM_I register 0x0D. As you can see, it returns the correct value 0x4A.

 

12385_12385.jpg

 

Multiple bytes of data can be read from sequential registers after each MMA8652FC acknowledgment (AK) is received until a no acknowledge (NAK) occurs from the KL25Z followed by a stop condition (SP) signaling an end of transmission. A burst read of 6 bytes from registers 0x01 to 0x06 is shown below. It also shows how the INT1 pin is automatically deasserted by reading the acceleration output data.

 

12386_12386.jpg

 

 

3. At the beginning of the initialization, all registers are reset to their default values by setting the RST bit of the CTRL_REG2 register. The dynamic range is set to ±2g and to achieve the highest resolution, the lowest ODR (1.56Hz) and the High Resolution mode are selected (more details in AN4075). The DRDY interrupt is enabled and routed to the INT1 interrupt pin that is configured to be a push-pull, active-low output.

void MMA8652FC_Init (void)

{

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, CTRL_REG2, 0x40);          // Reset all registers to POR values

    

     Pause(0x631);          // ~1ms delay

    

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, XYZ_DATA_CFG_REG, 0x00);   // +/-2g range with ~0.977mg/LSB 

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, CTRL_REG2, 0x02);          // High Resolution mode

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, CTRL_REG3, 0x00);          // Push-pull, active low interrupt

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, CTRL_REG4, 0x01);          // Enable DRDY interrupt

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, CTRL_REG5, 0x01);          // DRDY interrupt routed to INT1 - PTA5

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, CTRL_REG1, 0x39);          // ODR = 1.56Hz, Active mode      

}

 

4. A simple offset calibration method is implemented according to the AN4069.

 

void MMA8652FC_Calibration (void)

{

     char X_offset, Y_offset, Z_offset;

    

     DataReady = 0;      

         while (!DataReady){}          // Is a first set of data ready?

     DataReady = 0;

    

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, CTRL_REG1, 0x00);          // Standby mode     

    

     I2C_ReadMultiRegisters(MMA8652FC_I2C_ADDRESS, OUT_X_MSB_REG, 6, AccelData);          // Read data output registers 0x01-0x06       

           

     Xout_12_bit = ((short) (AccelData[0]<<8 | AccelData[1])) >> 4;             // Compute 12-bit X-axis acceleration output value

     Yout_12_bit = ((short) (AccelData[2]<<8 | AccelData[3])) >> 4;             // Compute 12-bit Y-axis acceleration output value

     Zout_12_bit = ((short) (AccelData[4]<<8 | AccelData[5])) >> 4;             // Compute 12-bit Z-axis acceleration output value

           

     X_offset = Xout_12_bit / 2 * (-1);          // Compute X-axis offset correction value

     Y_offset = Yout_12_bit / 2 * (-1);          // Compute Y-axis offset correction value

     Z_offset = (Zout_12_bit - SENSITIVITY_2G) / 2 * (-1);         // Compute Z-axis offset correction value

           

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, OFF_X_REG, X_offset);            

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, OFF_Y_REG, Y_offset);      

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, OFF_Z_REG, Z_offset);      

           

     I2C_WriteRegister(MMA8652FC_I2C_ADDRESS, CTRL_REG1, 0x39);          // Active mode again

}

 

5. In the ISR, only the interrupt flag is cleared and the DataReady variable is set to indicate the arrival of new data.

 

void PORTA_IRQHandler()

{

     PORTA_PCR5 |= PORT_PCR_ISF_MASK;          // Clear the interrupt flag

     DataReady = 1;   

}

 

6. The output values from accelerometer registers 0x01 – 0x06 are first converted to signed 12-bit values and afterwards to real values in g’s.

 

if (DataReady)             // Is a new set of data ready?

{            

     DataReady = 0;

                                                                                                                  

     I2C_ReadMultiRegisters(MMA8652FC_I2C_ADDRESS, OUT_X_MSB_REG, 6, AccelData);          // Read data output registers 0x01-0x06

         

         // 12-bit accelerometer data

     Xout_12_bit = ((short) (AccelData[0]<<8 | AccelData[1])) >> 4;             // Compute 12-bit X-axis acceleration output value

     Yout_12_bit = ((short) (AccelData[2]<<8 | AccelData[3])) >> 4;             // Compute 12-bit Y-axis acceleration output value

     Zout_12_bit = ((short) (AccelData[4]<<8 | AccelData[5])) >> 4;             // Compute 12-bit Z-axis acceleration output value

                  

         // Accelerometer data converted to g's

     Xout_g = ((float) Xout_12_bit) / SENSITIVITY_2G;              // Compute X-axis output value in g's

     Yout_g = ((float) Yout_12_bit) / SENSITIVITY_2G;              // Compute Y-axis output value in g's

     Zout_g = ((float) Zout_12_bit) / SENSITIVITY_2G;              // Compute Z-axis output value in g's              

}  

 

7. The calculated values can be watched in the "Variables" window on the top right of the Debug perspective or in the FreeMASTER application. To open and run the FreeMASTER project, install the FreeMASTER application and FreeMASTER Communication Driver.

 

12387_12387.jpg

 

12388_12388.jpg

 

Attached you can find the complete source code written in the CW for MCU's (Eclipse IDE) including the FreeMASTER project.

 

If there are any questions regarding this simple application, do not hesitate to ask below. Your feedback or suggestions are also welcome.

 

Regards,

Tomas

标签 (1)
附件
评论

Hello Tomas,

I found this project very helpful, and I follow it to configure my MMA8652FC.

But I want to work with it using only 8 bits.

I'm able to configure it to use only 8 bits, and I get the Xout_8_bit, Yout_8_bit, Zout_8_bit. But how do I calculate the offset values?

X_offset_8_bit = ?

Y_offset_8_bit = ?

Z_offset_8_bit = ?

Can you help me?

Thanks.

Regards,

Sérgio

Hello Sérgio,

 

SENSITIVITY_2G_8bits        64

SENSITIVITY_4G_8bits        32

SENSITIVITY_8G_8bits        16

 

±2g:

X_offset_2G_8_bit = Xout_8_bit * 8 * (-1);   

Y_offset_2G_8_bit = Yout_8_bit * 8 * (-1);   

Z_offset_2G_8_bit = (Zout_8_bit - SENSITIVITY_2G_8bits) * 8 * (-1);

 

±4g:

X_offset_4G_8_bit = Xout_8_bit * 16 * (-1);   

Y_offset_4G_8_bit = Yout_8_bit * 16 * (-1);   

Z_offset_4G_8_bit = (Zout_8_bit - SENSITIVITY_4G_8bits) * 16 * (-1);

 

±8g:

X_offset_8G_8_bit = Xout_8_bit * 32 * (-1);   

Y_offset_8G_8_bit = Yout_8_bit * 32 * (-1);   

Z_offset_8G_8_bit = (Zout_8_bit - SENSITIVITY_8G_8bits) * 32 * (-1);

 

Best regards,

Tomas

Hello Tomas,

Thanks for all the help.

Regards,

Sérgio

%3CLINGO-SUB%20id%3D%22lingo-sub-1126869%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3EMMA8652FC%20-%20%E8%A3%B8%E6%9C%BA%E9%A1%B9%E7%9B%AE%E7%A4%BA%E4%BE%8B%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1126869%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%E5%A4%A7%E5%AE%B6%E5%A5%BD%EF%BC%8C%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3E%E6%88%91%E6%83%B3%E5%9C%A8%E8%BF%99%E9%87%8C%E5%88%86%E4%BA%AB%E5%8F%A6%E4%B8%80%E4%B8%AA%E7%AE%80%E5%8D%95%E7%9A%84%E8%A3%B8%E6%9C%BA%E7%A4%BA%E4%BE%8B%E4%BB%A3%E7%A0%81%2F%E6%BC%94%E7%A4%BA%EF%BC%8C%E7%94%A8%E4%BA%8E%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fproducts%2Fsensors%2Fmotion-sensors%2F3-axis%2F2g-4g-8g-low-g-12-bit-digital-accelerometer%3AMMA8652FC%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EXtrinsic%20MMA8652FC%20%E6%95%B0%E5%AD%97%E5%8A%A0%E9%80%9F%E5%BA%A6%E8%AE%A1%EF%BC%8C%3C%2FA%3E%E8%BF%99%E6%98%AF%E6%88%91%E5%9C%A8%E4%BD%BF%E7%94%A8%20Freescale%20%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fdevelopment-boards%2Ffreedom-development-boards%2Fmcu-boards%2Ffreedom-development-platform-for-kinetis-kl14-kl15-kl24-kl25-mcus%3AFRDM-KL25Z%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EFRDM-KL25Z%20%E5%BC%80%E5%8F%91%E5%B9%B3%E5%8F%B0%3C%2FA%3E%E5%92%8C%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fdevelopment-boards%2Ffreedom-development-boards%2Fsensors%2Ffreedom-development-platform-for-nxp-sensors-with-bluetooth-%3AFRDM-FXS-MULT2-B%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EFRDM-FXS-MULTI(-B)%20%E4%BC%A0%E6%84%9F%E5%99%A8%E6%89%A9%E5%B1%95%E6%9D%BF%3C%2FA%3E%E6%97%B6%E5%88%9B%E5%BB%BA%E7%9A%84%E3%80%82%E4%B8%BA%E4%BA%86%E5%8F%AF%E8%A7%86%E5%8C%96%E9%80%9A%E8%BF%87%20I%20%3CSUP%3E2%3C%2FSUP%3E%20C%20%E6%8E%A5%E5%8F%A3%E4%BD%BF%E7%94%A8%E4%B8%AD%E6%96%AD%E6%8A%80%E6%9C%AF%E4%BB%8E%20MMA8652FC%20%E8%AF%BB%E5%8F%96%E7%9A%84%E5%8A%A0%E9%80%9F%E5%BA%A6%E6%95%B0%E6%8D%AE%EF%BC%8C%E6%88%91%E4%BD%BF%E7%94%A8%E4%BA%86%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fsoftware%2Fdevelopment-software%2Ffreemaster-run-time-debugging-tool%3AFREEMASTER%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EFreeMASTER%20%E5%B7%A5%E5%85%B7%3C%2FA%3E%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3E%E6%AD%A4%E7%A4%BA%E4%BE%8B%E8%AF%B4%E6%98%8E%EF%BC%9A%3C%2FP%3E%0A%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2010pt%3B%20line-height%3A%201.5em%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2010pt%3B%20line-height%3A%201.5em%3B%22%3E1.%20MKL25Z128%20MCU%20%E7%9A%84%E5%88%9D%E5%A7%8B%E5%8C%96%EF%BC%88%E4%B8%BB%E8%A6%81%E6%98%AF%20I%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22line-height%3A%201.5em%3B%22%3E%3CSUP%3E2%3C%2FSUP%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010pt%3B%20line-height%3A%201.5em%3B%22%3EC%20%E5%92%8C%20PORT%20%E6%A8%A1%E5%9D%97%EF%BC%89%E3%80%82%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3E2.%20%3CSUP%3EI2C%3C%2FSUP%3E%E6%95%B0%E6%8D%AE%E5%86%99%E5%85%A5%E3%80%81%E8%AF%BB%E5%8F%96%E6%93%8D%E4%BD%9C%E3%80%82%3C%2FP%3E%0A%3CP%3E3.%20%E5%88%9D%E5%A7%8B%E5%8C%96%E5%8A%A0%E9%80%9F%E5%BA%A6%E8%AE%A1%E4%BB%A5%E5%AE%9E%E7%8E%B0%E6%9C%80%E9%AB%98%E5%88%86%E8%BE%A8%E7%8E%87%E3%80%82%3C%2FP%3E%0A%3CP%3E4.%E5%9F%BA%E4%BA%8E%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note%2FAN4069.pdf%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EAN4069%3C%2FA%3E%E7%9A%84%E7%AE%80%E5%8D%95%E5%A4%B1%E8%B0%83%E6%A0%A1%E5%87%86%E3%80%82%3C%2FP%3E%0A%3CP%3E5.%E9%87%87%E7%94%A8%E4%B8%AD%E6%96%AD%E6%8A%80%E6%9C%AF%E8%BE%93%E5%87%BA%E6%95%B0%E6%8D%AE%E8%AF%BB%E5%8F%96%E3%80%82%3C%2FP%3E%0A%3CP%3E6.%20%E5%B0%86%E5%AF%84%E5%AD%98%E5%99%A8%200x01%20%E2%80%93%200x06%20%E7%9A%84%E8%BE%93%E5%87%BA%E5%80%BC%E8%BD%AC%E6%8D%A2%E4%B8%BA%20g%20%E4%B8%AD%E7%9A%84%E5%AE%9E%E9%99%85%E5%8A%A0%E9%80%9F%E5%BA%A6%E5%80%BC%E3%80%82%3C%2FP%3E%0A%3CP%3E7.%20%E5%9C%A8%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fsoftware%2Fdevelopment-software%2Ffreemaster-run-time-debugging-tool%3AFREEMASTER%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EFreeMASTER%20%E5%B7%A5%E5%85%B7%3C%2FA%3E%E4%B8%AD%E5%8F%AF%E8%A7%86%E5%8C%96%E8%BE%93%E5%87%BA%E5%80%BC%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3E1.%E6%AD%A3%E5%A6%82%E6%82%A8%E5%9C%A8%20FRDM-FXS-MULTI(-B)%2FFRDM-KL25Z%20%E5%8E%9F%E7%90%86%E5%9B%BE%E5%92%8C%E4%B8%8B%E5%9B%BE%E4%B8%AD%E6%89%80%E7%9C%8B%E5%88%B0%E7%9A%84%EF%BC%8CI2C%20%E4%BF%A1%E5%8F%B7%E8%A2%AB%E8%B7%AF%E7%94%B1%E5%88%B0%20KL25Z%20MCU%20%E7%9A%84%20I2C1%20%E6%A8%A1%E5%9D%97%EF%BC%88PTC1%20%E5%92%8C%20PTC2%20%E5%BC%95%E8%84%9A%EF%BC%89%EF%BC%8C%E5%B9%B6%E4%B8%94%20INT1%20%E8%BE%93%E5%87%BA%E8%BF%9E%E6%8E%A5%E5%88%B0%20PTA5%20%E5%BC%95%E8%84%9A%EF%BC%88%E7%A1%AE%E4%BF%9D%E4%BC%A0%E6%84%9F%E5%99%A8%E6%89%A9%E5%B1%95%E6%9D%BF%E4%B8%8A%20J4%20%E7%9A%84%E5%BC%95%E8%84%9A%203%20%E5%92%8C%20J6%20%E8%BF%9E%E6%8E%A5%E5%99%A8%E7%9A%84%E5%BC%95%E8%84%9A%202%20%E8%BF%9E%E6%8E%A5%E5%9C%A8%E4%B8%80%E8%B5%B7%EF%BC%89%E3%80%82MMA8652FC%20%E7%9A%84%20INT1%20%E8%BE%93%E5%87%BA%E9%85%8D%E7%BD%AE%E4%B8%BA%E6%8E%A8%E6%8C%BD%E5%BC%8F%E4%BD%8E%E7%94%B5%E5%B9%B3%E6%9C%89%E6%95%88%E8%BE%93%E5%87%BA%EF%BC%8C%E5%9B%A0%E6%AD%A4%E7%9B%B8%E5%BA%94%E7%9A%84%20PTA5%20%E5%BC%95%E8%84%9A%E9%85%8D%E7%BD%AE%E4%B8%BA%E4%B8%8B%E9%99%8D%E6%B2%BF%E4%B8%AD%E6%96%AD%E7%9A%84%20GPIO%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%2212383_12383.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%2212383_12383.jpg%22%20style%3D%22width%3A%20810px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F117659i98FD4BED6903F4DA%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%2212383_12383.jpg%22%20alt%3D%2212383_12383.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E12383_12383.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3E%E5%9B%A0%E6%AD%A4%EF%BC%8CMCU%20%E9%85%8D%E7%BD%AE%E5%A6%82%E4%B8%8B%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Evoid%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%3CSTRONG%3EMCU_Init%3C%2FSTRONG%3E(%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Evoid%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%2F%2FI2C1%20module%20initialization%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3ESIM_SCGC4%20%7C%3D%20SIM_SCGC4_I2C1_MASK%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20%E6%89%93%E5%BC%80%20I2C1%20%E6%A8%A1%E5%9D%97%E7%9A%84%E6%97%B6%E9%92%9F%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3ESIM_SCGC5%20%7C%3D%20SIM_SCGC5_PORTC_MASK%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20%E6%89%93%E5%BC%80%E7%AB%AF%E5%8F%A3%20C%20%E6%A8%A1%E5%9D%97%E7%9A%84%E6%97%B6%E9%92%9F%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EPORTC_PCR1%20%7C%3D%20PORT_PCR_MUX(0x2)%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20PTC1%20%E5%BC%95%E8%84%9A%E4%B8%BA%20I2C1%20SCL%20%E7%BA%BF%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EPORTC_PCR2%20%7C%3D%20PORT_PCR_MUX(0x2)%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20PTC2%20%E5%BC%95%E8%84%9A%E4%B8%BA%20I2C1%20SDA%20%E7%BA%BF%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EI2C1_F%20%7C%3D%20I2C_F_ICR(0x14)%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20SDA%20%E4%BF%9D%E6%8C%81%E6%97%B6%E9%97%B4%20%3D%202.125us%EF%BC%8CSCL%20%E5%90%AF%E5%8A%A8%E4%BF%9D%E6%8C%81%E6%97%B6%E9%97%B4%20%3D%204.25us%EF%BC%8CSCL%20%E5%81%9C%E6%AD%A2%E4%BF%9D%E6%8C%81%E6%97%B6%E9%97%B4%20%3D%205.125us%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EI2C1_C1%20%7C%3D%20I2C_C1_IICEN_MASK%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20%E5%90%AF%E7%94%A8%20I2C1%20%E6%A8%A1%E5%9D%97%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%E9%85%8D%E7%BD%AEPTA5%E5%BC%95%E8%84%9A%EF%BC%88%E8%BF%9E%E6%8E%A5%E5%88%B0MMA8652FC%E7%9A%84INT1%EF%BC%89%E7%94%A8%E4%BA%8E%E4%B8%8B%E9%99%8D%E6%B2%BF%E4%B8%AD%E6%96%AD%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3ESIM_SCGC5%20%7C%3D%20SIM_SCGC5_PORTA_MASK%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20%E6%89%93%E5%BC%80%E7%AB%AF%E5%8F%A3%20A%20%E6%A8%A1%E5%9D%97%E7%9A%84%E6%97%B6%E9%92%9F%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EPORTA_PCR5%20%7C%3D%20(0%7CPORT_PCR_ISF_MASK%7C%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%E6%B8%85%E9%99%A4%E4%B8%AD%E6%96%AD%E6%A0%87%E5%BF%97%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EPORT_PCR_MUX(0x1)%7C%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20PTA5%20%E9%85%8D%E7%BD%AE%E4%B8%BA%20GPIO%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EPORT_PCR_IRQC(0xA))%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20PTA5%20%E9%85%8D%E7%BD%AE%E4%B8%BA%E4%B8%8B%E9%99%8D%E6%B2%BF%E4%B8%AD%E6%96%AD%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%E5%9C%A8NVIC%E4%B8%8A%E5%90%AF%E7%94%A8PORTA%E4%B8%AD%E6%96%AD%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3ENVIC_ICPR%20%7C%3D%201%20%26lt%3B%26lt%3B%20((%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22color%3A%20%230000c0%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CEM%3EINT_PORTA%3C%2FEM%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E-%2016)%2532)%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3ENVIC_ISER%20%7C%3D%201%20%26lt%3B%26lt%3B%20((%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22color%3A%20%230000c0%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CEM%3EINT_PORTA%3C%2FEM%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E-%2016)%2532)%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7D%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3E2.%20MMA8652FC%20%E7%9A%84%207%20%E4%BD%8D%20I%20%3CSUP%3E2%3C%2FSUP%3E%20C%20%E5%9C%B0%E5%9D%80%E4%B8%BA%E5%9B%BA%E5%AE%9A%E5%80%BC%200x1D%E3%80%82%E5%A6%82%E4%B8%8A%E6%89%80%E7%A4%BA%EF%BC%8CSCL%20%E7%BA%BF%E8%BF%9E%E6%8E%A5%E5%88%B0%20PTC1%20%E5%BC%95%E8%84%9A%EF%BC%8CSDA%20%E7%BA%BF%E8%BF%9E%E6%8E%A5%E5%88%B0%20PTC2%20%E5%BC%95%E8%84%9A%E3%80%82I2C%E6%97%B6%E9%92%9F%E9%A2%91%E7%8E%87%E4%B8%BA125%20kHz%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%E4%B8%8B%E9%9D%A2%E7%9A%84%E5%B1%8F%E5%B9%95%E6%88%AA%E5%9B%BE%E6%98%BE%E7%A4%BA%E4%BA%86%E5%B0%86%E5%80%BC%200x39%20%E5%86%99%E5%85%A5%20CTRL_REG1%20(0x2A)%20%E7%9A%84%E5%86%99%E5%85%A5%E6%93%8D%E4%BD%9C%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%209.0pt%3B%20font-family%3A%20'Arial'%2C'sans-serif'%3B%20background%3A%20white%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%209.0pt%3B%20font-family%3A%20'Arial'%2C'sans-serif'%3B%20background%3A%20white%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%2212384_12384.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%2212384_12384.jpg%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F117660i0EEB2A640B959CC9%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%2212384_12384.jpg%22%20alt%3D%2212384_12384.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E12384_12384.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%209.0pt%3B%20font-family%3A%20'Arial'%2C'sans-serif'%3B%20background%3A%20white%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%E8%BF%99%E6%98%AF%E4%BB%8E%20WHO_AM_I%20%E5%AF%84%E5%AD%98%E5%99%A8%200x0D%20%E8%AF%BB%E5%8F%96%E7%9A%84%E5%8D%95%E4%B8%AA%E5%AD%97%E8%8A%82%E3%80%82%E5%A6%82%E6%82%A8%E6%89%80%E8%A7%81%EF%BC%8C%E5%AE%83%E8%BF%94%E5%9B%9E%E6%AD%A3%E7%A1%AE%E7%9A%84%E5%80%BC0x4A%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%20margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%2212385_12385.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%2212385_12385.jpg%22%20style%3D%22width%3A%20985px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F117661iF1B19761AF5AE278%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%2212385_12385.jpg%22%20alt%3D%2212385_12385.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E12385_12385.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%20margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%E5%9C%A8%E6%8E%A5%E6%94%B6%E5%88%B0%E6%AF%8F%E4%B8%AA%20MMA8652FC%20%E7%A1%AE%E8%AE%A4%20(AK)%20%E5%90%8E%EF%BC%8C%E5%8F%AF%E4%BB%A5%E4%BB%8E%E8%BF%9E%E7%BB%AD%E5%AF%84%E5%AD%98%E5%99%A8%E8%AF%BB%E5%8F%96%E5%A4%9A%E4%B8%AA%E5%AD%97%E8%8A%82%E7%9A%84%E6%95%B0%E6%8D%AE%EF%BC%8C%E7%9B%B4%E5%88%B0%20KL25Z%20%E5%8F%91%E5%87%BA%E6%97%A0%E7%A1%AE%E8%AE%A4%20(NAK)%20%E4%BF%A1%E5%8F%B7%EF%BC%8C%E9%9A%8F%E5%90%8E%E5%87%BA%E7%8E%B0%E8%A1%A8%E7%A4%BA%E4%BC%A0%E8%BE%93%E7%BB%93%E6%9D%9F%E7%9A%84%E5%81%9C%E6%AD%A2%E6%9D%A1%E4%BB%B6%20(SP)%E3%80%82%E4%B8%8B%E9%9D%A2%E6%98%BE%E7%A4%BA%E4%BA%86%E4%BB%8E%E5%AF%84%E5%AD%98%E5%99%A8%200x01%20%E8%87%B3%200x06%20%E7%9A%84%206%20%E4%B8%AA%E5%AD%97%E8%8A%82%E7%9A%84%E7%AA%81%E5%8F%91%E8%AF%BB%E5%8F%96%E3%80%82%E5%AE%83%E8%BF%98%E6%98%BE%E7%A4%BA%E4%BA%86%E5%A6%82%E4%BD%95%E9%80%9A%E8%BF%87%E8%AF%BB%E5%8F%96%E5%8A%A0%E9%80%9F%E5%BA%A6%E8%BE%93%E5%87%BA%E6%95%B0%E6%8D%AE%E8%87%AA%E5%8A%A8%E5%8F%96%E6%B6%88%20INT1%20%E5%BC%95%E8%84%9A%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%20margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%2212386_12386.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%2212386_12386.jpg%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F117662i43F527D64FE4AC04%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%2212386_12386.jpg%22%20alt%3D%2212386_12386.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E12386_12386.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%20margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3E3.%20%E5%9C%A8%E5%88%9D%E5%A7%8B%E5%8C%96%E5%BC%80%E5%A7%8B%E6%97%B6%EF%BC%8C%E9%80%9A%E8%BF%87%E8%AE%BE%E7%BD%AE%20CTRL_REG2%20%E5%AF%84%E5%AD%98%E5%99%A8%E7%9A%84%20RST%20%E4%BD%8D%E5%B0%86%E6%89%80%E6%9C%89%E5%AF%84%E5%AD%98%E5%99%A8%E9%87%8D%E7%BD%AE%E4%B8%BA%E5%85%B6%E9%BB%98%E8%AE%A4%E5%80%BC%E3%80%82%E5%8A%A8%E6%80%81%E8%8C%83%E5%9B%B4%E8%AE%BE%E7%BD%AE%E4%B8%BA%C2%B12g%EF%BC%8C%E4%B8%BA%E4%BA%86%E5%AE%9E%E7%8E%B0%E6%9C%80%E9%AB%98%E5%88%86%E8%BE%A8%E7%8E%87%EF%BC%8C%E9%80%89%E6%8B%A9%E4%BA%86%E6%9C%80%E4%BD%8EODR%EF%BC%881.56Hz%EF%BC%89%E5%92%8C%E9%AB%98%E5%88%86%E8%BE%A8%E7%8E%87%E6%A8%A1%E5%BC%8F%EF%BC%88%E6%9B%B4%E5%A4%9A%E8%AF%A6%E7%BB%86%E4%BF%A1%E6%81%AF%E8%AF%B7%E5%8F%82%E8%A7%81%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note%2FAN4075.pdf%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EAN4075%3C%2FA%3E%20%EF%BC%89%E3%80%82DRDY%20%E4%B8%AD%E6%96%AD%E5%B7%B2%E5%90%AF%E7%94%A8%E5%B9%B6%E8%B7%AF%E7%94%B1%E8%87%B3%E9%85%8D%E7%BD%AE%E4%B8%BA%E6%8E%A8%E6%8C%BD%E5%BC%8F%E3%80%81%E4%BD%8E%E7%94%B5%E5%B9%B3%E6%9C%89%E6%95%88%E8%BE%93%E5%87%BA%E7%9A%84%20INT1%20%E4%B8%AD%E6%96%AD%E5%BC%95%E8%84%9A%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Evoid%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%3CSTRONG%3EMMA8652FC_Init%3C%2FSTRONG%3E%20(%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Evoid%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EI2C_WriteRegister(MMA8652FC_I2C_ADDRESS%2C%20CTRL_REG2%2C%200x40)%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20%E5%B0%86%E6%89%80%E6%9C%89%E5%AF%84%E5%AD%98%E5%99%A8%E9%87%8D%E7%BD%AE%E4%B8%BA%20POR%20%E5%80%BC%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E6%9A%82%E5%81%9C%EF%BC%880x631%EF%BC%89%EF%BC%9B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%E5%BB%B6%E8%BF%9F%E7%BA%A6%201%20%E6%AF%AB%E7%A7%92%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EI2C_WriteRegister(MMA8652FC_I2C_ADDRESS%2C%20XYZ_DATA_CFG_REG%2C%200x00)%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20%2B%2F-2g%20%E8%8C%83%E5%9B%B4%EF%BC%8C~0.977mg%2FLSB%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EI2C_WriteRegister(MMA8652FC_I2C_ADDRESS%2C%20CTRL_REG2%2C%200x02)%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%E9%AB%98%E5%88%86%E8%BE%A8%E7%8E%87%E6%A8%A1%E5%BC%8F%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EI2C_WriteRegister(MMA8652FC_I2C_ADDRESS%2C%20CTRL_REG3%2C%200x00)%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%E6%8E%A8%E6%8C%BD%EF%BC%8C%E4%BD%8E%E7%94%B5%E5%B9%B3%E6%9C%89%E6%95%88%E4%B8%AD%E6%96%AD%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EI2C_WriteRegister(MMA8652FC_I2C_ADDRESS%2C%20CTRL_REG4%2C%200x01)%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%E5%90%AF%E7%94%A8DRDY%E4%B8%AD%E6%96%AD%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EI2C_WriteRegister(MMA8652FC_I2C_ADDRESS%2C%20CTRL_REG5%2C%200x01)%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2FDRDY%E4%B8%AD%E6%96%AD%E8%B7%AF%E7%94%B1%E5%88%B0INT1%20-%20PTA5%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EI2C_WriteRegister(MMA8652FC_I2C_ADDRESS%2C%20CTRL_REG1%2C%200x39)%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20ODR%20%3D%201.56Hz%EF%BC%8C%E4%B8%BB%E5%8A%A8%E6%A8%A1%E5%BC%8F%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7D%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E4.%20%E6%A0%B9%E6%8D%AE%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note%2FAN4069.pdf%22%20target%3D%22_blank%22%20rel%3D%22noopener%20nofollow%20noreferrer%22%3EAN4069%3C%2FA%3E%E5%AE%9E%E7%8E%B0%E4%BA%86%E4%B8%80%E7%A7%8D%E7%AE%80%E5%8D%95%E7%9A%84%E5%A4%B1%E8%B0%83%E6%A0%A1%E5%87%86%E6%96%B9%E6%B3%95%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%20margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Evoid%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%3CSTRONG%3EMMA8652FC_Calibration%3C%2FSTRONG%3E%20%EF%BC%88%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Evoid%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%EF%BC%89%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%E5%AD%97%E7%AC%A6%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EX_offset%EF%BC%8CY_offset%EF%BC%8CZ_offset%EF%BC%9B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E6%95%B0%E6%8D%AE%E5%B0%B1%E7%BB%AA%3D0%EF%BC%9B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Ewhile%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E(!DataReady)%7B%7D%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20%E7%AC%AC%E4%B8%80%E7%BB%84%E6%95%B0%E6%8D%AE%E5%87%86%E5%A4%87%E5%A5%BD%E4%BA%86%E5%90%97%EF%BC%9F%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E6%95%B0%E6%8D%AE%E5%B0%B1%E7%BB%AA%3D0%EF%BC%9B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EI2C_WriteRegister(MMA8652FC_I2C_ADDRESS%2C%20CTRL_REG1%2C%200x00)%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%E5%BE%85%E6%9C%BA%E6%A8%A1%E5%BC%8F%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EI2C_ReadMultiRegisters(MMA8652FC_I2C_ADDRESS%2C%20OUT_X_MSB_REG%2C%206%2C%20AccelData)%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%E8%AF%BB%E5%8F%96%E6%95%B0%E6%8D%AE%E8%BE%93%E5%87%BA%E5%AF%84%E5%AD%98%E5%99%A80x01-0x06%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EXout_12_bit%20%3D%20((%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Eshort%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%20(AccelData%5B0%5D%26lt%3B%26lt%3B8%20%7C%20AccelData%5B1%5D))%20%26gt%3B%26gt%3B%204%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%E8%AE%A1%E7%AE%9712%E4%BD%8DX%E8%BD%B4%E5%8A%A0%E9%80%9F%E5%BA%A6%E8%BE%93%E5%87%BA%E5%80%BC%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EYout_12_bit%20%3D%20((%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Eshort%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%20(AccelData%5B2%5D%26lt%3B%26lt%3B8%20%7C%20AccelData%5B3%5D))%20%26gt%3B%26gt%3B%204%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20%E8%AE%A1%E7%AE%9712%E4%BD%8DY%E8%BD%B4%E5%8A%A0%E9%80%9F%E5%BA%A6%E8%BE%93%E5%87%BA%E5%80%BC%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EZout_12_bit%20%3D%20((%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Eshort%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%20(AccelData%5B4%5D%26lt%3B%26lt%3B8%20%7C%20AccelData%5B5%5D))%20%26gt%3B%26gt%3B%204%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%E8%AE%A1%E7%AE%9712%E4%BD%8DZ%E8%BD%B4%E5%8A%A0%E9%80%9F%E5%BA%A6%E8%BE%93%E5%87%BA%E5%80%BC%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EX_offset%20%3D%20Xout_12_bit%20%2F%202%20*%20(-1)%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%E8%AE%A1%E7%AE%97X%E8%BD%B4%E5%81%8F%E7%A7%BB%E6%A0%A1%E6%AD%A3%E5%80%BC%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EY_offset%20%3D%20Yout_12_bit%20%2F%202%20*%20(-1)%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%E8%AE%A1%E7%AE%97Y%E8%BD%B4%E5%81%8F%E7%A7%BB%E6%A0%A1%E6%AD%A3%E5%80%BC%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EZ_offset%20%3D%20(Zout_12_bit%20-%20SENSITIVITY_2G)%20%2F%202%20*%20(-1)%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%E8%AE%A1%E7%AE%97Z%E8%BD%B4%E5%81%8F%E7%A7%BB%E6%A0%A1%E6%AD%A3%E5%80%BC%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EI2C_WriteRegister%EF%BC%88MMA8652FC_I2C_ADDRESS%EF%BC%8COFF_X_REG%EF%BC%8CX_offset%EF%BC%89%EF%BC%9B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EI2C_WriteRegister%EF%BC%88MMA8652FC_I2C_ADDRESS%EF%BC%8COFF_Y_REG%EF%BC%8CY_offset%EF%BC%89%EF%BC%9B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EI2C_WriteRegister%EF%BC%88MMA8652FC_I2C_ADDRESS%EF%BC%8COFF_Z_REG%EF%BC%8CZ_offset%EF%BC%89%EF%BC%9B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EI2C_WriteRegister(MMA8652FC_I2C_ADDRESS%2C%20CTRL_REG1%2C%200x39)%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%E5%86%8D%E6%AC%A1%E8%BF%9B%E5%85%A5%E6%B4%BB%E5%8A%A8%E6%A8%A1%E5%BC%8F%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7D%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E5.%E5%9C%A8ISR%E4%B8%AD%EF%BC%8C%E4%BB%85%E6%B8%85%E9%99%A4%E4%B8%AD%E6%96%AD%E6%A0%87%E5%BF%97%E5%B9%B6%E8%AE%BE%E7%BD%AEDataReady%E5%8F%98%E9%87%8F%E4%BB%A5%E6%8C%87%E7%A4%BA%E6%96%B0%E6%95%B0%E6%8D%AE%E7%9A%84%E5%88%B0%E8%BE%BE%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3CSPAN%20style%3D%22font-weight%3A%20inherit%3B%20font-style%3A%20inherit%3B%20font-size%3A%2010pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010pt%3B%20font-style%3A%20inherit%3B%20font-family%3A%20inherit%3B%20font-weight%3A%20inherit%3B%22%3E%3CSTRONG%3E%E6%97%A0%E6%95%88%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-weight%3A%20inherit%3B%20font-style%3A%20inherit%3B%20font-size%3A%2010pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%3CSPAN%20style%3D%22font-style%3A%20inherit%3B%20font-family%3A%20inherit%3B%20font-weight%3A%20inherit%3B%22%3E%3CSTRONG%3EPORTA_IRQHandler%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%EF%BC%88%EF%BC%89%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3CSPAN%20style%3D%22font-weight%3A%20inherit%3B%20font-style%3A%20inherit%3B%20font-size%3A%2010pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3CSPAN%20style%3D%22font-weight%3A%20inherit%3B%20font-style%3A%20inherit%3B%20font-size%3A%2010pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EPORTA_PCR5%20%7C%3D%20PORT_PCR_ISF_MASK%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-weight%3A%20inherit%3B%20font-style%3A%20inherit%3B%20font-size%3A%2010pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%E6%B8%85%E9%99%A4%E4%B8%AD%E6%96%AD%E6%A0%87%E5%BF%97%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3CSPAN%20style%3D%22font-weight%3A%20inherit%3B%20font-style%3A%20inherit%3B%20font-size%3A%2010pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E6%95%B0%E6%8D%AE%E5%B0%B1%E7%BB%AA%3D1%EF%BC%9B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%20color%3A%20%233d3d3d%3B%22%3E%3CSPAN%20style%3D%22font-weight%3A%20inherit%3B%20font-style%3A%20inherit%3B%20font-size%3A%2010pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7D%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%20margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E6.%E5%8A%A0%E9%80%9F%E5%BA%A6%E8%AE%A1%E5%AF%84%E5%AD%98%E5%99%A8%200x01%20%E2%80%93%200x06%20%E7%9A%84%E8%BE%93%E5%87%BA%E5%80%BC%E9%A6%96%E5%85%88%E8%BD%AC%E6%8D%A2%E4%B8%BA%E6%9C%89%E7%AC%A6%E5%8F%B7%E7%9A%84%2012%20%E4%BD%8D%E5%80%BC%EF%BC%8C%E7%84%B6%E5%90%8E%E8%BD%AC%E6%8D%A2%E4%B8%BA%20g%20%E7%9A%84%E5%AE%9E%E5%80%BC%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%20margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Eif%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E(DataReady)%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20%E6%96%B0%E7%9A%84%E4%B8%80%E7%BB%84%E6%95%B0%E6%8D%AE%E6%98%AF%E5%90%A6%E5%87%86%E5%A4%87%E5%A5%BD%E4%BA%86%EF%BC%9F%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E6%95%B0%E6%8D%AE%E5%B0%B1%E7%BB%AA%3D0%EF%BC%9B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EI2C_ReadMultiRegisters(MMA8652FC_I2C_ADDRESS%2C%20OUT_X_MSB_REG%2C%206%2C%20AccelData)%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%E8%AF%BB%E5%8F%96%E6%95%B0%E6%8D%AE%E8%BE%93%E5%87%BA%E5%AF%84%E5%AD%98%E5%99%A80x01-0x06%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%2012-bit%20accelerometer%20data%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EXout_12_bit%20%3D%20((%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Eshort%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%20(AccelData%5B0%5D%26lt%3B%26lt%3B8%20%7C%20AccelData%5B1%5D))%20%26gt%3B%26gt%3B%204%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%E8%AE%A1%E7%AE%9712%E4%BD%8DX%E8%BD%B4%E5%8A%A0%E9%80%9F%E5%BA%A6%E8%BE%93%E5%87%BA%E5%80%BC%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EYout_12_bit%20%3D%20((%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Eshort%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%20(AccelData%5B2%5D%26lt%3B%26lt%3B8%20%7C%20AccelData%5B3%5D))%20%26gt%3B%26gt%3B%204%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20%E8%AE%A1%E7%AE%9712%E4%BD%8DY%E8%BD%B4%E5%8A%A0%E9%80%9F%E5%BA%A6%E8%BE%93%E5%87%BA%E5%80%BC%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EZout_12_bit%20%3D%20((%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Eshort%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%20(AccelData%5B4%5D%26lt%3B%26lt%3B8%20%7C%20AccelData%5B5%5D))%20%26gt%3B%26gt%3B%204%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%E8%AE%A1%E7%AE%9712%E4%BD%8DZ%E8%BD%B4%E5%8A%A0%E9%80%9F%E5%BA%A6%E8%BE%93%E5%87%BA%E5%80%BC%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20%E5%8A%A0%E9%80%9F%E5%BA%A6%E8%AE%A1%E6%95%B0%E6%8D%AE%E8%BD%AC%E6%8D%A2%E4%B8%BA%20g%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EXout_g%20%3D%20((%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Efloat%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%20Xout_12_bit)%20%2F%20SENSITIVITY_2G%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20%E8%AE%A1%E7%AE%97%20g%20%E4%B8%AD%E7%9A%84%20X%20%E8%BD%B4%E8%BE%93%E5%87%BA%E5%80%BC%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EYout_g%20%3D%20((%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Efloat%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%20Yout_12_bit)%20%2F%20SENSITIVITY_2G%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20%E8%AE%A1%E7%AE%97%20Y%20%E8%BD%B4%E8%BE%93%E5%87%BA%E5%80%BC%EF%BC%88%E5%8D%95%E4%BD%8D%E4%B8%BA%20g%EF%BC%89%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EZout_g%20%3D%20((%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Efloat%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%20Zout_12_bit)%20%2F%20SENSITIVITY_2G%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F%2F%20%E8%AE%A1%E7%AE%97%20g%20%E4%B8%AD%E7%9A%84%20Z%20%E8%BD%B4%E8%BE%93%E5%87%BA%E5%80%BC%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20black%3B%20font-family%3A%20Consolas%3B%20font-size%3A%2010pt%3B%20line-height%3A%201.5em%3B%22%3E%7D%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20black%3B%20font-family%3A%20Consolas%3B%20font-size%3A%2010pt%3B%20line-height%3A%201.5em%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3E7.%20%E6%82%A8%E5%8F%AF%E4%BB%A5%E5%9C%A8%E8%B0%83%E8%AF%95%E8%A7%86%E8%A7%92%E5%8F%B3%E4%B8%8A%E8%A7%92%E7%9A%84%E2%80%9C%E5%8F%98%E9%87%8F%E2%80%9D%E7%AA%97%E5%8F%A3%E6%88%96%20FreeMASTER%20%E5%BA%94%E7%94%A8%E7%A8%8B%E5%BA%8F%E4%B8%AD%E6%9F%A5%E7%9C%8B%E8%AE%A1%E7%AE%97%E5%80%BC%E3%80%82%E8%A6%81%E6%89%93%E5%BC%80%E5%B9%B6%E8%BF%90%E8%A1%8C%20FreeMASTER%20%E9%A1%B9%E7%9B%AE%EF%BC%8C%E8%AF%B7%E5%AE%89%E8%A3%85%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fsoftware%2Fdevelopment-software%2Ffreemaster-run-time-debugging-tool%3AFREEMASTER%22%20target%3D%22_blank%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3EFreeMASTER%20%E5%BA%94%E7%94%A8%E7%A8%8B%E5%BA%8F%3C%2FA%3E%E5%92%8C%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fwebapp%2Fsps%2Fdownload%2Flicense.jsp%3FcolCode%3DFMASTERSCIDRV%22%20target%3D%22_blank%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3EFreeMASTER%20%E9%80%9A%E4%BF%A1%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%3C%2FA%3E%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22line-height%3A%201.5em%3B%20color%3A%20%233d3d3d%3B%20font-size%3A%2010pt%3B%20font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22line-height%3A%201.5em%3B%20color%3A%20%233d3d3d%3B%20font-size%3A%2010pt%3B%20font-family%3A%20'Helvetica%20Neue'%2C%20Helvetica%2C%20Arial%2C%20'Lucida%20Grande'%2C%20sans-serif%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%2212387_12387.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%2212387_12387.jpg%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F117663i406293ABF1946E2D%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%2212387_12387.jpg%22%20alt%3D%2212387_12387.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E12387_12387.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3CBR%20%2F%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%20lia-image-align-inline%22%20image-alt%3D%2212388_12388.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%2212388_12388.jpg%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F117664iADBF69B1F6440CC8%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%2212388_12388.jpg%22%20alt%3D%2212388_12388.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E12388_12388.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3E%E9%99%84%E4%BB%B6%E4%B8%AD%E6%82%A8%E5%8F%AF%E4%BB%A5%E6%89%BE%E5%88%B0%E7%94%A8%3CA%20href%3D%22https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fsoftware%2Fdevelopment-software%2Fcodewarrior-development-tools%2Fcodewarrior-legacy%2Fcodewarrior-for-mcus-eclipse-ide-coldfire-56800-e-dsc-qorivva-56xx-rs08-s08-s12z-11-1%3ACW-MCU10%22%20target%3D%22_blank%22%20rel%3D%22nofollow%20noopener%20noreferrer%22%3ECW%20%E4%B8%BA%20MCU%3C%2FA%3E%20%EF%BC%88Eclipse%20IDE%EF%BC%89%E7%BC%96%E5%86%99%E7%9A%84%E5%AE%8C%E6%95%B4%E6%BA%90%E4%BB%A3%E7%A0%81%EF%BC%8C%E5%8C%85%E6%8B%AC%20FreeMASTER%20%E9%A1%B9%E7%9B%AE%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3E%E8%8B%A5%E5%AF%B9%E6%9C%AC%E7%AE%80%E6%98%93%E5%BA%94%E7%94%A8%E5%AD%98%E5%9C%A8%E4%BB%BB%E4%BD%95%E7%96%91%E9%97%AE%EF%BC%8C%E8%AF%B7%E9%9A%8F%E6%97%B6%E5%9C%A8%E4%B8%8B%E6%96%B9%E7%95%99%E8%A8%80%E6%8F%90%E9%97%AE%E3%80%82%E4%B9%9F%E6%AC%A2%E8%BF%8E%E6%8F%90%E4%BE%9B%E5%8F%8D%E9%A6%88%E6%88%96%E5%BB%BA%E8%AE%AE%E3%80%82%3C%2FP%3E%0A%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3E%E6%AD%A4%E8%87%B4%EF%BC%8C%3C%2FP%3E%0A%3CP%3ETomas%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-LABS%20id%3D%22lingo-labs-1126869%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CLINGO-LABEL%3E%E5%8A%A0%E9%80%9F%E5%BA%A6%E4%BC%A0%E6%84%9F%E5%99%A8%3C%2FLINGO-LABEL%3E%3C%2FLINGO-LABS%3E%3CLINGO-SUB%20id%3D%22lingo-sub-1126872%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%E5%9B%9E%E5%A4%8D%EF%BC%9AMMA8652FC%20-%20%E8%A3%B8%E6%9C%BA%E7%A4%BA%E4%BE%8B%E9%A1%B9%E7%9B%AE%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1126872%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%26lt%3Bmeta%20http-equiv%3D%22Content-Type%22%20content%3D%22text%2Fhtml%3B%20charset%3Dutf-8%22%20%2F%26gt%3B%0A%3CP%3EHello%20Tomas%2C%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E8%B0%A2%E8%B0%A2%E4%BD%A0%E7%9A%84%E5%B8%AE%E5%8A%A9%E3%80%82%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E6%AD%A4%E8%87%B4%EF%BC%8C%3C%2FP%3E%3CP%3ES%C3%A9rgio%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-1126871%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%E5%9B%9E%E5%A4%8D%EF%BC%9AMMA8652FC%20-%20%E8%A3%B8%E6%9C%BA%E7%A4%BA%E4%BE%8B%E9%A1%B9%E7%9B%AE%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1126871%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%26lt%3Bmeta%20http-equiv%3D%22Content-Type%22%20content%3D%22text%2Fhtml%3B%20charset%3Dutf-8%22%20%2F%26gt%3B%0A%3CDIV%20class%3D%22%22%3E%3CP%3EHello%20S%C3%A9rgio%2C%3C%2FP%3E%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%3CP%3E%E7%81%B5%E6%95%8F%E5%BA%A6_2G_8%E4%BD%8D%2064%3C%2FP%3E%3CP%3E%E7%81%B5%E6%95%8F%E5%BA%A6_4G_8%E4%BD%8D%2032%3C%2FP%3E%3CP%3E%E7%81%B5%E6%95%8F%E5%BA%A6_8G_8%E4%BD%8D%2016%3C%2FP%3E%3CBR%20%2F%3E%3CP%3E%C2%B12g%3A%3C%2FP%3E%3CP%3EX_offset_2G_8_bit%20%3D%20Xout_8_bit%20*%208%20*%20(-1)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%3CP%3EY_offset_2G_8_bit%20%3D%20Yout_8_bit%20*%208%20*%20(-1)%3B%3C%2FP%3E%3CP%3EZ_offset_2G_8_bit%20%3D%20(Zout_8_bit%20-%20SENSITIVITY_2G_8bits)%20*%208%20*%20(-1)%3B%3C%2FP%3E%3CBR%20%2F%3E%3CP%3E%C2%B14g%3A%3C%2FP%3E%3CP%3EX_offset_4G_8_bit%20%3D%20Xout_8_bit%20*%2016%20*%20(-1)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%3CP%3EY_offset_4G_8_bit%20%3D%20Yout_8_bit%20*%2016%20*%20(-1)%3B%3C%2FP%3E%3CP%3EZ_offset_4G_8_bit%20%3D%20(Zout_8_bit%20-%20SENSITIVITY_4G_8bits)%20*%2016%20*%20(-1)%3B%3C%2FP%3E%3CBR%20%2F%3E%3CP%3E%C2%B18g%3A%3C%2FP%3E%3CP%3EX_offset_8G_8_bit%20%3D%20Xout_8_bit%20*%2032%20*%20(-1)%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%3C%2FP%3E%3CP%3EY_offset_8G_8_bit%20%3D%20Yout_8_bit%20*%2032%20*%20(-1)%3B%3C%2FP%3E%3CP%3EZ_offset_8G_8_bit%20%3D%20(Zout_8_bit%20-%20SENSITIVITY_8G_8bits)%20*%2032%20*%20(-1)%3B%3C%2FP%3E%3CP%20style%3D%22min-height%3A%208pt%3B%20padding%3A%200px%3B%22%3E%26nbsp%3B%3C%2FP%3E%3CP%3E%E9%A1%BA%E7%A5%9D%E5%95%86%E7%A5%BA%EF%BC%81%3C%2FP%3E%3CP%3ETomas%3C%2FP%3E%3C%2FDIV%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-1126870%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%E5%9B%9E%E5%A4%8D%EF%BC%9AMMA8652FC%20-%20%E8%A3%B8%E6%9C%BA%E7%A4%BA%E4%BE%8B%E9%A1%B9%E7%9B%AE%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1126870%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%26lt%3Bmeta%20http-equiv%3D%22Content-Type%22%20content%3D%22text%2Fhtml%3B%20charset%3Dutf-8%22%20%2F%26gt%3B%0A%3CP%3EHello%20Tomas%2C%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E6%88%91%E5%8F%91%E7%8E%B0%E8%BF%99%E4%B8%AA%E9%A1%B9%E7%9B%AE%E9%9D%9E%E5%B8%B8%E6%9C%89%E7%94%A8%EF%BC%8C%E6%88%91%E6%8C%89%E7%85%A7%E5%AE%83%E6%9D%A5%E9%85%8D%E7%BD%AE%E6%88%91%E7%9A%84%20MMA8652FC%E3%80%82%3C%2FP%3E%3CP%3E%E4%BD%86%E6%88%91%E5%8F%AA%E6%83%B3%E4%BD%BF%E7%94%A8%208%20%E4%BD%8D%E6%9D%A5%E5%A4%84%E7%90%86%E5%AE%83%E3%80%82%3C%2FP%3E%3CP%3E%E6%88%91%E5%8F%AF%E4%BB%A5%E5%B0%86%E5%85%B6%E9%85%8D%E7%BD%AE%E4%B8%BA%E4%BB%85%E4%BD%BF%E7%94%A8%208%20%E4%BD%8D%EF%BC%8C%E5%B9%B6%E4%B8%94%E6%88%91%E5%BE%97%E5%88%B0%E4%BA%86%20Xout_8_bit%E3%80%81Yout_8_bit%20%E5%92%8C%20Zout_8_bit%E3%80%82%E4%BD%86%E6%98%AF%E6%88%91%E5%A6%82%E4%BD%95%E8%AE%A1%E7%AE%97%E5%81%8F%E7%A7%BB%E5%80%BC%EF%BC%9F%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EX_%E5%81%8F%E7%A7%BB_8_%E4%BD%8D%3D%3C%2FSPAN%3E%20%EF%BC%9F%3C%2FP%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EY_%E5%81%8F%E7%A7%BB_8_%E4%BD%8D%3D%3C%2FSPAN%3E%20%EF%BC%9F%3C%2FP%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EZ_offset_8_bit%20%3D%3C%2FSPAN%3E%20%3F%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E4%BD%A0%E8%83%BD%E5%B8%AE%E5%8A%A9%E6%88%91%E5%90%97%EF%BC%9F%3C%2FP%3E%3CP%3E%E8%B0%A2%E8%B0%A2%E3%80%82%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E6%AD%A4%E8%87%B4%EF%BC%8C%3C%2FP%3E%3CP%3ES%C3%A9rgio%3C%2FP%3E%3C%2FLINGO-BODY%3E
无评分
版本历史
最后更新:
‎02-03-2026 05:19 PM
更新人: