We plan to upgrade SPSDK to 2.0 in the next release which includes a large scale of changes. Customers are suggested to prepare for the changes before the 2.0 release (end of Sept 2023). Major changes in 2.0 are:
- elftosb will be replaced by nxpimage
- nxpcertgen and nxpkeygen will be replaced by nxpcrypto
- select appropriate family will be done using: -f/–family parameter
- move towards options for all parameters with an exception to BLHost
- removal of crypto backends
- extend dedicated spsdk.crypto module - serve as the de-facto backend of SPSDK
- module level imports via init files