Changes in Secure Provisioning SDK 2.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Changes in Secure Provisioning SDK 2.0

Changes in Secure Provisioning SDK 2.0

We plan to upgrade SPSDK to 2.0 in the next release which includes a large scale of changes.  Customers are suggested to prepare for the changes before the 2.0 release (end of Sept 2023).  Major changes in 2.0 are:

  • elftosb will be replaced by nxpimage
  • nxpcertgen and nxpkeygen will be replaced by nxpcrypto
  • select appropriate family will be done using: -f/–family parameter
  • move towards options for all parameters with an exception to BLHost
  • removal of crypto backends
  • extend dedicated spsdk.crypto module - serve as the de-facto backend of SPSDK
  • module level imports via init files
ラベル(1)
評価なし
バージョン履歴
最終更新日:
‎08-08-2023 04:32 PM
更新者: