What security feature differences btw SE050 and TPM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What security feature differences btw SE050 and TPM

3,020 Views
nxa00071
NXP Employee
NXP Employee

I would like to know the security point of veiw on SE050 compared to TPM.

What kind of seucurity feature is SE050 superior than TPM? Need more tamper security features. 

2 Replies

2,776 Views
harvey_chang
Contributor I

Another TPM question, could we use SE050 to do software attestation just like TPM using its PCR to do measure boot and software attestation?

0 Kudos
Reply

2,776 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi 

For the TPM and SE050 difference, as I know, SE050 provides main TPM function, so actually it can be used as a TPM but depends on the use case, for example, for the case of secure boot. SE050 also offers many additional features can be used for use cases in which other TPM products can not be adapted.

Have  a great day !

BR

Jonathan