SE050F2 as Smart card interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SE050F2 as Smart card interface

Jump to solution
3,118 Views
hitesh_gambhava
Contributor I

Hi NXP team,

I have a query with SE050F2 secure element. Can it work as smart card over I2C interface or it is must to use ISO 7816 to get this functionality?

Thanks,

Hitesh

0 Kudos
Reply
1 Solution
3,094 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @hitesh_gambhava ,

 

Not sure what is the requirement meant when you specified "smart card interface". SE050F is a "smart card". It can receive commands using the interfaces I²C (using T1oI2C protocol), and ISO14443. When you place the NFC antenna over a contactless reader, it will be discovered as a smart card. The contact based ISO7816 interface is a classic smart card interface, but it does not matter of the commands are exchanges over contact, contactless or I2C interface. Over all interfaces the SE05x can be made recognized by an system as "smart card". E.g. for the I2C interface the K64F CCID example can be used which shows the connected SE05x as a smart card to a host system. Most likely your question is if the SE050F then supports the commands expected by the system, right? Please kindly clarify.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
3,078 Views
hitesh_gambhava
Contributor I

Hi Kan,

Thanks for the response. My question is more about as classic Smart card interface i.e. from PC/Laptop USB to K64F USB (over CCID) and K64F to SE050 over I2C interface. As per your response it looks this is possible. Please confirm.

Thanks,

Hitesh

0 Kudos
Reply
3,072 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @hitesh_gambhava ,

 

Yes, you may use either of the following CCID examples out of the MW for evaluation purpose.

Kan_Li_1-1697435820985.pngKan_Li_1-1697435820985.png

 

and after plugging into a Laptop, you will find the following notification.

Kan_Li_0-1697435774825.pngKan_Li_0-1697435774825.png

 

Regarding how to program the bin file into the K64F-FRDM board, please kindly refer to "3.3 Flash FRDM-K64F with VCOM software " in https://www.nxp.com.cn/docs/en/application-note/AN12398.pdf for details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
3,068 Views
hitesh_gambhava
Contributor I

Hi @Kan_Li ,

Thanks for the confirmation. Yes, this information will really help for further development.

Thanks,

Hitesh

0 Kudos
Reply
3,095 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @hitesh_gambhava ,

 

Not sure what is the requirement meant when you specified "smart card interface". SE050F is a "smart card". It can receive commands using the interfaces I²C (using T1oI2C protocol), and ISO14443. When you place the NFC antenna over a contactless reader, it will be discovered as a smart card. The contact based ISO7816 interface is a classic smart card interface, but it does not matter of the commands are exchanges over contact, contactless or I2C interface. Over all interfaces the SE05x can be made recognized by an system as "smart card". E.g. for the I2C interface the K64F CCID example can be used which shows the connected SE05x as a smart card to a host system. Most likely your question is if the SE050F then supports the commands expected by the system, right? Please kindly clarify.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply