SE050 memory writes, wear leveling?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SE050 memory writes, wear leveling?

跳至解决方案
2,336 次查看
deang
Contributor III

Per the datasheet, the SE050 memory reliability is "100 Mio write cycles/25 years".  

What does "Mio" mean?  Is this short for Million?

Also, does the se050 implement any kind of wear leveling?

 

Thanks,

Dean

0 项奖励
回复
1 解答
2,273 次查看
deang
Contributor III

 @Kan_Li Thanks for the clarification.

Dean

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,279 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @deang ,

 

Yes, it is short for Million, and  SE05x implements automatic wear leveling. This is why in the datasheet we only specify one global write endurance, as we are spreading writes automatically over the whole flash of the SE.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
2,273 次查看
deang
Contributor III

 @Kan_Li Thanks for the clarification.

Dean

 

0 项奖励
回复