SE050ARD-E with Raspberry Pi - SCP03

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SE050ARD-E with Raspberry Pi - SCP03

跳至解决方案
3,678 次查看
psvz
Contributor IV

Following https://www.nxp.com/docs/en/application-note/AN12570.pdf

Para 5.3: with ccmake . I have out of the box:

PTMW_SCP SCP03_SSS
PTMW_SE05X_Auth None

It won't let me change None -> PlatfSCP03 saying:

accessManager is not copied to default binary directory upon install

What do I do to make it work?

Following paragraph 5.2.2 this seems false:

EdgeLock SE Plug & Trust Middleware will first look for the default path
/tmp/SE05X/plain_scp.txt, if it is not able to find the file, it will try to use the
environment variable EX_SSS_BOOT_SCP03_PATH, and lastly, it will fall back to pre-compiled keys.

I exported EX_SSS_BOOT_SCP03_PATH and Figure 29 won't appear - instead, it still says

sss :WARN :Communication channel is Plain.

Is this expected?

标签 (1)
0 项奖励
回复
1 解答
3,669 次查看
michaelsalfer
NXP Employee
NXP Employee

Hello,

this (accessManager is not copied to default binary directory upon install) is only a message to make you aware that the binary will not be copied. 

Did you after the "c"onfigure step as well do the "g"enerate step?

If PTMW_SE05X_Auth is set to any authentication value then the common example startup code will always execute the authentication - if it fails, then the example will not be started (sss_entry() will not be called). 

Kind regards,
Michael

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,670 次查看
michaelsalfer
NXP Employee
NXP Employee

Hello,

this (accessManager is not copied to default binary directory upon install) is only a message to make you aware that the binary will not be copied. 

Did you after the "c"onfigure step as well do the "g"enerate step?

If PTMW_SE05X_Auth is set to any authentication value then the common example startup code will always execute the authentication - if it fails, then the example will not be started (sss_entry() will not be called). 

Kind regards,
Michael

0 项奖励
回复
3,660 次查看
psvz
Contributor IV

@michaelsalfer Although se05x_Minimal now behaves as expected i.e.,

App :INFO :Using default PlatfSCP03 keys.

I have similar problem with ssscli still:

ssscli se05x uid

sss :WARN :Communication channel is Plain.

I have built ssscli in letter with para 9.3.1.3 of the docs. How do I make ssscli use SCP03, please?

标记 (1)
0 项奖励
回复
3,664 次查看
psvz
Contributor IV

@michaelsalfer I think I have figured it out. Sorry - I never used ccmak before. I expected option list when I pressed "c" - and "Enter" is actually what making the change. All Sorted!

0 项奖励
回复
3,667 次查看
psvz
Contributor IV
Hi Michael
I didn't do 'g' step because I do not know how to change None -> PlatfSCP03 in ccmake before the 'g' step. What do I miss?
0 项奖励
回复