SE050ARD Antenna Design/Specification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SE050ARD Antenna Design/Specification

2,496 Views
davidward
Contributor I

Regarding AN12395OM-SE050ARD hardware overview the application schematic says, "Route Antenna as shown in reference design".

However the reference design is not included in the documents that can be downloaded from NxP's website. Where can I obtain the reference design or a specification for the antenna design?

Labels (1)
0 Kudos
Reply
2 Replies

2,394 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi David,

I think the reference design in the AN might just mean the board, but anyway , what are you looking for indeed? Gerber File of OM-SE050ARD? Please kindly clarify. I may help to check if it is available.

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,394 Views
jgutierrez1
Contributor I

Hello,

I am also looking for the schematic and pcb design: EDA project or gerbers. I think that it is very important for antenna design.

Julen

0 Kudos
Reply