SE050 using Energy Harvesting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SE050 using Energy Harvesting

2,365件の閲覧回数
nandanito
Contributor I

We are planning to connect SE050 as I2C Slave by using NTAG 5 Boost (passive mode) as I2C Master. Can NFC Readers like mobile phones, such as iPhone 11, induce enough power to make SE050 operational, if SE were to be used for specific cryptographic operations (without sensor, of course)?

Thanks!

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

2,264件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Actually SE050 supports ISO14443/NFC interface, no need to use NTAG 5 family to act as a bridge. If you have SE050ARD demo board, you may configure it as below to enable the CL interface.

pastedImage_1.png

What is the scenario for your application? what kind of cryptographic operations do you want to use based on SE050? Would you please clarify?

Thanks for your patience!

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信