SE050 feature support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SE050 feature support

3,411件の閲覧回数
muneeswaran_r
Contributor II

Can SE050 supports TPM2.0 specification?

#Security

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,299件の閲覧回数
muneeswaran_r
Contributor II

Hi Kan,

Thanks for your Answer.

But I don't see anything related to TPM feature in SE050 datasheet.

Can you share any link if anything available regarding TPM2.0 and SE050 for reference purpose?

0 件の賞賛
返信

3,299件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Muneeswaran R,

SE050 provides PCR secure object for TPM functions. Please kindly refer to "3.2.1.8 PCR" in the following for details.

https://www.nxp.com/docs/en/application-note/AN12413-SE050_APDU_specification.pdf 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

3,299件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

SE050 comes with main TPM functionality required for IoT Security and offers many additional features.

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信