SE050 ed25519 (EdDSA) example code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SE050 ed25519 (EdDSA) example code

Jump to solution
4,421 Views
ethanlooney
Contributor II

Hi, 

Is there any available example code that deals with EdDSA? I am unable to find much in reference to this in the documentation or examples.

Thanks,

Ethan

Labels (1)
1 Solution
4,386 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @ethanlooney ,

 

There is no example available for EdDSA, but the best demo as base for EdDSA is ex_ecc. Please kindly refer to the attachment for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
4,387 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @ethanlooney ,

 

There is no example available for EdDSA, but the best demo as base for EdDSA is ex_ecc. Please kindly refer to the attachment for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply