SE050 change default I2C address

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SE050 change default I2C address

ソリューションへジャンプ
3,096件の閲覧回数
atc024
Contributor I

Hi,
The default slave address of the SE050 is configured to 0x48. How it can be changed?
Regards, Tomek

ラベル(1)
0 件の賞賛
返信
1 解決策
3,088件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @atc024 ,

 

No, SE050 doesn't support this, but it is possible with SE051, please kindly refer to https://www.nxp.com/webapp/Download?colCode=AN13015 for details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,089件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @atc024 ,

 

No, SE050 doesn't support this, but it is possible with SE051, please kindly refer to https://www.nxp.com/webapp/Download?colCode=AN13015 for details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信