SE050 change default I2C address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SE050 change default I2C address

Jump to solution
3,095 Views
atc024
Contributor I

Hi,
The default slave address of the SE050 is configured to 0x48. How it can be changed?
Regards, Tomek

Labels (1)
0 Kudos
Reply
1 Solution
3,087 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @atc024 ,

 

No, SE050 doesn't support this, but it is possible with SE051, please kindly refer to https://www.nxp.com/webapp/Download?colCode=AN13015 for details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
3,088 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @atc024 ,

 

No, SE050 doesn't support this, but it is possible with SE051, please kindly refer to https://www.nxp.com/webapp/Download?colCode=AN13015 for details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply