SE050 RSA Performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SE050 RSA Performance

5,635 Views
klaus_mueller
Contributor I

Hi,

i am working with SE050 Arduino kit connected to Raspberry Pi. In my setup the ECC sign and verify commands are very fast. But if I use RSA 2k keys, I experience in my setup roughly 4 seconds for RSA sign and roughly 4 seconds for RSA verify. Is this an expected performance range or might there be an issue on my side?

Thanks

Labels (1)
0 Kudos
Reply
6 Replies

5,239 Views
klaus_mueller
Contributor I

Hi, 

one short adder to my previous description. I have realized that RSA verify takes in majority cases roughly 4s, but in few cases (e.g. previous log) much less e.g. 760ms.. 

Thanks.

0 Kudos
Reply

5,239 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

Thanks for the information! I will try it on my side.

BTW, I didn't see and time measurement info from the log, so how did you measure the time? Please kindly clarify.

Thanks for your patience!

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

5,239 Views
klaus_mueller
Contributor I

Hi,

within above log RSA sign was 4282ms and verify was 761ms. Please look for the line starting with msec time. 

RSA sign is very stable in the area of 4282. The RSA verify is either 761ms (in roughly 1/4 cases) or roughly 4000ms (in roughly 3/4 cases).

Please see how I measured:

I have patched the file ex_sss_rsa.c in function ex_sss_entry(…).

On top of the file I have included time.h. I get the time (in ns) before and after the function call

To “sss_asymmetric_sign_digest”. I calculate the time difference and print it.

 

#include <time.h>

 

Long int start_time;

Long int time_difference;   

Struct timespec gettime_now;

 ...

   clock_gettime(CLOCK_REALTIME, &gettime_now);

    start_time = gettime_now.tv_nsec;

 

    status = sss_asymmetric_sign_digest(&ctx_asymm, digest, digestLen, signature, &signatureLen);

 

    clock_gettime(CLOCK_REALTIME, &gettime_now);

    time_difference = gettime_now.tv_nsec - start_time;

    printf("nsec time is %lu\n", time_difference);

    printf("msec time is %f\n", (float)(((unsigned long int)time_difference)/1000000));

...

0 Kudos
Reply

5,239 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Klaus Mueller,

I think the method you used for measure the timing is correct, but it also take other parts into calculation, for example, since you run the application in the linux, there were multiple tasks run at the same time, so the context switching also consume some time, so I think better measure based on a nonOS situation, you know, we have also released SE050 FRDMK64 version hostlib, based on that you may get the correct RSA performance. Please refer to https://www.nxp.com/webapp/Download?colCode=SDK-FRDM-K64F-SE050 for details.

I use the LPTMR to measure the time and the result is as below:

pastedImage_2.png

Please note this result still take the I2C communication into calculation, so the real rsa performance should be shorter.

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

5,239 Views
klaus_mueller
Contributor I

Hi Kan,

I have been using the middleware package called  se050_mw_v02.10.02.zip ( md5sum: b713c482eb52a795061ba1b747044b07).

I included the example called "ex_sss_ecc.c" and "ex_sss_rsa.c" into the build ending up with the binaries called ex_ecc and ex_rsa which I can call from my shell on raspberry pi.

When measuring the execution time of the call "sss_asymetric_sign_digest" and "sss_asymetric_verify_digest" in ex_sss_ecc.c I can see values around 80ms. Applying the same principle to the calls in file "ex_sss_rsa.c" I end up with values around 4 seconds.

Below you can find the information of my SE050 when executing the example "se05x_Get_Info" and the output of “ex_rsa”.

 

       App:WARN :#####################################################

       App:INFO :Applet Major = 3

       App:INFO :Applet Minor = 1

       App:INFO :Applet patch = 0

       App:INFO :AppletConfig = 6FFF

       App:INFO :With    ECDAA

       App:INFO :With    ECDSA_ECDH_ECDHE

       App:INFO :With    EDDSA

       App:INFO :With    DH_MONT

       App:INFO :With    HMAC

       App:INFO :With    RSA_PLAIN

       App:INFO :With    RSA_CRT

       App:INFO :With    AES

       App:INFO :With    DES

       App:INFO :With    PBKDF

       App:INFO :With    TLS

       App:INFO :With    MIFARE

       App:INFO :With    I2CM

       App:INFO :SecureBox = 010B

       App:WARN :#####################################################

       App:INFO :Tag value - proprietary data 0xFE = 0xFE

       App:INFO :Length of following data 0x45 = 0x45

       App:INFO :Tag card identification data (Len=2)

                        DF 28

       App:INFO :Length of card identification data 0x46 = 0x42

       App:INFO :Tag configuration ID 0x01 = 0x01

       App:INFO :Length configuration ID 0x0C = 0x0C

       App:INFO :Configuration ID (Len=12)

                        00 04 A1 F4             45 88 4F 17             E5 19 C0 69

       App:INFO :OEF ID (Len=2)

                        A1 F4

       App:INFO :Tag patch ID 0x02 = 0x02

       App:INFO :Length patch ID 0x08 = 0x08

       App:INFO :Patch ID (Len=8)

                        00 00 00 00             00 00 00 01

       App:INFO :Tag platform build ID1 0x03 = 0x03

       App:INFO :Length platform build ID 0x18 = 0x18

       App:INFO :Platform build ID (Len=24)

                        4A 33 52 33             35 31 30 32             31 45 45 45             30 34 30 30

                        BC 03 04 79             33 8D 18 10

       App:INFO :JCOP Platform ID = J3R351021EEE0400

       App:INFO :Tag FIPS mode 0x05 = 0x05

       App:INFO :Length FIPS mode 0x01 = 0x01

       App:INFO :FIPS mode var = 0x00

       App:INFO :Tag pre-perso state 0x07 = 0x07

       App:INFO :Length pre-perso state 0x01 = 0x01

       App:INFO :Bit mask of pre-perso state var = 0x00

       App:INFO :Tag ROM ID 0x08 = 0x08

       App:INFO :Length ROM ID 0x08 = 0x08

       App:INFO :ROM ID (Len=8)

                        2E 5A D8 84             09 C9 BA DB

       App:INFO :Status Word (SW) (Len=2)

                        90 00

       App:INFO :ex_sss Finished

                  

ex_rsa

 

       App:INFO :PlugAndTrust_v02.10.02_20190809

       App:INFO :Running ./ex_rsa

       App:INFO :If you want to over-ride the selection, use ENV=EX_SSS_BOOT_SSS_PORT or pass in command line arguments.

       sss:INFO :atr (Len=35)

                        00 A0 00 00             03 96 04 03             E8 00 FE 02             0B 03 E8 08

                        01 00 00 00             00 64 00 00             0A 4A 43 4F             50 34 20 41

                        54 50 4F

       sss:WARN :Communication channel is Plain.

       sss:WARN :!!!Not recommended for production use.!!!

       App:INFO :Running RSA Example ex_sss_rsa.c

       App:INFO :Do Signing

       App:INFO :digest (Len=32)

                        00 01 02 03             04 05 06 07             08 09 0A 0B             0C 0D 0E 0F

                        10 11 12 13             14 15 16 17             18 19 1A 1B             1C 1D 1E 1F

msec time is 4282.000000

       App:INFO :Signing successful !!!

       App:INFO :signature (Len=256)

                        7F D3 4E A2             2F F7 BE B9             DC 73 F0 60             F5 B8 16 1C

                        27 B7 A6 38             D1 67 C1 6A             1D D0 5D 9F             5E 16 C0 E8

                        DE 36 F1 45             6C 45 0A C1             63 21 A0 B2             0E 94 ED B4

                        65 5F 9D 2E             5F 65 47 18             1B CB 10 41             87 BD 5B 6F

                        9E 13 B4 3A             44 A3 67 B5             46 9E 97 84             88 C1 F7 5C

                        2F AE B8 91             53 2B D2 84             6B 8E 9B B9             6E F3 B5 AE

                        51 50 16 DB             16 A3 1A 1C             93 D1 F6 C4             C6 CB 1F 83

                        0E 31 E2 39             19 3E F0 E5             B9 B3 9A D8             CF BE 93 4A

                        7B 53 83 1F             62 DB A8 50             F2 4D 0D AF             8F 8C D6 57

                        3B 9C C3 34             DF E6 BC E1             31 6A 98 87             62 54 53 12

                        5C 1F 21 B5             12 B3 04 89             4D A7 4B 83             97 E7 9D 50

                        2D 91 F8 0C             29 73 38 B8             62 2B BC B0             F1 F6 F2 A2

                        BF E5 BE 41             91 EF D9 52             BA BC 0F D8             3E 11 ED 90

                        47 E0 D5 0C             ED 84 EF 75             F0 96 3B B0             32 97 AA 84

                        B0 FF 25 0A             CB A2 8C D4             0D 0F F7 5F             BC 1A 8B 87

                        AE 4E F8 42             3C E1 FE 44             B1 E0 52 66             E1 D0 A3 64

       App:INFO :Do Verification

msec time is 761.000000

       App:INFO :Verification successful !!!

       App:INFO :ex_sss_RSA Example Success !!!...

       App:INFO :ex_sss Finished

0 Kudos
Reply

5,239 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

Do you have the test log? I will try to reproduce this issue here.

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply