SE050 Dev Board - Communication via NFC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SE050 Dev Board - Communication via NFC

3,162件の閲覧回数
julian_sauer
Contributor III

Can the SE050 Dev Board be tested via NFC. We want to communicate with the SE050 via a Android Smartphone via NFC.

Is this possible?

3 返答(返信)

3,072件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Yes, the Dev Board supports NFC interface via J6 and J7 jumper settings. Please kindly refer to the following for details.

pastedImage_1.png

pastedImage_2.png

 but to communicate with the SE050 via a Android Smartphone, you have to build a custom App to issue the SE050 APDU commands. 

Please kindly refer to https://www.nxp.com/docs/en/application-note/AN12413-SE050_APDU_specification.pdf  and https://www.nxp.com/docs/en/user-guide/UM11225.pdf  for more details.

Hope that helps,

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,647件の閲覧回数
albertobattistello
Contributor II

Hi,

I am using a OM-SE050ARD,

I have set jumper J6 to 2-3 and J7 to 2-3.

I have installed the NXP TagInfo app version 4.25.4 on my Samsung smartphone (which can read other NFC tags).

However, when approaching the OM-SE050ARD antenna to the phone, nothing happens. Is this a problem with the smartphone app not sending the APDUS or do I need to program something into the SE050?

Best regards,

Alberto

0 件の賞賛
返信

2,645件の閲覧回数
albertobattistello
Contributor II

Ok,

by following the information on https://www.nxp.com/docs/en/application-note/AN12395.pdf, Section 4.4.1, I was able to read the OM-SE050ARD.

It reads it as unknown IC with OS Javacard.

Best Regards,

Alberto

0 件の賞賛
返信