ReadObject can't read binary file in sessionless access PnT nano

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ReadObject can't read binary file in sessionless access PnT nano

跳至解决方案
1,297 次查看
Jansch
Contributor II

How to I allow my ReadObject command to output a binary file while in sessionless access? I am just receiving 0's when checking for content, instead of the actual content. Maybe I have to set policies differently when writing the binary file? I thought default policies enable all access.

标签 (1)
0 项奖励
回复
1 解答
1,219 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Jansch ,

 

Please kindly refer to https://github.com/NXPPlugNTrust/nano-package/blob/ccd5782c1acc855b4bee7be9de6a1d6c9416e7e0/examples... for details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
1,246 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Jansch ,

 

The demo in simw-top\demos\se05x\se05x_GetCertificate shows how to use SSS APIs to get a certificate in the SE, you may use it as a reference.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,235 次查看
Jansch
Contributor II
Thank you very much for your answer Kan!

Is there an example on how to do this with the nano mw aswell, which doesn't have the SSS API?

Best wishes

Jansch
0 项奖励
回复
1,220 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Jansch ,

 

Please kindly refer to https://github.com/NXPPlugNTrust/nano-package/blob/ccd5782c1acc855b4bee7be9de6a1d6c9416e7e0/examples... for details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------