Plug&Trust Nano Package compatible with SE050C2 config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Plug&Trust Nano Package compatible with SE050C2 config

Jump to solution
2,668 Views
deang
Contributor III

I'm working with the Plug&Trust nano package running on Zephyr.  Unfortunately the SCP keys defined in app note AN12436 for the C2 config (0xA200) do not seem to work.  I'm unable to create a secure channel.  Triple checked everything, nothing obvioius.

Question:  Are there any know issues or compatibility issues w/the Nano package and an SE050C2 config?

Thanks,

Dean

0 Kudos
Reply
1 Solution
2,637 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @deang ,

 

Thanks for the info! Actually the key pair you are using is for SE050C2(A201), not C1(A200), Please kindly refer to the following for details.

Kan_Li_0-1684318682829.png

 

There is a typo in table 6 of SE050 configurations (nxp.com) and we will update it later.

 

Sorry for the confusion that has caused.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

View solution in original post

0 Kudos
Reply
4 Replies
2,653 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @deang ,

 

May I have your SCP03 key definition similar as below?

Kan_Li_0-1684214995395.png

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply
2,644 Views
deang
Contributor III

deang_0-1684247929831.png

Keys I'm using.

0 Kudos
Reply
2,638 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @deang ,

 

Thanks for the info! Actually the key pair you are using is for SE050C2(A201), not C1(A200), Please kindly refer to the following for details.

Kan_Li_0-1684318682829.png

 

There is a typo in table 6 of SE050 configurations (nxp.com) and we will update it later.

 

Sorry for the confusion that has caused.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply
2,634 Views
deang
Contributor III

Thanks Kan, that fixed the problem!  

I can now connect using SCP03.

Dean

0 Kudos
Reply