Platform SCP keys

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,759件の閲覧回数
bboozzoo
Contributor I

Maybe I missed that in the documentation, but when the SCP keys are rotated using SCPInitializeUpdate as described in GlobalPlatform Technology Secure Channel Protocol '03' Card Specification v2.3 – Amendment D, do the the Platform SCP keys listed in AN12436 for the specific chip become invalid and it is no longer possible to establish SCP using those keys?

0 件の賞賛
返信
1 解決策
2,752件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @bboozzoo ,

 

Yes, after rotation, the Platform SCP03 keys used during initial authentication will be replaced with the new keys, but if you save the old keys somewhere, it is also possible to rotate them back.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,753件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @bboozzoo ,

 

Yes, after rotation, the Platform SCP03 keys used during initial authentication will be replaced with the new keys, but if you save the old keys somewhere, it is also possible to rotate them back.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 件の賞賛
返信