Platform SCP keys

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Platform SCP keys

跳至解决方案
1,767 次查看
bboozzoo
Contributor I

Maybe I missed that in the documentation, but when the SCP keys are rotated using SCPInitializeUpdate as described in GlobalPlatform Technology Secure Channel Protocol '03' Card Specification v2.3 – Amendment D, do the the Platform SCP keys listed in AN12436 for the specific chip become invalid and it is no longer possible to establish SCP using those keys?

0 项奖励
回复
1 解答
1,760 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @bboozzoo ,

 

Yes, after rotation, the Platform SCP03 keys used during initial authentication will be replaced with the new keys, but if you save the old keys somewhere, it is also possible to rotate them back.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,761 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @bboozzoo ,

 

Yes, after rotation, the Platform SCP03 keys used during initial authentication will be replaced with the new keys, but if you save the old keys somewhere, it is also possible to rotate them back.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 项奖励
回复