OM-SE050ARD with STM32 with NXP PlugNTrust nano-package

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OM-SE050ARD with STM32 with NXP PlugNTrust nano-package

847 次查看
Alon1
Contributor I

Hello,

we are running the nano-package on stm32, we run 2 examples

  • se05x_GetInfo
  • se05x_crypto

we are getting this kind of output, please help to understand the warning and failures

sw_status = Se05x_API_GetVersion(session_ctx, applet_version, &applet_versionLen);

i'm getting: sw_status = SM_ERR_CONDITIONS_OF_USE_NOT_SATISFIED

 

this is the output:

 

Se05x Getinfo Example !
Plug and Trust nano package - version: 1.3.0
No SemsLite Applet Available.
Plug and Trust nano package - version: 1.3.0
Failed Se05x_API_CheckObjectExists
Failed Se05x_API_GetVersion sw_status 0x6985

Applet Major = 3
Applet Minor = 1
Applet patch = 0
AppletConfig = 6FFF
With ECDSA_ECDH_ECDHE
With EDDSA
With DH_MONT
With HMAC
With RSA_PLAIN
With RSA_CRT
With AES
With DES
With PBKDF
With TLS
With MIFARE
With I2CM
#####################################################
Tag value - proprietary data 0xFE = 0xFE
Length of following data 0x45 = 0x45
Length of card identification data = 0x42
Tag configuration ID (Must be 0x01) = 0x01
OEF ID = 0xA1 0xF4
Tag patch ID (Must be 0x02) = 0x02
Tag platform build ID1 (Must be 0x03) = 0x03
JCOP Platform ID = J3R351021EEE0400
Tag FIPS mode (Must be 0x05) = 0x05
FIPS mode var = 0x00
Tag pre-perso state (Must be 0x07) = 0x07
Bit mask of pre-perso state var = 0x00
Tag ROM ID (Must be 0x08) = 0x08
se05x_GetInfoPlainApplet Example Success !!!...

SE05x Getinfo Example Success !
Se05x crypto Example !
Plug and Trust nano package - version: 1.3.0
Get Version ==>
Error in Se05x_API_GetVersion
ex_get_version, FAILED
Error in Se05x_API_CheckObjectExists
ex_generate_nist256_key, FAILED
Error in Se05x_API_CheckObjectExists
ex_set_get_nist256_key, FAILED
Error in Se05x_API_CheckObjectExists
ex_nist256_sign_verify, FAILED
Error in Se05x_API_CheckObjectExists
ex_set_certificate, FAILED
Error in Se05x_API_CheckObjectExists
ex_ecdh, FAILED
Error in Se05x_API_WriteSymmKey
ex_aes_ECB_NOPAD, FAILED
Error in Se05x_API_WriteSymmKey
ex_aes_CBC_NOPAD, FAILED
Error in Se05x_API_WriteSymmKey
ex_aes_CTR, FAILED
Error in Se05x_API_CheckObjectExists
ex_nist256_sign_policy, FAILED
SE05x crypto Example Success !

0 项奖励
回复
1 回复

811 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Alon1 ,

 

I just replied your ticket on the same topic in the tech support center, Please kindly check it there.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------