JCOP modules installation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JCOP modules installation

5,702 Views
liran_bh
Contributor I

hi

i installed all jcop tools , activated it , its all working great

but

during the installation process the manual refers to additional jcop modules to install 

I cant find the files. all files should be zip files with name starting with jcopx-api-module

where can i find it?

the guide is "getting started with jcop tools" chapter 6.1

thanks

liran

0 Kudos
Reply
4 Replies

5,625 Views
liran_bh
Contributor I

any idea?

0 Kudos
Reply

5,575 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @liran_bh ,

 

I am checking with the expert regarding your questions, and will let you know when I have any feedback from there.

Thanks for your patience!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

5,688 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @liran_bh ,

 

May I have the version of JCOP you are working with? Is there any snapshot regarding the issue you had during the installation? Thanks for your patience! 

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

5,668 Views
liran_bh
Contributor I

hi

i asked for jcop4 - im not sure that this is the version i got from docstore

the version of the tools is: JCOP-Tools-v53204_RC1

on the installation guide i see a section to install modules (attached screenshot of the files dialog from the manual)

files.jpg

i cant find those modules 

while starting a new project i can use only classic java card packages (attached new project dialog)

Capture.PNG

 

thanks

liran

0 Kudos
Reply