I would like to use ISO7816 interface in SE050

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I would like to use ISO7816 interface in SE050

跳至解决方案
2,717 次查看
masa_m
Contributor I

Dear NXP support team,

I would like to use ISO7816 interface in SE050.

(i) Can the following environment use ISO7816 interface?
- EdgeLock® SE050 Development Kit
- SE050C2 chip

(ii) If answer of (i) is "yes", would you tell me what document should I refer to in order to use ISO7816 interface?

Best Regards,
Masahiro Marume

标签 (1)
0 项奖励
回复
1 解答
2,675 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @masa_m ,

 

Actually this kind of interface is just available with some custom type of SE050. You have to contact your local NXP Marketing/sales or local FAE for further help.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,693 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @masa_m ,

 

I am sorry, but this kind of interface is not supported in the following environment:

- EdgeLock® SE050 Development Kit
- SE050C2 chip

Only the following interfaces are available.

Kan_Li_0-1631771940515.png

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
2,687 次查看
masa_m
Contributor I

Hi Kan,

Thank you for your response.
Would you tell me which environment supports ISO7816 interface?

I found the following description in SE050 datasheet
So, I thought SE050 can use ISO7816 interface.

masa_m_0-1631773068999.png

masa_m_1-1631773093622.png

Regards,
Masahiro Marume

0 项奖励
回复
2,676 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @masa_m ,

 

Actually this kind of interface is just available with some custom type of SE050. You have to contact your local NXP Marketing/sales or local FAE for further help.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复