How to Integrate SE05x in a Dunfell Yocto Image?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to Integrate SE05x in a Dunfell Yocto Image?

1,024 次查看
shreyaschandran
Contributor I

Hello,

I have built a Yocto image based on the Dunfell release for a LoRaWAN gateway following the STMicroelectronics guides. Now, I need to integrate NXP’s SE05x Secure Element into this setup for enhanced security.

Could you provide guidance on the following:

  1. Yocto Layer & Recipe – Are there any existing meta-se05x layers or recipes compatible with Dunfell?
  2. Dependency Management – What additional libraries or dependencies are required for SE05x integration?
  3. Device Tree & Driver Support – How should I modify the device tree and enable the required kernel drivers?
  4. Software Stack – What middleware is recommended for SE05x in Yocto?
  5. Integration Steps – Any step-by-step guide, reference implementation, or example for integrating SE05x in a dunfell yocto image?

Any documentation links, example implementations, or insights would be highly appreciated.

Thanks!

0 项奖励
回复
1 回复

979 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @shreyaschandran ,

 

We provide a doc on this topic based on imx8 platform, please kindly refer to se05x_mw_v04.05.01/simw-top/doc/dev-platforms/platform_imx8_linux.html#platform-imx-linux for details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复