Hardware reset jumper on SE050ARD-E

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hardware reset jumper on SE050ARD-E

Jump to solution
1,886 Views
psvz
Contributor IV

Hi

Re OM-SE05xARD hardware overview (nxp.com) section 4.4

Could you please confirm what does "reset" mean? Does it erase any keys inside SE050? 

In configuration with Raspberry Pi - which pins I need to close on J12 to trigger reset - it is not clear from that document.

Thank you.

Labels (1)
0 Kudos
Reply
1 Solution
1,865 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @psvz ,

 

No, it doesn't erase any key in the SE050, this signal routes to the reset pin of ISO7816 interface, which is pin 14 of SE050. To connect OM-SE050ARD-E with a Raspberry Pi board, it would be much easier with a  OM-SE05xRPI board, or via wires as mentioned in https://www.nxp.com.cn/docs/en/application-note/AN12570.pdf . Please kindly refer to "2.1.2.1 Using the OM-SE05xRPI adapter board" or "2.1.2.2 Connecting the OM-SE05xARD with wires" for details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,866 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @psvz ,

 

No, it doesn't erase any key in the SE050, this signal routes to the reset pin of ISO7816 interface, which is pin 14 of SE050. To connect OM-SE050ARD-E with a Raspberry Pi board, it would be much easier with a  OM-SE05xRPI board, or via wires as mentioned in https://www.nxp.com.cn/docs/en/application-note/AN12570.pdf . Please kindly refer to "2.1.2.1 Using the OM-SE05xRPI adapter board" or "2.1.2.2 Connecting the OM-SE05xARD with wires" for details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply