Government/Military CAC compatibility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Government/Military CAC compatibility

2,333件の閲覧回数
kalimadragon
Contributor I

I'm in the military and trying to use a computer with US Government/Military CAC cards. 

My machine is currently configured with a PR5331C3HN/C370E

1. Is this reader compatible with a military ID card (CAC)

2. could I get an updated driver for this reader

3. if this reader is not compatible with military CAC is there another reader that is compatible with my machine. I'm currently working on a Panasonic toughbook CF33

Thank you in advance.

タグ(1)
0 件の賞賛
返信
1 返信

2,325件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @kalimadragon ,

 

Actually I have no idea about the RF protocol that the US Government/Military CAC cards supports, but PR5331C3HN supports the PCD mode for FeliCa (212 kbps and 424 kbps),ISO/IEC14443 Type A and B (from 106 kbps to 848 kbps), MIFARE (106 kbps), B' cards(106 kbps), picoPass tag (106 kbps) and Innovision Jewel cards (106 kbps), so if the cards follows either of the above standards, there should be no problem. and you may find all the materials for development in https://www.nxp.com/confidential/PR533_PSP_261713 .

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信