Government/Military CAC compatibility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Government/Military CAC compatibility

2,378 Views
kalimadragon
Contributor I

I'm in the military and trying to use a computer with US Government/Military CAC cards. 

My machine is currently configured with a PR5331C3HN/C370E

1. Is this reader compatible with a military ID card (CAC)

2. could I get an updated driver for this reader

3. if this reader is not compatible with military CAC is there another reader that is compatible with my machine. I'm currently working on a Panasonic toughbook CF33

Thank you in advance.

Tags (1)
0 Kudos
Reply
1 Reply

2,370 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @kalimadragon ,

 

Actually I have no idea about the RF protocol that the US Government/Military CAC cards supports, but PR5331C3HN supports the PCD mode for FeliCa (212 kbps and 424 kbps),ISO/IEC14443 Type A and B (from 106 kbps to 848 kbps), MIFARE (106 kbps), B' cards(106 kbps), picoPass tag (106 kbps) and Innovision Jewel cards (106 kbps), so if the cards follows either of the above standards, there should be no problem. and you may find all the materials for development in https://www.nxp.com/confidential/PR533_PSP_261713 .

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply