Generate RSA certificat inside the SE050

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generate RSA certificat inside the SE050

Jump to solution
3,305 Views
ninomedj
Contributor I

Hello,

I'm trying to generate RSA certificate after successfully generating RSA key pairs, and i'm using Openssl as my hostcrypto, but i run to this error:

 

App :INFO :PlugAndTrust_v04.01.01_20220112
App :INFO :Running ./generate_certificate
App :INFO :If you want to over-ride the selection, use ENV=EX_SSS_BOOT_SSS_PORT or pass in command line arguments.
App :INFO :Using default PlatfSCP03 keys. You can use keys from file using ENV=EX_SSS_BOOT_SCP03_PATH
sss :INFO :atr (Len=35)
00 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 08
01 00 00 00 00 64 00 00 0A 4A 43 4F 50 34 20 41
54 50 4F
App :INFO :sss_key_store_get_key status 5a5a5a5a
App :INFO :len = 729
sss :ERROR:Selected padding is not supported for RSA Sign in SE050
App :INFO :ex_sss Finished
App :ERROR:ex_sss_entry Failed
App :ERROR:!ERROR! ret != 0.

 

So my qst is: can we generate RSA certificate like we do with ECC.

 

Thank you.

0 Kudos
Reply
1 Solution
3,293 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @ninomedj ,

 

I am sorry, but so far this demo just supports signing with ECC.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
3,294 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @ninomedj ,

 

I am sorry, but so far this demo just supports signing with ECC.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply