Establishing I2C communication between STM32 Nucleo F030 and SE050

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Establishing I2C communication between STM32 Nucleo F030 and SE050

跳至解决方案
3,322 次查看
badhri_radhakri
Contributor II

Hey guys I'm using a STM32 Nucleo F030 board as my Host device and would like to communicate with the secure element SE050 using I2C protocol. Is there any example programs that I can go through for better understanding ? The user manual for SE05x I2C specs is the document I'm currently using. I would really appreciate if someone has any leads.

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
3,134 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

Yes, there is a middle ware for SE050 available, but so far this MW just supports NXP MCU&MPU products, you have to do the porting by yourself. We have a porting guide available , please refer to https://www.nxp.com/docs/en/application-note/AN12488-SE050_middleware_porting_guidelines.pdf  for details.

Hope that helps,

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
48 次查看
CureSaba
Contributor I

it seems link not working

its says not found

0 项奖励
回复
3,135 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

Yes, there is a middle ware for SE050 available, but so far this MW just supports NXP MCU&MPU products, you have to do the porting by yourself. We have a porting guide available , please refer to https://www.nxp.com/docs/en/application-note/AN12488-SE050_middleware_porting_guidelines.pdf  for details.

Hope that helps,

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------