Hi @Jamier ,
SSSCLI tool is built based on the MW which is configured for some specific SE05x device, so if you change the se05x device, you have to rebuild the MW to generate the proper sssapisw lib for that device, which is referenced by the ssscli tool. Reinstalling the image doesn't help with it at all.
Hope that makes sense,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------