Encrypted Key (KEK) injection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Encrypted Key (KEK) injection

ソリューションへジャンプ
2,906件の閲覧回数
psvz
Contributor IV

I couldn't find source code for function Se05x_API_WriteSymmKey()

Could you please confirm that key decryption and persistence is handled atomically inside SE050, so that decrypted key is never transmitted back to the host?

I can see from the source code that only symmetric keys can be injected with KEK. Could you please confirm requirements for KEK itself - is it only AES? DES? Could it be asymmetric? It would help if you had some example code...

Thank you.

 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,886件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @psvz ,

 

Please kindly refer to the following for details.

 

1/ where is the source code for function Se05x_API_WriteSymmKey()?

-Please refer to \simw-top\hostlib\hostLib\se05x_03_xx_xx\se05x_APDU_impl.h for details.

2/ when injecting with KEK (no examples available) - could you please confirm that key decryption and persistence is handled atomically inside SE050, so that decrypted key is never transmitted back to the host?

- Yes, they are handled automatically inside the SE.

3/ What type of key (AES, DES, RSA, EC) can SE050 use as KEK (not documented)?

-The key type is defined in https://www.rfc-editor.org/rfc/rfc3394 .

 

Please kindly refer to https://www.nxp.com/docs/en/application-note/AN12413.pdf for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,897件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @psvz ,

 

Are you going to inject a symmetric key for both Encryption and Decryption? If so , please kindly refer to the demo in "simw-top\sss\ex\symmetric\ex_sss_symmetric.c" for details.

 

For symmetric keys, read back is not possible.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,891件の閲覧回数
psvz
Contributor IV

@Kan_Li - the example simw-top\sss\ex\symmetric\ex_sss_symmetric.c does NOT use KEK, so it is not helpful. Let's discuss all the questions because it is a deal-breaker for me:

1/ where is the source code for function Se05x_API_WriteSymmKey()?

2/ when injecting with KEK (no examples available) - could you please confirm that key decryption and persistence is handled atomically inside SE050, so that decrypted key is never transmitted back to the host?

3/ What type of key (AES, DES, RSA, EC) can SE050 use as KEK (not documented)?

If you could please answer each question or point me out to NXP product folks who could help?

Thank you.

0 件の賞賛
返信
2,887件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @psvz ,

 

Please kindly refer to the following for details.

 

1/ where is the source code for function Se05x_API_WriteSymmKey()?

-Please refer to \simw-top\hostlib\hostLib\se05x_03_xx_xx\se05x_APDU_impl.h for details.

2/ when injecting with KEK (no examples available) - could you please confirm that key decryption and persistence is handled atomically inside SE050, so that decrypted key is never transmitted back to the host?

- Yes, they are handled automatically inside the SE.

3/ What type of key (AES, DES, RSA, EC) can SE050 use as KEK (not documented)?

-The key type is defined in https://www.rfc-editor.org/rfc/rfc3394 .

 

Please kindly refer to https://www.nxp.com/docs/en/application-note/AN12413.pdf for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,882件の閲覧回数
psvz
Contributor IV

@Kan_Li - Kan, this is very very VERY helpful!!! You've made my day - Thanks a lot!

0 件の賞賛
返信