ECDSA secp256k1 curve key pair can be stored in SE050

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ECDSA secp256k1 curve key pair can be stored in SE050

3,723件の閲覧回数
krsuresh
Contributor III

Hi Team,

I would like to know whether SE050 supports the following requirements,

1) The capability of storing ECDSA secp256k1 asymmetric key pairs
2) Signing messages with the private key of the asymmetric key pair

 
Thanks,
Sureshkumar R
ラベル(1)
0 件の賞賛
返信
8 返答(返信)

3,154件の閲覧回数
krsuresh
Contributor III

Hi @Kan_Li,

This sample code for the Plug and Trust middleware nano package se050_sign has been updated to support the curved type secp256k1 and it's been tested on OM-SEC050ARD-C2 Ardino board with no issues. When I test with the SE050-C1 secure chip, the same code fails.
The Se05x_API_WriteECKey returns "SM_ERR_CONDITIONS_OF_USE_NOT_SATISFIED" as an error code. Please let me know if I am missing anything.

 

Thanks,

Sureshkumar R

0 件の賞賛
返信

3,563件の閲覧回数
krsuresh
Contributor III

Hi @Kan_Li,

Thanks for the reply. 

According to the SE050 datasheet, it supports only ECC NIST (192 to 512 bit). Does my understanding make sense? 
 
As I have gone through the ex_sss_ecc.c code, it appears that it is used in the NISTP curve. 
In my operation, I am generating a secp256k1 key using BIP32 protocol and storing it in SE050 and doing a signature.
Se05x_API_WriteECKey allowed me to store the secp256 key into se050, but Se05x_API_ECDSASign returned an error during signature. 
When I am using NIST keys the same is getting success. 
 
Thanks,
Sureshkumar R
0 件の賞賛
返信

3,555件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @krsuresh ,

 

I am sorry, my bad! I forgot to mention that the key value used in this demo should also be updated according to the cipher type. When you change the kSSS_CipherType_EC_NIST_P to kSSS_CipherType_EC_NIST_K, please use the following key value instead.

const uint8_t keyPairData[] = { 
0x30,0x74,0x02,0x01,0x01,0x04,0x20,0xEB,0x27,0x3D,0xBE,0x73,0x6D,0xD5,0x47,0xC8,0xCF,0xD4,0xCE,0x91,0xCC,0x2F,0x48,0x60,0x1A,0x12,0x8D,0xB0,0x34,0xE6,0x14,0x35,0x95,0x35,0x5C,0xDD,0x0A,0x32,0x5A,0xA0,0x07,0x06,0x05,0x2B,0x81,0x04,0x00,0x0A,0xA1,0x44,0x03,0x42,0x00,0x04,0x18,0x6A,0x85,0x20,0x98,0xA0,0x35,0x3F,0x5D,0x93,0x05,0x61,0x75,0x9E,0xE4,0x7D,0xA0,0xD4,0x8C,0x56,0xA1,0x24,0x33,0x4C,0xD0,0x38,0xC5,0x0F,0x12,0x38,0x7B,0x57,0x38,0xC0,0x55,0xE9,0xF1,0x39,0x40,0x10,0x87,0xFF,0x3F,0x39,0x4E,0x65,0xC9,0xB0,0x34,0x9F,0xE7,0xDC,0xB9,0xE7,0x1B,0x31,0xB3,0x8E,0x54,0xB7,0xA1,0x23,0x36,0x42
};

const uint8_t extPubKeyData[] = { 0x30,0x56,0x30,0x10,0x06,0x07,0x2A,0x86,0x48,0xCE,0x3D,0x02,0x01,0x06,0x05,0x2B,0x81,0x04,0x00,0x0A,0x03,0x42,0x00,0x04,0x18,0x6A,0x85,0x20,0x98,0xA0,0x35,0x3F,0x5D,0x93,0x05,0x61,0x75,0x9E,0xE4,0x7D,0xA0,0xD4,0x8C,0x56,0xA1,0x24,0x33,0x4C,0xD0,0x38,0xC5,0x0F,0x12,0x38,0x7B,0x57,0x38,0xC0,0x55,0xE9,0xF1,0x39,0x40,0x10,0x87,0xFF,0x3F,0x39,0x4E,0x65,0xC9,0xB0,0x34,0x9F,0xE7,0xDC,0xB9,0xE7,0x1B,0x31,0xB3,0x8E,0x54,0xB7,0xA1,0x23,0x36,0x42
};

 

Please kindly refer to the following for more details.

smCom :DEBUG:Get ATR (Len=4)
00 00 00 00
smCom :DEBUG:pAtr (Len=39)
00 00 00 23 01 A0 00 00 03 96 04 03 E8 00 FE 02
0B 03 E8 00 01 00 00 00 00 64 13 88 0A 00 65 53
45 30 35 31 00 00 00
smCom :DEBUG:H> (Len=4)
01 00 00 16
smCom :DEBUG:Tx> (Len=22)
00 A4 04 00 10 A0 00 00 03 96 54 53 00 00 00 01
03 00 00 00 00 00
smCom :DEBUG:<H (Len=4)
01 00 00 09
smCom :DEBUG:<Rx (Len=9)
06 00 00 3F FF FF FF 90 00
smCom :INFO :selectResponseData (Len=7)
06 00 00 3F FF FF FF
sss :INFO :atr (Len=35)
01 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 00
01 00 00 00 00 64 13 88 0A 00 65 53 45 30 35 31
00 00 00
sss :WARN :Communication channel is Plain.
sss :WARN :!!!Not recommended for production use.!!!

APDU :DEBUG:ReadIDList []
APDU :DEBUG:kSE05x_TAG_1 [output offset] = 0x0
APDU :DEBUG:kSE05x_TAG_2 [filter] = 0xFF
smCom :DEBUG:H> (Len=4)
01 00 00 10
smCom :DEBUG:Tx> (Len=16)
80 02 00 25 00 00 07 41 02 00 00 42 01 FF 00 00
smCom :DEBUG:<H (Len=4)
01 00 00 A5
smCom :DEBUG:<Rx (Len=165)
41 01 01 42 82 00 9C EF 00 00 94 EF 00 00 74 7D
A0 00 04 7D A0 00 13 7D A0 00 03 7D A0 00 12 7D
A0 00 02 7F FF 02 0A 7D A0 00 11 7D A0 00 01 7F
FF 02 07 7F FF 02 05 F0 00 01 23 F0 00 01 21 F0
00 01 13 F0 00 01 11 F0 00 01 03 F0 00 01 01 F0
00 01 22 F0 00 01 20 F0 00 01 12 F0 00 01 10 F0
00 01 02 F0 00 01 00 F0 00 00 03 F0 00 00 01 F0
00 00 02 F0 00 00 00 F0 00 00 11 F0 00 00 10 F0
00 00 13 F0 00 00 12 F0 00 00 20 F0 00 33 94 7F
FF 02 0B 7F FF 02 04 7F FF 02 02 7F FF 02 01 7F
FF 02 06 90 00

APDU :DEBUG:DeleteSecureObject []
APDU :DEBUG:kSE05x_TAG_1 [object id] = 0xEF000094
smCom :DEBUG:H> (Len=4)
01 00 00 0B
smCom :DEBUG:Tx> (Len=11)
80 04 00 28 06 41 04 EF 00 00 94
smCom :DEBUG:<H (Len=4)
01 00 00 02
smCom :DEBUG:<Rx (Len=2)
90 00

APDU :DEBUG:DeleteSecureObject []
APDU :DEBUG:kSE05x_TAG_1 [object id] = 0xEF000074
smCom :DEBUG:H> (Len=4)
01 00 00 0B
smCom :DEBUG:Tx> (Len=11)
80 04 00 28 06 41 04 EF 00 00 74
smCom :DEBUG:<H (Len=4)
01 00 00 02
smCom :DEBUG:<Rx (Len=2)
90 00

APDU :DEBUG:ReadCryptoObjectList []
smCom :DEBUG:H> (Len=4)
01 00 00 05
smCom :DEBUG:Tx> (Len=5)
80 02 10 25 00
smCom :DEBUG:<H (Len=4)
01 00 00 06
smCom :DEBUG:<Rx (Len=6)
41 82 00 00 90 00
App :INFO :Running Elliptic Curve Cryptography Example ex_sss_ecc.c

APDU :DEBUG:CheckObjectExists []
APDU :DEBUG:kSE05x_TAG_1 [object id] = 0xEF000076
smCom :DEBUG:H> (Len=4)
01 00 00 0B
smCom :DEBUG:Tx> (Len=11)
80 04 00 27 06 41 04 EF 00 00 76
smCom :DEBUG:<H (Len=4)
01 00 00 05
smCom :DEBUG:<Rx (Len=5)
41 01 02 90 00
sss :DEBUG:sss_key_store_set_key(@EF000076, cipherType=kSSS_CipherType_EC_NIST_K, keyBitLen=256)

APDU :DEBUG:ReadECCurveList []
smCom :DEBUG:H> (Len=4)
01 00 00 05
smCom :DEBUG:Tx> (Len=5)
80 02 0B 25 00
smCom :DEBUG:<H (Len=4)
01 00 00 17
smCom :DEBUG:<Rx (Len=23)
41 82 00 11 02 01 02 01 02 01 01 01 01 01 01 01
01 01 01 02 01 90 00

APDU :DEBUG:CheckObjectExists []
APDU :DEBUG:kSE05x_TAG_1 [object id] = 0xEF000076
smCom :DEBUG:H> (Len=4)
01 00 00 0B
smCom :DEBUG:Tx> (Len=11)
80 04 00 27 06 41 04 EF 00 00 76
smCom :DEBUG:<H (Len=4)
01 00 00 05
smCom :DEBUG:<Rx (Len=5)
41 01 02 90 00

APDU :DEBUG:Se05x_API_WriteECKey_Ver []
APDU :INFO :Policy is NULL
APDU :DEBUG:kSE05x_TAG_MAX_ATTEMPTS [maxAttempt] = 0x0
APDU :DEBUG:kSE05x_TAG_1 [object id] = 0xEF000076
APDU :DEBUG:kSE05x_TAG_2 [curveID] = 0x10
APDU :DEBUG:kSE05x_TAG_3 [privKey] (Len=32)
EB 27 3D BE 73 6D D5 47 C8 CF D4 CE 91 CC 2F 48
60 1A 12 8D B0 34 E6 14 35 95 35 5C DD 0A 32 5A
APDU :DEBUG:kSE05x_TAG_4 [pubKey] (Len=65)
04 18 6A 85 20 98 A0 35 3F 5D 93 05 61 75 9E E4
7D A0 D4 8C 56 A1 24 33 4C D0 38 C5 0F 12 38 7B
57 38 C0 55 E9 F1 39 40 10 87 FF 3F 39 4E 65 C9
B0 34 9F E7 DC B9 E7 1B 31 B3 8E 54 B7 A1 23 36
42
APDU :DEBUG:kSE05x_TAG_11 [version] = 0x0
smCom :DEBUG:H> (Len=4)
01 00 00 79
smCom :DEBUG:Tx> (Len=121)
80 01 61 00 74 41 04 EF 00 00 76 42 01 10 43 20
EB 27 3D BE 73 6D D5 47 C8 CF D4 CE 91 CC 2F 48
60 1A 12 8D B0 34 E6 14 35 95 35 5C DD 0A 32 5A
44 41 04 18 6A 85 20 98 A0 35 3F 5D 93 05 61 75
9E E4 7D A0 D4 8C 56 A1 24 33 4C D0 38 C5 0F 12
38 7B 57 38 C0 55 E9 F1 39 40 10 87 FF 3F 39 4E
65 C9 B0 34 9F E7 DC B9 E7 1B 31 B3 8E 54 B7 A1
23 36 42 4B 04 00 00 00 00
smCom :DEBUG:<H (Len=4)
01 00 00 02
smCom :DEBUG:<Rx (Len=2)
90 00
App :INFO :Do Signing
App :INFO :digest (Len=32)
48 65 6C 6C 6F 20 57 6F 72 6C 64 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

APDU :DEBUG:ECDSASign []
APDU :DEBUG:kSE05x_TAG_1 [objectID] = 0xEF000076
APDU :DEBUG:kSE05x_TAG_2 [ecSignAlgo] = 0x21
APDU :DEBUG:kSE05x_TAG_3 [inputData] (Len=32)
48 65 6C 6C 6F 20 57 6F 72 6C 64 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
smCom :DEBUG:H> (Len=4)
01 00 00 30
smCom :DEBUG:Tx> (Len=48)
80 03 0C 09 2B 41 04 EF 00 00 76 42 01 21 43 20
48 65 6C 6C 6F 20 57 6F 72 6C 64 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
smCom :DEBUG:<H (Len=4)
01 00 00 4D
smCom :DEBUG:<Rx (Len=77)
41 82 00 47 30 45 02 20 7E A1 14 35 BF CA BE 3C
65 FB 91 23 4C E6 93 55 B2 5D 0B A4 F5 FC 15 F9
3C 1F B8 F2 BD 83 63 27 02 21 00 ED 0F 60 45 CD
2E 78 57 2C D9 F0 4F 51 45 E2 F5 F8 72 43 9E A1
7E 20 7E 55 C1 E1 3B 17 94 73 2D 90 00
App :INFO :signature (Len=71)
30 45 02 20 7E A1 14 35 BF CA BE 3C 65 FB 91 23
4C E6 93 55 B2 5D 0B A4 F5 FC 15 F9 3C 1F B8 F2
BD 83 63 27 02 21 00 ED 0F 60 45 CD 2E 78 57 2C
D9 F0 4F 51 45 E2 F5 F8 72 43 9E A1 7E 20 7E 55
C1 E1 3B 17 94 73 2D
App :INFO :Signing Successful !!!

APDU :DEBUG:CheckObjectExists []
APDU :DEBUG:kSE05x_TAG_1 [object id] = 0xEF000096
smCom :DEBUG:H> (Len=4)
01 00 00 0B
smCom :DEBUG:Tx> (Len=11)
80 04 00 27 06 41 04 EF 00 00 96
smCom :DEBUG:<H (Len=4)
01 00 00 05
smCom :DEBUG:<Rx (Len=5)
41 01 02 90 00
sss :DEBUG:sss_key_store_set_key(@EF000096, cipherType=kSSS_CipherType_EC_NIST_K, keyBitLen=256)

APDU :DEBUG:ReadECCurveList []
smCom :DEBUG:H> (Len=4)
01 00 00 05
smCom :DEBUG:Tx> (Len=5)
80 02 0B 25 00
smCom :DEBUG:<H (Len=4)
01 00 00 17
smCom :DEBUG:<Rx (Len=23)
41 82 00 11 02 01 02 01 02 01 01 01 01 01 01 01
01 01 01 02 01 90 00

APDU :DEBUG:CheckObjectExists []
APDU :DEBUG:kSE05x_TAG_1 [object id] = 0xEF000096
smCom :DEBUG:H> (Len=4)
01 00 00 0B
smCom :DEBUG:Tx> (Len=11)
80 04 00 27 06 41 04 EF 00 00 96
smCom :DEBUG:<H (Len=4)
01 00 00 05
smCom :DEBUG:<Rx (Len=5)
41 01 02 90 00

APDU :DEBUG:Se05x_API_WriteECKey_Ver []
APDU :INFO :Policy is NULL
APDU :DEBUG:kSE05x_TAG_MAX_ATTEMPTS [maxAttempt] = 0x0
APDU :DEBUG:kSE05x_TAG_1 [object id] = 0xEF000096
APDU :DEBUG:kSE05x_TAG_2 [curveID] = 0x10
APDU :DEBUG:kSE05x_TAG_3 [privKey] (Len=0)
APDU :DEBUG:kSE05x_TAG_4 [pubKey] (Len=65)
04 18 6A 85 20 98 A0 35 3F 5D 93 05 61 75 9E E4
7D A0 D4 8C 56 A1 24 33 4C D0 38 C5 0F 12 38 7B
57 38 C0 55 E9 F1 39 40 10 87 FF 3F 39 4E 65 C9
B0 34 9F E7 DC B9 E7 1B 31 B3 8E 54 B7 A1 23 36
42
APDU :DEBUG:kSE05x_TAG_11 [version] = 0x0
smCom :DEBUG:H> (Len=4)
01 00 00 57
smCom :DEBUG:Tx> (Len=87)
80 01 21 00 52 41 04 EF 00 00 96 42 01 10 44 41
04 18 6A 85 20 98 A0 35 3F 5D 93 05 61 75 9E E4
7D A0 D4 8C 56 A1 24 33 4C D0 38 C5 0F 12 38 7B
57 38 C0 55 E9 F1 39 40 10 87 FF 3F 39 4E 65 C9
B0 34 9F E7 DC B9 E7 1B 31 B3 8E 54 B7 A1 23 36
42 4B 04 00 00 00 00
smCom :DEBUG:<H (Len=4)
01 00 00 02
smCom :DEBUG:<Rx (Len=2)
90 00
App :INFO :Do Verify
App :INFO :digest (Len=32)
48 65 6C 6C 6F 20 57 6F 72 6C 64 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
App :INFO :signature (Len=71)
30 45 02 20 7E A1 14 35 BF CA BE 3C 65 FB 91 23
4C E6 93 55 B2 5D 0B A4 F5 FC 15 F9 3C 1F B8 F2
BD 83 63 27 02 21 00 ED 0F 60 45 CD 2E 78 57 2C
D9 F0 4F 51 45 E2 F5 F8 72 43 9E A1 7E 20 7E 55
C1 E1 3B 17 94 73 2D

APDU :DEBUG:ECDSAVerify []
APDU :DEBUG:kSE05x_TAG_1 [objectID] = 0xEF000096
APDU :DEBUG:kSE05x_TAG_2 [ecSignAlgo] = 0x21
APDU :DEBUG:kSE05x_TAG_3 [inputData] (Len=32)
48 65 6C 6C 6F 20 57 6F 72 6C 64 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
APDU :DEBUG:kSE05x_TAG_5 [signature] (Len=71)
30 45 02 20 7E A1 14 35 BF CA BE 3C 65 FB 91 23
4C E6 93 55 B2 5D 0B A4 F5 FC 15 F9 3C 1F B8 F2
BD 83 63 27 02 21 00 ED 0F 60 45 CD 2E 78 57 2C
D9 F0 4F 51 45 E2 F5 F8 72 43 9E A1 7E 20 7E 55
C1 E1 3B 17 94 73 2D
smCom :DEBUG:H> (Len=4)
01 00 00 79
smCom :DEBUG:Tx> (Len=121)
80 03 0C 0A 74 41 04 EF 00 00 96 42 01 21 43 20
48 65 6C 6C 6F 20 57 6F 72 6C 64 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
45 47 30 45 02 20 7E A1 14 35 BF CA BE 3C 65 FB
91 23 4C E6 93 55 B2 5D 0B A4 F5 FC 15 F9 3C 1F
B8 F2 BD 83 63 27 02 21 00 ED 0F 60 45 CD 2E 78
57 2C D9 F0 4F 51 45 E2 F5 F8 72 43 9E A1 7E 20
7E 55 C1 E1 3B 17 94 73 2D
smCom :DEBUG:<H (Len=4)
01 00 00 05
smCom :DEBUG:<Rx (Len=5)
41 01 01 90 00
App :INFO :Verification Successful !!!
App :INFO :ex_sss_ecc Example Success !!!...
App :INFO :ex_sss Finished

APDU :DEBUG:CloseSession []

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛
返信

3,498件の閲覧回数
krsuresh
Contributor III
Hi @Kan_Li,
 
Thank you for your input. The sign-in was successful with your sample key and kSSS_CipherType_EC_NIST_K.
Let me know how you generate key pairs. A keypair contains 108 bytes and a public key contains 91 bytes.
According to the BIP32 protocol, the private key is 32 bytes, and the public key is 65 bytes [uncompressed SECP256K1 curve key].
Using the ex_ecc sample, I cannot send the 65 byte public to SE050 for signature verification. 
 
 
My Sample keys: 
 
    const uint8_t PrivKey[] = {
    0x87, 0xc5, 0xb9, 0xe0, 0xa2, 0x91, 0xd3, 0x18, 0x3e, 0x6a, 0xd5, 0x17, 0x05, 0xcf, 0xa2, 0x8c,
0xb4, 0xaa, 0x7b, 0x5b, 0xc0, 0x95, 0x61, 0xd6, 0x3d, 0xa4, 0xcc, 0x9f, 0xea, 0xe3, 0x17, 0xf1 };
 
    const uint8_t PubKey[] = {
    0x04, 0x47, 0xb2, 0x38, 0xcc, 0x5b, 0xda, 0x1e, 0x64, 0xa3, 0x10, 0x4a, 0x5b, 0xeb, 0x4b, 0x77,
0xc1, 0x72, 0x93, 0xf8, 0x13, 0xc1, 0xb2, 0x51, 0xe3, 0x98, 0xe6, 0x2c, 0x05, 0x23, 0xd8, 0x5b,
0xb8, 0x80, 0xcb, 0x28, 0xf1, 0x81, 0x59, 0x09, 0xdf, 0xfb, 0xaf, 0x1c, 0xf3, 0xa4, 0x59, 0x7c,
0x1a, 0x26, 0x13, 0xed, 0xd3, 0xf8, 0xcf, 0x59, 0x78, 0x8e, 0x88, 0x48, 0xa1, 0xb6, 0x5f, 0x30,
0x71};
 
Thanks,
Sureshkumar R
0 件の賞賛
返信

3,494件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @krsuresh ,

 

You may generate the key pair with openssl , just like below:

openssl ecparam -name secp256k1 -genkey -noout -out private-key.pem

openssl ec -in private-key.pem -pubout -out public-key.pem

 

Please also note the input key format for SSS APIs should be passed DER encoded using PKCS #8. Please kindly refer to simw-top/doc/sss/doc/apis-sss_key-format.html for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

3,481件の閲覧回数
krsuresh
Contributor III

Hi @Kan_Li,

 

Thanks for the reply, I am able to test ex_ecc sign-in with the new secp256k1 key. 

 

Thanks,

Sureshkumar R

3,680件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @krsuresh ,

 

Yes, it supports, and you may verify this with the demo of ex_ecc out of the MW which can be downloaded from https://www.nxp.com/webapp/Download?colCode=SE05x-PLUG-TRUST-MW&appType=license . The quick start guide for imx platform can be found in https://www.nxp.com/docs/en/application-note/AN13027.pdf .

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

3,640件の閲覧回数
krsuresh
Contributor III

Hi @Kan_Li,

Thanks for the reply, I will check the code.

Thanks,

Sureshkumar R

0 件の賞賛
返信