Does the Nano Package support authenticate sessions?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the Nano Package support authenticate sessions?

ソリューションへジャンプ
3,307件の閲覧回数
deang
Contributor III

I'd like to create an authenticated session with the se050 using an AES key.  The nano package doesn't seem to support this.  Is my understanding correct?

This is important b/c I would like to set policies for secure keys and data for a specific key.  I know you can set the authid to 0 when setting policies, but that's not what I need.

Another example, if I set the RESERVED_ID_FACTORY_RESET key with an AES key, then how do I create an authenticated session to use the DeleteAll function?

0 件の賞賛
返信
1 解決策
3,227件の閲覧回数
deang
Contributor III

Thanks Kan,  

Yes this is what I was looking for.   Let me give it a shot before closing this post.

Dean

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,258件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @deang ,

 

For AESKey session example, please kindly refer to https://github.com/NXPPlugNTrust/nano-package/blob/feature/zephyr-integration/examples/se05x_qi_auth... .

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
3,228件の閲覧回数
deang
Contributor III

Thanks Kan,  

Yes this is what I was looking for.   Let me give it a shot before closing this post.

Dean

0 件の賞賛
返信
3,266件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @deang ,

 

Actually only platform SCP is supported by Nano Package. In case, applet session is required, it can be done at the application level (inside example code).. and use scp functions to again encrypt the data. The example is available in https://github.com/NXPPlugNTrust/nano-package/blob/master/examples/se05x_mandate_scp03/src/ex_se05x_... , in which a UserId session is opened , and the data is encrypted / decrypted in example using scp functions . You may do similarly with an AESKey session.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
3,171件の閲覧回数
deang
Contributor III

Tried using the examples, but still unable to create an AES authenticated session. I don't want to burn a lot of time on debugging and porting this code.  Not being able to create an authenticated session is a big problem.  Without the ability to set policies to protect keys and objects the se050 is vulnerable and limited. 

Hopefully future versions of the Nano package will directly support authenticated sessions.

For now I will close this topic, but the problem remains.

0 件の賞賛
返信